Generating an image file

When building a project, you can optionally generate a flash image from the executable file.

To generate an image file:

  1. In the project properties, go to C/C++ Build > Settings > Cross Settings and enable the Create flash image option.


    Enabling the Create Flash Image tool

  2. Click Apply. The left pane of the dialog box now shows the Standard S32DS Create Flash Image section.
  3. In the Settings page, go to Standard S32DS Create Flash Image > General. Select the required image format and specify other options. Find the details in the Standard S32DS Create Flash Image section (Reference) of this documentation.


    Motorola S-record

    Click Apply and Close.

  4. Build the project.
  5. In the Project Explorer, open the folder with the build output (Debug or other) and find the required image file.