The following table lists options available on the SDK Management page. Some buttons can be disabled depending on the selected SDK type.
| Option | Result |
|---|---|
| Load... | Adds the SDK using the XML descriptor. |
| Reload | Updates the SDK content according to the latest changes in the SDK descriptor. |
| Edit/View... | Modifies the properties of the existing SDK (only when the SDK is not attached to any project) or displays the properties if the selected SDK is read-only. |
| Remove | Removes the selected SDK. |
| Export... | Exports the selected SDK to an archive file |
| Import... | Imports the SDK from an archive file or from a directory. |
| Import MCAL SDK | Creates a new SDK on the basis of the MCAL SDK. |
| Create... | Creates a new SDK. |
| Show Attached | Shows the list of projects to which the SDK is attached. |