The following table describes the settings that you can configure on this page.
| Option | Description |
|---|---|
| Cortex |
The ArmĀ® core used in the selected processor. Note: This check box cannot be cleared. Click Back to
select a different processor on the General properties
page.
|
|
FPU Support |
This setting enables GCC to build a project with the floating point support provided either by the processor or by a software library. The availability of options depends on the ArmĀ® core and ToolChain selection. Options:
Note: Find more information about Arm options in the GCC toolchain documentation on
the web.
|
|
Language |
This setting sets up the default compiler, linker, and preprocessor options for the toolchain and configures other project files, such as main, for the target language. Note: The selected programming language defines the toolchain settings for the
linker and compiler that will be available in the properties for the created
project. Selecting C limits the toolchain options to this
specific language. If you select C++, you will be able to
configure settings for the C and C++ compiler, linker, and preprocessor. The
toolchain settings can be further configured after creating the project. For
details, see section "C/C++ Build Tool Settings".
Options:
|
|
SDKs |
This setting allows you to select an SDK to be added to the project. Click the search button
(...) to select an SDK from the list.
Default: SDK is not
selected.Note: The
Select SDK window lists the SDKs available in S32 Design Studio . If you do not see your SDK, add it on the SDK Management page. Find the details in Adding an SDK.
|