Migrate wizard

The Migrate wizard assists you in migrating projects to new SDK or toolchain available.

The availability of migrations depends on the installed packages.


Migrate wizard

The following table describes the settings that you can configure.

Table 1. Migrate wizard properties
Option Description
Projects Shows the available projects.
Note: If opened from the Project Explorer, the corresponding projects will be selected.
Note: Multiselection is available.
Available migrations The availability of migrations depends on Projects selection (project type based).
Details Brief information on the selected migration to be performed.
Create backup Enable this option to create a backup of your project.
File The location where the project backup will be stored. Click Browse button to select location and filename.

If Create backup checkbox is clear, this field is inactive. The Browse button and backup properties selection are inactive.

Backup format Backup archive type selection. Options:
  • Use zip format
  • Use tar format
Compress the content Enable this option to compresses the contents in the archive that is created.
Backup linked resources Enable this option to backup project with all linked resources.