To edit the builder settings, open the project properties and click C/C++ Build in the left pane and the Builder Settings tab in the right pane.

| Settings | Description |
|---|---|
| Builder | Specify the builder settings:
|
| Makefile generation | Generate makefiles automatically: Enable this option to
generate a makefile with each build. Remove the flag if you have edited the makefile manually and need to keep these changes in the next builds. If required, specify a different folder for build output in the Build directory field. |
| Build location | Build directory: Specify the path of the build folder. |