To create a project with a device configuration:
-
On the main menu, click .
-
In the project creation wizard, select the processor family and the core and
specify a unique project name. Use alphanumerics (A-Z, a-z, 0-9) and underscores
('_'). Do not start the project name with a digit.
-
Click Next.
-
On the next page, define the required cores and parameters. Select an SDK to be
used.
Note: The S32 Configuration Tools are enabled by default
when an SDK is selected for the project. If SDK is not selected the
S32 Configuration Tools are not accessible for
the project.
-
Click Finish. The new project appears in the
Project Explorer.