Editing a device configuration

To let you edit a device configuration, S32 Design Studio provides perspectives named Pins, Clocks, Peripherals, DCD (Device Configuration Data), IVT (Image Vector Table), QuadSPI and DDR. The settings that you edit and save in these perspectives are automatically stored in the configuration file of the currently used project.

To edit a device configuration in a perspective, do any of the following:

The use of settings in the perspectives is beyond the scope of this document. You can read more about the subject in the S32 Configuration Tools Getting Started guide. To open this guide, click Help > Help Contents on the menu.

While configuring your processor, you can switch between the perspectives using the (Open S32 Configuration) toolbar button.

To save the changes to the project, use the Update Code toolbar button. A click on this button either saves the latest device configuration silently or opens the Update Files dialog box.

When saving the changes for the first time, click Update Code > Open Update Code Dialog.


Updating the device configuration in the project

In the Update Files dialog box, select the device configuration files to be created in the project and updated with the latest pin, clock, peripheral and other settings:


Updating the device configuration in the project

When you click OK, the project will be updated as follows:

You can configure the Update Code button to always open the Update Files dialog box or not. To do it, select or deselect the Always show details before Update Code option in the Update Files dialog box, then click OK.