This topic describes how to start a debug session in the simulation environment.
Before you proceed, make sure that you have installed the simulation software and
performed the required configuration settings. For details, refer to .
When using a certain VDK for the first time, add the VDK
configuration files to the Synopsys workspace:
- In the S32 Design Studio installation directory, go to
/S32DS/config/vpconfigs/. Copy the required
S32x folder to the clipboard.
- In your Synopsys workspace directory, browse to
/NXP_S32xxxx_ECU/vpconfigs/ where the VDK configurations for the
required target processor are located. Drop the copied S32x folder
inside.
To run a debug session:
If you need to debug a multi-core program, run launch configurations for all cores
before clicking Resume Suspended Simulation. Notice that you can
suspend execution of only one thread at a time during
debugging.