Exporting a project to a system folder or an archive file
To export a project to a system folder or to a ZIP or TAR archive file:
Right-click the project in the Project Explorer and
click Export on the context menu.
In the Export wizard, go to
General and select Archive
File or File System as the destination
for export. Click Next.
On the next wizard page, do the following:
In the left pane, remove flags from the project folders that you want to
be excluded from export. Click a folder in the left pane to see all
included files in the right pane. Remove flags from the project files to
be excluded from export.
Browse to the destination folder or archive file, or enter the path
manually. If the specified folder or archive file does not exist, it
will be created during export.