Exporting a project to a ProjectInfo.xml file

To export a project to a system folder or to a ZIP or TAR archive file:

  1. Right-click the project in the Project Explorer and click Export on the context menu.
  2. In the Export wizard, click S32 Design Studio for S32 Platform > S32DS Project as ProjectInfo XML and click Next.


    Exporting to project info

  3. Select the configuration to export.
  4. Choose to use default or absolute paths.
  5. Click Finish.
The data is exported to the ProjectInfo.xml file in the project tree and its contents are shown in the editor area.