Exporting a device configuration

To export device configuration files:

  1. Open a project with the implemented device configuration.
  2. Select the project in the Project Explorer and click File > Export on the main menu.
  3. In the Export dialog box, double-click S32 Configuration Tools. Click to export the MEX file, or expand the tool folder and click to export an HTML report, registers, pins, or source files. Click Next.


    Exporting files with device configuration

  4. If you export an HTML report, registers, or pins, browse to the destination folder. For the MEX file, specify the file name and the destination path.
    If you export the source files, click the cores which files you need to export. For each core, specify the destination folder (for instance, the board folder in a different project):


    Exporting source files

  5. Click Finish.