To import a project into the workspace:
-
Click on the main menu.
-
In the Import dialog click , then click Next
-
Browse to the ProjectInfo.xml file.
-
Specify the project name.
-
In the Project type list select the toolchain available
for the core.
Note: Be careful to select the appropriate core type toolchain, f.e.: if
importing project with linux core type, select the linux configuration.
Selecting the wrong toolchain during import may lead to unavailability to
compile the project.
-
In the Build configuration list select the configuration
available for the project type and core.
-
If you need a new launch configuration for debugging enable the
Create launch configuration option, select the debug
configuration type from the list.
-
Click Finish.
If imported with the
Create launch configuration option
enabled, the
Debug Configurations dialog will appear with a new
configuration created and the
Debugger tab displayed. For
debugger settings details refer to topic
Debugger
tab.