SVD Support tab

The SVD Support tab allows you to configure SVD files. This tab appears in debug configurations intended for debugging with PEMicro and S32 Debug Probes.


SVD support tab

Table 1. Debug Configurations - SVD Support tab
Setting Description
Clear content of Watch Registers view Enable if you want an automatic clearing of all info about registers used in the Watch registers view in previous debug session with the same SVD files. If you want system to ask confirmation for any clear, enable the Ask before clear checkbox. Default: Disabled.
Note: If the option is enabled, registers info will be cleared for all configurations that use the same SVD files.
SVD source Specify the SVD file to be used. Default: Use default SVD file.
If required, uncheck the Use default SVD file checkbox and select one of these options:
  • Specify the path manually: Type in a path to the location of the SVD file,
  • Select Device: Specify the path via specifying the device,
  • Browse Workspace: Specify the path browsing the workspace,
  • Browse File System: Specify the path browsing the file system,
  • Variables: Specify the path via setting the variable.
The new path to the SVD file appears in the SVD source field.
Support Arm Core registers Arm SVD sourse to be used. Default: Enabled (if available).