You can use the Migrate wizard
to convert SDK or GCC based tolchain for your project.
Note: Generally the SDK migration contains a toolchain migration in it.
Note: For toolchain migration refer steps 1-5 only.
The following explains how to migrate your project:
If the selected toolchain is not supported in the
New Project
wizard for the processor type of the original project, the migrated project may contain
some errors.
If system generates any errors or warnings, you can see them in the
Problems view. You can use the Quick
Fix option if possible.
Note: SDK migration has now the migrate option for SDK with no manifest. In this
situation a window should appear notifying the user that a new version of the
missing SDK is available. The window should ask the user if he wants to migrate
to the new version or to detach if he doesn't want the migration to
happen.