The integrated S32 Configuration Tools enable you to create and develop a device configuration within a project.
A device configuration sets up interconnections between the device’s pins and clocks and connected peripherals. A typical configuration specifies pin electrical features, signal routing from pins to peripherals, muxing, clock element settings, and clock output frequencies.
To store a device configuration, the S32 Configuration Tools generates a MEX configuration file and the empty board folder for the source files.

The topics in this section describe how to work with a device configuration in a project:
To learn more about the S32 Configuration Tools, refer to the S32 Configuration Tools Getting Started guide. This document can be reached from the menu.