Removing a project

When a project is finished and saved to a storage, you may prefer to remove it from the workspace and permanently delete it from the disk.

To remove a project:

  1. Right-click the project in the Project Explorer and click Delete on the context menu.
  2. In the Delete Resources dialog box, select the Delete project contents... option if you prefer to permanently delete the project files from the disk. Click OK.


    NXP licenses on the host

If you have removed the project with the Delete project contents... option not selected, the project can be restored in the workspace as described in topic Importing a project. Otherwise, the removal cannot be reverted.