You can permanently delete one or multiple custom SDKs from the workspace. When you
delete a custom SDK, it is automatically detached from all projects where it was
used.
To delete a custom SDK:
Open the location where the SDK is available:
To open the list of SDKs in the workspace, click Window > Preferences on the main menu. In the
Preferences dialog box, go to S32 Design Studio for S32 Platform > SDK Management.
To open the list of SDKs in the project, right-click the project in the
Project Explorer and click
Properties on the context menu. In the
Properties dialog box, go to
SDKs.
Select one or several SDKs and click Remove.
In the Remove SDK confirmation dialog box, click
OK to confirm the removal.