Sensor Toolbox Development Boards for FXLS8471Q 3-Axis Linear Accelerometer

Overview

Features

Features

FRDMSTBC-A8471 Shield Board and FRDMKL25-A8471 Demo Kit

FRDMSTBC-A8471  Shield Board and FRDMKL25-A8471 Demo Kit

BRKTSTBC-A8471 Breakout Board for the FXLS8471Q

BRKTSTBC-A8471 Breakout Board for the FXLS8471Q

NXP® Sensor Toolbox Demo at FTF 2016

NXP<sup>&#174;</sup> Sensor Toolbox Demo at FTF 2016 thumbnail

Running the Out of Box Demo for the FXLS8471 Linear Accelerometer

Running the Out of Box Demo for the FXLS8471 Linear Accelerometer thumbnail

Modifying the FXLS8471 Demo

Modifying the FXLS8471 Demo thumbnail

Supported Devices

Related Products

Complementary Software & Tools

Getting Started with STB-CE:

Get an ‘Out of the Box’ sensor demonstration in three simple steps:

  • Take the FXLS8471Q demo kit as listed above.
  • Plug it in to the USB port of a Windows PC.
  • Launch the Sensor Toolbox-CE software and follow the given prompts.

You can start evaluating FXLS8471Q sensor with the launched demo.

For more details on getting started with a sensor kit and sensor software tools, please find: