LPCXPRESSO: LPCXpresso IDE v8.2.2

LPCXpresso IDE Pro Edition Purchases

Before purchasing LPCXpresso IDE Pro Edition, please note...

If you already are using LPCXpresso IDE Pro Edition for an existing project, then it is still possible to purchase new Pro Edition seats. However we no longer recommend the use of LPCXpresso IDE for new projects, either in Free Edition form or the paid-for Pro Edition. MCUXpresso IDE has now replaced LPCXpresso IDE as the recommended software development toolchain for our Cortex-M based LPC microcontrollers, as well as for our Kinetis MCUs and i.MX RT crossover processors.

For more details, please visit http://www.nxp.com/mcuxpresso/ide

If you still wish to purchase LPCXpresso IDE Pro Edition:

The Pro Edition of LPCXpresso IDE provides the following enhancements over the Free Edition:

  • No debug download code size limits
  • Enhanced trace and profiling features

LPCXpresso IDE Pro Edition activation codes can purchased online from the LPCXpresso IDE webstore:

* http://sites.fastspring.com/nxpsemiconductors/product/lpcxpressoide

Information about purchasing through Fastspring, our webstore partner, can be found at:

* https://fastspring.com/purchasing-through-fastspring

Note: An LPCXpresso IDE Pro Edition activation code will also enable the Pro Edition features of MCUXpresso IDE v10.1.1 and earlier. However MCUXpresso IDE v10.2.0 and later have all functionality enabled by default without the need for a Pro Edition activation code.