I can’t verify that the meanings of the errors are correct, but I did notice that there are some references to other FAQs that should be hyperlinked but are not. I’ll highlight below in green. I also changed the wording on two answers (highlighted in yellow).
Message - 5: "Unable to use the plugin"
It is licensed and a valid license key was not found. No such feature exists.
- A. The specified feature is missing in the license file. Either it is an incomplete license file or a tools/software part is used which is not covered by the license file. Please contact support.
Message - 9: "Unable to use the plugin"
It is licensed and a valid license key was not found. Invalid host. The hostid of this system does not match the hostid specified in the license file.
Message - 10: "Unable to use the plugin"
It is licensed and a valid license key was not found.
Feature has expired.
- The license file has expired. If you want to continue using the product, you need a new license file with a valid expiration date.
Message - 25: "Unable to use the plugin"
It is licensed and a valid license key was not found. License server does not support this version of this feature.
- License file is invalid. Or an outdated license file is used with a new version of the software.
Message - 88: " Unable to use the plugin"
It is licensed and a valid license key was not found. System clock has been set back.
- This error appears when you’re using a temporary license and your computer’s clock has been set back. Modifying the date or time on your computer will prevent you from using a temporary licenses. The clock may have been set back accidentally or by installing software which installs files with illegal (future) file dates. You need to set the correct date on your system and review for any file created with invalid dates.
Message - 90
Future license file format or misspelling in license file. The file was issued for a later version of FLEXlm than this program understands.
- You may be using your software in terminal server mode. There is an option for a flag in the license file (TS_OK) which could help here. You should ask support for a new license file with the TS_OK flag set.