LPC Production Programming

Efficient and fast Flash programming in the production flow is a critical part of cost-effective manufacturing and field servicing of LPC microcontrollers. LPC ecosystem partners offer a range of scalable, leading-edge programming solutions to optimize this flow.

Some partners specialize in production programming systems, designed to scale to highly parallel mass production. These systems support various programming schemes, using both parallel and SWB-based "used to program devices already mounted on boards, utilizing LPC MCUs' built-in flash programming routines. Various JTAG debuggers and emulators can also be used to program the on-chip Flash of LPC devices on a smaller scale and for field upgrades.

For a complete list of partners offering production programming services, please review their introductory messages below. Refer to the Partner Cross Reference for LPC MCUs for specific devices supported by each partner.

Elnec

Elnec is Europe's leading provider of solutions for programming NAND Flash memories, microcontrollers and other programmable devices. Elnec is committed to set a new standard in the industry by providing highly universal, reliable and cost effective programming solutions for devices in any package, whether programmed in a socket or through ISP on a circuit board.

ESA

ESA provide products, consulting and training for embedded systems. Our expertise covers many microcontroller architectures and their development tools, with a focus on Controller Area Network (CAN), CANopen, consumer, industrial, medical, sub-sea and automotive. We develop and manage a full range of CANopen software products and development tools, along with bootloaders, network analysis and simulation. We are the developers of Flash Magic for ISP of NXP microcontrollers.

SEGGER

SEGGER offers professional Embedded Software and Development Tools designed from the ground up specifically for embedded systems. With decades of experience in programming efficiently on embedded systems, SEGGER has created highly integrated, cost-effective programming and development tools, such as the industry leading JLink/JTrace line of debug probes and Flashers (stand-alone flash programmer) which make use of SEGGER's own RTOS (embOS) and middleware.

SMH Technologies

SMH Technologies is a global, independent, leader in Silicon Device In-System Programming and related services for the electronic board manufacturing industry. FlashRunner series is a range of high-performance, standalone In-System Programmers specific for Flash-based microcontrollers and serial memories, which easily interfaces on a programming system or Automatic Test Equipment (ATE) and can work either in full standalone mode or under the control of a host system. FlashRunner's flexible and modular design, enables the same algorithms to be used on all product models.

Xeltek

Xeltek has developed and manufactured universal Parallel, ISP, Production and Automated Programmers since 1991. Universal programmers and adapters from the SuperPro® line cover programming demands from engineering development to automated volume production at competitive prices; universal socket adapters support various package types such as PLCC, SOIC, SOP, TSOP, QFP, SDIP and uBGA. Contact Xeltek to learn about new release of faster programmers that meet new performance expectation for both parallel and in-system (LabVIEW interface) programming technology.

PEmicro

PEmicro is an industry trendsetter in hardware and software development tools for NXP and Arm® Cortex® microcontrollers. We take pride in our committment to providing professional, low-cost development tools and prompt, knowledgeable customer support. PEmicro was founded in Boston and incorporated in 1982. Early on we developed and marketed the first general purpose EPROM programmer, and we've since continued to innovate embedded systems tools with cutting-edge features, such as our popular Cyclone production programmers.