MCUXpresso Integrated Development Environment (IDE)

MCUXpresso IDE Pro Edition Purchases

The Pro Edition of MCUXpresso IDE provides the following enhancements over the Free Edition:

  • Enhanced LinkServer/LPC-Link2 SWO trace and profiling features:
  • Technical support: one year of email ticket-based support from NXP engineers on the use of MCUXpresso IDE (in addition to free forum-based support)

A dedicated MCUXpresso IDE webstore will be available shortly. In the meantime, an LPCXpresso IDE Pro Edition activation code will also enable Pro Edition features for MCUXpresso IDE. You can purchase an LPCXpresso IDE Pro Edition activation code via : http://www.nxp.com/lpcxpresso/purchase