Processor Expert® Software Suites

Processor Expert Software is a development system to create, configure, optimize, migrate, and deliver software components that generate source code for NXP silicon. Processor Expert software covers Our S08/RS08, S12(X), Coldfire, Coldfire+, Kinetis, DSC 56800/E, QorIQ and some other Power Architecture processors. Processor Expert software is available as part of the CodeWarrior tool suite or as an Eclipse-based plug-in feature for installation into an independent Eclipse environment.