Connectivity Tool Suite

CONNECTIVITY-TOOL-SUITE

Roll over image to zoom in

Software Details

Select a section:

Features

Kinetis Protocol Analyzer Adapter

  • Bluetooth® Low Energy and IEEE 802.15.4 radio packets sniffing
  • Start sniffing in one click
  • Choose any combination of Bluetooth® Low Energy primary advertising channels on which to start sniffing
  • Filter Bluetooth® Low Energy traffic by the advertiser and/or initiator addresses of a specific connection
  • Easily choose the filtering addresses from a list of auto-detected addresses
  • Follow secured Bluetooth® Low Energy connections
  • Live edit the LTK key of a specific connection to decrypt packets
  • Add any number of predefined LTK keys (to use them now or just store them for later)
  • Easy ignore specific COM ports by adding them to a list
  • Open Wireshark on a preselected virtual interface in just one click

Firmware Loader

  • New, updated and improved user interface
  • Download new firmware onto the flash memory of NXP development boards
  • Rewrite the whole flash memory
  • Easily write a combo of an application and a bootloader (or any other combo)
  • Save the combo as one binary for future use
  • Use Motorola S-record (.srec) files and binary files (.bin)
  • Select a checkbox to mark a file as bootloader and the rest is handled
  • Easily change the writing start address of each file selected
  • Have the last 10 browsed images at hand to use them again quickly
  • Erase the flash memory in one click
  • Read the whole flash memory or just a specific section
  • View the read data in the application or save it as .bin, .txt or .log
  • Reset the board in just one click

NXP Test Tool – Command Console

  • Send and receive IEEE 802.15.4, Thread, Bluetooth® Low Energy and ZigBee 3.0 commands to and from an NXP development board
  • Easily configure the serial connection settings for a selected COM port
  • Quickly open Device Manager in one click
  • Send data to devices that are in low-power mode
  • Select a device connected to a remote PC using a TCP/IP connection
  • Send commands to the board in just a double-click
  • Easily switch among different sets of commands depending on the preferred protocol
  • Add shortcut to commands
  • Save two or more commands as a macro script to send them as a group now or later
  • Customize the colors of the text and background or filter of the RX/TX log entries

NXP Test Tool – Firmware Loader

  • Download new firmware onto the flash memory of NXP development boards
  • Rewrite the whole flash memory
  • Easily write a combo of an application and a bootloader
  • Use Motorola S-record (.srec) files and binary files (.bin)

NXP Test Tool – OTA Updates for MAC, Thread and Bluetooth® Low Energy

  • Download new firmware onto the flash memory of NXP Kinetis development boards
  • Over-the-air (OTA) update of firmware
  • Use Motorola S-record (.srec) files and binary files (.bin)
  • Easily connect to the OTA server device
  • Get live updates about the transfer between the server and the client

NXP Test Tool – Zigbee® Gateway Graphical User Interface (ZGWUI)

  • Set up and run a Zigbee network easily using NXP ZigBee 3.0 IoT Control Bridge
  • Easily configure and open a new serial connection
  • Configure the nodes and join them to the network using a classic join or NFC
  • Send commands to control the devices
  • Receive live responses from devices
  • Add devices into groups and use group commands
  • Associate a scene to a group and send scene commands
  • Send over-the-air (OTA) upgrades to clients

Connectivity Tools Launcher

  • Easily manage all the connectivity tools installed on the system
  • Download any connectivity tool from the NXP website
  • Minimalist interface
  • Quickly launch any connectivity application
  • Open documentation
  • Update the application
  • Open the license
  • Uninstall the application
  • Open the containing folder of the application

Over-the-Air Programming

  • Download new firmware wirelessly onto the flash memory of NXP development boards
  • Quickly switch among 802.15.4 MAC, Thread, Bluetooth Low Energy, Matter and Zigbee protocols
  • Follow OTAP demo steps for the preferred protocol
  • Easily set up and run a ZigBee or Thread network from the OTAP interface
  • Save the OTA file (including the OTA header) as binary
  • Drag and drop Motorola S-record (.srec) files or binary files (.bin)
  • Have the last 10 browsed images at hand to use them again quickly
  • Filter detected binaries either by processor name or by a custom filter
  • Easily configure serial settings and connect to the OTA server device
  • Get live transfer details about the OTA transfer
  • Quickly open Firmware Loader from a shortcut button to download OTAP server/client firmware

Downloads

5 downloads

Note: For better experience, software downloads are recommended on desktop.

Documentation

Quick reference to our documentation types.

2 documents

Design Resources

Select a section:

Hardware

1-5 of 18 hardware offerings

Show All

Related Software

1 software file

Note: For better experience, software downloads are recommended on desktop.

Training

2 trainings

Support

What do you need help with?