Automotive Ethernet Congress

Munich, Germany
13 – 14 February

Powerful network for the computer on wheels

In 17 lectures, two keynotes, five workshops and a concluding panel discussion, the fifth Automotive Ethernet Congress on February 13 and 14, 2019 in Munich will shed light on the entire range of topics surrounding the use of Ethernet in vehicles.

The vehicle is undergoing the greatest change since its inception. Automation, networking, and digitalization of the vehicle with the environment and occupants will completely change individual mobility. Automotive Ethernet is important for this powerful vehicle network, as it is not only a fast and inexpensive form of data transmission in automobiles, but also offers advantages such as standardization, scalability and support for IP protocols.

Automotive Ethernet Congress Program

Don’t miss NXP’s technical presentations on latest NXP technologies:

Date Time Session/Workshop Presentation Title
February 13, 2019 11:30 - 12:00 Session 2 Automotive wake-up and Sleep - The Way From 100BASE-T1 to 1000BASE-T1
February 13, 2019 16:00- 18:00 Workshop 3 Workshop 3: TSN and Security: Dimensioning the Roles of the Switch and the Processor