MCUXpresso IDE - Project Settings


  • Posted Date: 05 October 2017
  • 3008 Views

The MCUXpresso IDE brings developers an easy-to-use Eclipse-based development environment for NXP MCUs based on Arm® Cortex®-M cores, including LPC and Kinetis microcontrollers. The MCUXpresso IDE offers advanced editing, compiling and debugging features with the addition of MCU-specific debugging views, code trace and profiling, multicore debugging, and more.

These short tutorial videos will show how to get an software development kit (SDK) package from the MCUXpresso SDK, import it into the MCXpresso IDE, and then get started using it. It will also show how to create an MCUXpresso SDK example project and debug it within the MCUXpresso IDE, how to inspect and remove installed SDK's, show SDK location on disk and configuration items, and go through the normal edit, debug, compile cycles. It will also cover how to import or create new projects from other IDEs (i.e. Kinetis Design Studio and LPCOpen).

Video Overview

This video will show users how to change the project settings and options in MCUXpresso IDE, including how to change the compiler, assembler and liner options.