1
Plug It In2
Get Software3
Build, Run4
Create5
LearnSign in to save your progress. Don't have an account? Create one.
Let's take your FRDM-KV11Z for a test drive! Please follow the detailed actions list below.
Something went wrong! Please try again.
Your FRDM-KV11Z comes loaded with a demonstration project called “frdmkv11z_bubble.bin”. The RGB LED will illuminate one color when tilt on one axis and another when tilted on the other. This project was compiled from the demo projects available in the MCUXpresso SDK
Something went wrong! Please try again.
The software and tools installation is detailed in the steps below.
The MCUXpresso SDK is complimentary and includes full source code under a permissive open source license for all hardware abstraction and peripheral driver software.
Click below to download a preconfigured SDK release for the FRDM-KV11Z.
You can also use the online SDK Builder to create a custom SDK package for the FRDM-K64F using the SDK builder.
Something went wrong! Please try again.
NXP offers a complimentary toolchain called MCUXpresso IDE.
Want to use a different toolchain?
No problem! The MCUXpresso SDK includes support for other tools such as IAR, Keil and command-line GCC.
Something went wrong! Please try again.
The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and also provides pin and clock tools to generate initialization C code for custom board support.
Something went wrong! Please try again.
Many of the example applications output data over the MCU UART so you'll want to make sure that the driver for the board's virtual COM port is installed. Before you run the driver installer, you MUST have the board plugged in to your PC.
With the serial port driver installed, run your favorite terminal application to view the serial output from the MCU's UART. Configure the terminal to 115200 baud rate, 8 data bits, no parity, and 1 stop bit. To determine the port number of the FRDM-K64F's virtual COM port, open the device manager and look under the "Ports" group.
Not sure how to use a terminal application? Try one of these tutorials:
Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
Something went wrong! Please try again.
Please follow along the steps below.
The MCUXpresso SDK comes with a long list of example applications code. To see what's available, browse
to the SDK boards folder of your SDK installation and select your board, the FRDM-KV11Z
(
To learn more about specific example code, open the readme.txt file in an example’s directory.
Something went wrong! Please try again.
If one or more of the demo applications or driver examples sounds interesting, you're probably wanting to know how you can build and debug yourself. The Getting Started with MCUXpresso SDK guide provides easy, step-by-step instructions on how to configure, build, and debug demos for all toolchains supported by the SDK.
Use the guide below to learn how to open, build and debug an example application using the MCUXpresso IDE.
Using a different toolchain?
The following steps will guide you through opening the hello_world application. These steps may change slightly for other example applications as some of these applications may have additional layers of folders in their path.
If not already done, open the desired example application workspace. Most example application workspace files can be located using the following path:
Using the hello_world demo as an example, the path is:
Select the desired build target from the drop-down. For this example, select the "hello_world — Debug" target.
To build the application, click the "Make" button, highlighted in red below.
The build will complete without errors.
The FRDM-KV11Z board comes loaded with the P&E bootloader and OpenSDA debug interface from the factory. If you have changed the debug OpenSDA application on your board, visit http://www.pemicro.com/opensda for information on updating or restoring your board to the factory state
Connect the development platform to your PC via USB cable between the "SDAUSB" USB port on the board and the PC USB connector.
Open the terminal application on the PC (such as PuTTY or TeraTerm) and connect to the debug COM port you determined earlier. Configure the terminal with these settings:
Click the "Download and Debug" button to download the application to the target.
The application is then downloaded to the target and automatically runs to the main() function.
Run the code by clicking the "Go" button to start the application.
The hello_world application is now running and a banner is displayed on the terminal. If this is not the case, check your terminal settings and connections.
After the MDK tools are installed, Cortex® Microcontroller Software Interface Standard (CMSIS) device packs must be installed to fully support the device from a debug perspective. These packs include things such as memory map information, register definitions and flash programming algorithms. Follow these steps to install the appropriate CMSIS pack.
Open the MDK IDE, which is called µVision. In the IDE, select the "Pack Installer" icon.
In the Pack Installer window, navigate to the section with the Kinetis packs (they are in alphabetical order). The Kinetis packs start with “Keil::Kinetis” and are followed by the MCU family name, for example “Keil::Kinetis_K80_DFP”. Because this example uses the FRDM-K82F platform, the K80 family pack is selected. Click on the “Install” button next to the pack. This process requires an internet connection to successfully complete.
After the installation finishes, close the Pack Installer window and return to the µVision IDE.
The following steps will guide you through opening the hello_world application. These steps may change slightly for other example applications as some of these applications may have additional layers of folders in their path.
If not already done, open the desired demo application workspace in:
The workspace file is named
To build the demo project, select the "Rebuild" button, highlighted in red.
The build will complete without errors.
The FRDM-KV11Z board comes loaded with the P&E boot loader and OpenSDA debug interface from the factory. If you have changed the debug OpenSDA application on your board, visit http://www.pemicro.com/opensda for information on updating or restoring your board to the factory state.
Connect the development platform to your PC via USB cable between the "SDAUSB" USB port on the board and the PC USB connector.
Open the terminal application on the PC (such as PuTTY or TeraTerm) and connect to the debug COM port you determined earlier. Configure the terminal with these settings:
After the application is properly built and debug setting complete, click the "Download" button to download the application to the target.
After clicking the "Download" button, the application downloads to the target and should be running. To debug the application, click the "Start/Stop Debug Session" button, highlighted in red.
Run the code by clicking the "Run" button to start the application.
The hello_world application is now running and a banner is displayed on the terminal. If this is not the case, check your terminal settings and connections.
The following steps will guide you through opening the hello_world example.
Find the Quickstart Panel in the lower left hand corner
Then click on Import SDK examples(s)…
Click on the frdmkv11z board to select that you want to import an example that can run on that board, and then click on Next.
Use the arrow button to expand the demo_apps category, and then click the checkbox next to hello_world to select that project. To use the UART for printing (instead of the default semihosting), clear the “Enable semihost” checkbox under the project options. Then, click on Next.
On the Advanced Settings wizard, clear the checkbox “Redirect SDK “PRINTF” to C library “printf”“ in order to use the MCUXpresso SDK console functions for printing instead of generic C library ones. Then click on Finish.
Now build the project by clicking on the project name and then click on the Build icon.
You can see the status of the build in the Console tab.
MCUXpresso IDE will probe for connected boards and should find the OpenSDA debug probe that is part of the integrated OpenSDA circuit on the FRDM-KV11Z. Click on OK to continue.
The firmware will be downloaded to the board and the debugger started.
Open up a terminal program and connect to the COM port the board enumerated as. Use 115200 baud 8 data bits, no parity and 1 stop bit.
Start the application by clicking the "Resume" button:
The hello_world application is now running and a banner is displayed on the terminal. If this is not the case, check your terminal settings and connections.
Use the controls in the menu bar to pause, step into, and step over instructions, and then stop the debugging session by click on the Terminate icon:
This section contains the steps to install the necessary components required to build and run a KSDK demo application with the Arm GCC toolchain, as supported by the Kinetis SDK. There are many ways to use Arm GCC tools, but this example focuses on a Windows environment. Though not discussed here, GCC tools can also be used with both Linux OS and Mac OSX.
Download and run the installer from https://developer.arm.com/open-source/gnutoolchain/gnu-rm. This is the actual toolchain (i.e., compiler, linker, etc.). The GCC toolchain should correspond to the latest supported version, as described in the Kinetis SDK Release Notes.
The Minimalist GNU for Windows (MinGW) development tools provide a set of tools that are not dependent on third party C-Runtime DLLs (such as Cygwin). The build environment used by the KSDK does not utilize the MinGW build tools, but does leverage the base install of both MinGW and MSYS. MSYS provides a basic shell with a Unix-like interface and tools.
Download the latest MinGW mingw-get-setup installer from sourceforge.net/projects/mingw/files/Installer/.
Run the installer. The recommended installation path is C:\MinGW, however, you may install to any location.
NOTE
The installation path cannot contain any spaces.
Ensure that the "mingw32-base" and "msys-base" are selected under Basic Setup.
Click "Apply Changes" in the "Installation" menu and follow the remaining instructions to complete the installation.
Add the appropriate item to the Windows operating system Path environment variable. It can be found under Control Panel -> System and Security -> System -> Advanced System Settings in the "Environment Variables..." section. The path is:
Assuming the default installation path, C:\MinGW, an example is shown below. If the path is not set correctly, the toolchain does not work.
NOTE
If you have "C:\MinGW\msys\x.x\bin" in your PATH variable (as required by KSDK 1.0.0), remove it to ensure that the new GCC build system works correctly.
Create a new system environment variable and name it ARMGCC_DIR. The value of this variable should point to the Arm GCC Embedded tool chain installation path, which, for this example, is:
C:\Program Files (x86)\GNU Tools Arm Embedded\4.9 2015q3
Reference the installation folder of the GNU Arm GCC Embedded tools for the exact path name of your installation.
Download CMake 3.0.x from www.cmake.org/cmake/resources/software.html.
Install CMake, ensuring that the option "Add CMake to system PATH" is selected when installing. It's up to the user to select whether it's installed into the PATH for all users or just the current user. In this example, the assumption is that it's installed for all users.
Follow the remaining instructions of the installer.
You may need to reboot your system for the PATH changes to take effect.
To build an example application, follow these steps.
If not already running, open a GCC Arm Embedded tool chain
command window. To launch the window, from the Windows
operating system Start menu, go to "Programs -> GNU
Tools Arm Embedded
Change the directory to the example application project directory, which has a path like this:
For this guide, the exact path is:
Type "build_debug.bat" on the command line or double click on the "build_debug.bat" file in Windows operating system Explorer to perform the build. The output is shown in this figure:
The GCC tools require a J-Link debug interface. To update the OpenSDA firmware on your board to the latest J-Link app, visit www.nxp.com/opensda. After installing the J-Link OpenSDA application, download the J-Link driver and software package from www.segger.com/downloads.html.
Connect the development platform to your PC via USB cable between the "SDAUSB" USB port on the board and the PC USB connector.
Open the terminal application on the PC (such as PuTTY or TeraTerm) and connect to the debug COM port you determined earlier. Configure the terminal with these settings:
Open the J-Link GDB Server application. Assuming the J-Link software is installed, the application can be launched by going to the Windows operating system Start menu and selecting "Programs -> SEGGER -> J-Link J-Link GDB Server".
Modify the settings as shown below. The target device selection chosen for this example is the "MK82FN256xxx15" and uses the SWD interface.
After it is connected, the screen should resemble this figure:
If not already running, open a GCC Arm Embedded tool chain
command window. To launch the window, from the Windows
operating system Start menu, go to "Programs -> GNU Tools
Arm Embedded
Change to the directory that contains the demo application output. The output can be found in using one of these paths, depending on the build target selected:
For this example, the path is:
Run the command "arm-none-eabi-gdb.exe
Run these commands:
The application is now downloaded and halted at the reset vector. Execute the “monitor go” command to start the example application
The hello_world application is now running and a banner is displayed in the terminal window.
Something went wrong! Please try again.
Option A: Use the MCUXpresso IDE to clone an example project.
Option B: Use the MCUXpresso Config Tool to clone an existing MCUXpresso SDK example for use with third party IDEs.
Something went wrong! Please try again.
Now, let’s use the Pins tool that is part of the MCUXpresso Config Tool to show how to add a new GPIO pin to your project to blink an LED.
Something went wrong! Please try again.
Next use the Clocks tool that is part of the MCUXpresso Config Tool to change the clock settings and change the rate that the LED blinks.
Something went wrong! Please try again.
With the application modified, you will see the FRDM-KV11Z’s blue LED slowly blinking. You can also view terminal output using the terminal program.
To clone an existing demo app or driver example for use with a third-party IDE use MCUXpresso Config Tool.
NOTE: This procedure for the two projects mc_pmsm and mc_bldc does not compile due to the library files not being copied with the project.
Select the directory to export the clock_config.c and clock_config.h files. In this example export to the “board” folder in the led_output project in the workspace.
(i.e. C:\MCUXpressoIDE_Lab\frdmkv11z_driver_examples_gpio_led_output\board). Remove the text “\Project\board” then select Finish.
Something went wrong! Please try again.
Explore beyond the FRDM-KV11 by adding other NXP solutions to your project and interact with our worldwide design community
Explore the world with a full assortment of NXP sensor solutions. From accelerometers, pressure sensors, touch sensors, and many more, NXP has a sensor solution for your project. Find out more at http://nxp.com/sensors
Something went wrong! Please try again.
Near Field Communication is a simple, intuitive technology that lets you interact securely with the world around you with a simple touch. Learn more about NXP’s NFC solutions at http://nxp.com/nfc
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with Kinetis MCUs and MCUXpresso Software and Tools. Join the community discussion in one of our two dedicated communities: Kinetis MCU Community or MCUXpresso Software and Tools Community
No problem! Your board simply came in the old packaging and has a different out-of-box demo loaded into the flash memory.
You should be seeing the red and green LEDs toggling back and forth. It's OK to move onto the next step when you're ready
Try proceeding to the next steps to get other example applications running on your board. If you still have problems, try contacting us through the NXP Community.
Something went wrong! Please try again.