NXP has released its Real-Time Drivers (RTD) software as the new S32K3 MCU family enters production.
Delivering on its promise to tackle the cost and complexity of automotive software development, NXP has released its Real-Time Drivers (RTD) software supporting all S32 automotive processors featuring Arm® Cortex®-M or Cortex-R52 cores. One of several new offerings in the S32 software enablement platform, RTD supports the new S32K3 and existing S32K1/S32G families with a package of production-grade, safety-compliant software drivers that aim to simplify AUTOSAR and non-AUTOSAR application development. The use of a common code base and software API helps maximize software reuse across processor platforms, while the inclusion of the production license in the silicon price broadens AUTOSAR access for mass market developers.
As modern cars transition to software-defined vehicles, automotive software has emerged as the central development challenge. The S32K3 MCU software offerings help customers address this challenge while benefiting from the S32 Automotive platform’s common architecture and high levels of functional safety and security.
Software includes:
RTD has also been extended to the successful S32K1 MCU family providing software portability across the entire S32K portfolio from 128 KB to 8 MB and 32-pin to 289-pin.
Additional complimentary software for S32K3 MCUs includes Hardware Security Engine (HSE) firmware designed to anticipate future OEM requirements, and an Inter-Platform Communication Framework (IPCF) – middleware for managing communication and resources in multi -core/OS systems. A new Safety Software Framework (SAF) is available under license and contains safety libraries for fault detection and reaction mechanisms providing a foundation for ISO 26262 compliance.
S32K3 samples, evaluation boards and developer resources are expected to be available from early November at NXP Connects 2021 and the S32K3 product page.
S32K3 Family Availability:
S32K3 Family | Features | Planned Availability |
---|---|---|
K344/24/14 | Lockstep / Dual / Single Arm Cortex-M7, ASIL D/B 4 MB Flash, HSE, CAN FD, Ethernet, OTA 257 MAPBGA, 172 MaxQFP (16x16 mm) |
Sampling now Production 4th quarter 2021 |
K312 | Single Arm Cortex-M7, ASIL B 2 MB Flash, HSE, CAN FD, Ethernet, OTA 172 MaxQFP, 100 MaxQFP (10x10 mm) |
Sampling now Production 2nd quarter 2022 |
K342/41/22 | Lockstep / Dual Arm Cortex-M7, ASIL D/B, 2/1/2 MB Flash, HSE, CAN FD, Ethernet, OTA 172 MaxQFP, 100 MaxQFP |
Sampling now Production 4th quarter 2022 |
NXP Semiconductors N.V. (NASDAQ: NXPI) enables secure connections for a smarter world, advancing solutions that make lives easier, better, and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the automotive, industrial & IoT, mobile, and communication infrastructure markets. Built on more than 60 years of combined experience and expertise, the company has approximately 29,000 employees in more than 30 countries and posted revenue of $8.61 billion in 2020. Find out more at NXP Semiconductors.
NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2021 NXP B.V.
Tags: Automotive, Corporate