Getting Started with the MCSPTE1AK344 Development Kit

Last Modified: Jul 8, 2026 updated Supports S32K344 BLDC/PMSM Development Kit

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Software
  • 3

    Plug It In
  • 4

    Build

1. Out of the Box

1.1 Introduction

The NXP MCSPTE1AK344 development kit provides an easy-to-use platform for evaluating and prototyping automotive brushless direct current (BLDC) and permanent magnet synchronous motor (PMSM) motor control applications. Based on the S32K344 microcontroller and GD3000 pre-driver, the kit helps you begin development before the final hardware is available.

This guide walks you through the process of setting up the MCSPTE1AK344 development kit, installing the required software, connecting the hardware, building and debugging the application project, and using FreeMASTER with the Motor Control Application Tuning (MCAT) tool to run and tune the motor.

1.2 Get to Know the MCSPTE1AK344 Motor Control Development Kit

Review each visual below to familiarize yourself with all of the components of the kit's parts.

Figure 1. MCSPTE1AK344 Motor Control Development Kit

Figure 1. MCSPTE1AK344 Motor Control Development Kit

1.3 Get to Know the S32K344 Evaluation Board

The diagram below locates and identifies components of the S32K344 evaluation board.

Figure 2. S32K3X4EVB-Q172 Board Features

Figure 2. S32K3X4EVB-Q172 Board Features

1.4 Get to Know the DEVKIT-MOTORGD

Labeled below are the components for the DEVKIT-MOTORGD.

Figure 3. DEVKIT-MOTORGD Board

Figure 3. DEVKIT-MOTORGD Board

1.5 Header/Pinout for PMSM Motor Control

The S32K344EVB controls the DEVKIT-MOTORGD through the inner pins of the I/O headers, which are Arduino compatible.

Below you will find the pin configuration for the PMSM motor control with the configurable pins indicated in red.

Figure 4. PMSM Pinout

Figure 4. PMSM Pinout

1.6 Header/Pinout for BLDC Motor Control

The S32K344EVB controls the DEVKIT-MOTORGD through the inner pins of the I/O headers, which are Arduino compatible.

Below you will find the pin configuration for the BLDC motor control with the configurable pins indicated in red.

Figure 5. BLDC Pinout

Figure 5. BLDC Pinout

2. Get Software

To access the software (SW) for this development kit, you will sign in at NXP.com with your credentials.

2.1 Download SW packages from Automotive Software Package Manager

First, you will open the Automotive Software Package Manager and select option "S32K3" under "General-Purpose MCUs".

Figure 6. Package Manager S32K3

Figure 6. Package Manager S32K3

Expand the "FRDM Automotive Board Installation Package" bundle and check the boxes for "S32 Design Studio", "Real-Time Drivers" and "FreeMASTER" software (other packages are optional).

Figure 7. Package Manager FRDM-A Bundle

Figure 7. Package Manager FRDM-A Bundle

Click the "Generate Bundle Installer" button at the end of the page.

Figure 8. Package Manager Generate Bundle Installer

Next you will go through accepting the Export Control and SW License Agreement. Review and scroll all the way to the bottom where you will accept the terms. Once you have accepted the terms, you will close the wizard to proceed with installation. Installer and Installer User Manual download will start automatically in a few moments.

Figure 9. MultiInstaller

Figure 9. MultiInstaller

To simplify the installation process for the FRDM Automotive Board Installation Package SW bundle, the installation and configuration is automated.

Figure 10. MultiInstaller

Figure 10. MultiInstaller

2.2 Add GNU Compiler Collection (GCC) Toolchain Version 10.2

Because the latest versions of S32 Design Studio only include GCC toolchain version 11.4., you will need to install version 10.2, which is compatible with Real-Time Drivers (RTD).

In S32 Design Studio, from the top menu, go to Help $rarr; S32DS Extensions and Updates. In the S32DS Extensions and Updates dialog, you will install GCC toolchain version 10.2.

Figure 11. GCC 10.2 Installation

Figure 11. GCC 10.2 Installation

For access to the optional SW go to S32 Design Studio and from the top menu, select Help → S32DS Extensions and Updates. In the S32DS Extensions and Updates dialog, click Add Update Sites.

Alternatively, you can drag the downloaded update site file and drop it into the S32DS Extensions and Updates dialog. The added software package will be automatically selected for installation.

Figure 12. Add Update Sites

Figure 12. Add Update Sites

2.3 Get FreeMASTER Application Tool for Real-Time Debugging

Download and install the FreeMASTER application tool for real-time debugging.

Figure 13. FreeMASTER Installer

Figure 13. FreeMASTER Installer

2.4 Get Automotive Math and Motor Control Library (AMMCLib) Set

Download and install AMMCLib for S32K3xx.

Figure 14. Download AMMCLib

Figure 14. Download AMMCLib

Figure 15. AMMCLib Installer

Figure 15. AMMCLib Installer

2.5 Download the Development Kit Application Software

Download and install the MCSTE1AK344 motor control application software package.

Figure 16. MCSPTE1AK344-SW Install

Figure 16. MCSPTE1AK344-SW Install

Figure 17. AMMCLib Install Request

Figure 17. AMMCLib Install Request

2.6 Elektrobit tresos Studio and Standalone RTDs (Optional Step for AUTOSAR Examples)

  1. Download and install Elektrobit tresos Studio / AUTOSAR® Configuration Tool from S32K3 Standard Software Package
  2. Figure 18. EB tresos Installer

    Figure 18. EB tresos Installer
  3. Download and install the .exe file of the S32K3 Real-Time Drivers for Cortex-M from the S32K3 Standard Software Package
  4. Figure 19. RTD Installer

    Figure 19. RTD Installer

    To save configuration time, select the EB tresos installation directory when prompted.

    If you installed RTD prior EB tresos, create a SW32K3_S32M27x_RTD_R23-11_7.0.0_QLP03.link file in C:\EB\tresos\links folder with the content: "path=C:/NXP/SW32K3_S32M27x_RTD_R23-11_7.0.0_QLP03".

    Figure 20. RTD Link

    Figure 20. RTD Link

3. Plug It In

This section will walk you through how to set up connections.

3.1 Check the Default Jumper Positions in the MCSPTE1AK344 Development Kit

Reference the charts and diagrams below for set-up of the development kit jumpers.

Figure 21. S32K3X4EVB-T172 Default Jumpers

Figure 21. S32K3X4EVB-T172 Default Jumpers
S32K3X4EVB-T172 Default Jumper Settings
Jumper State Notes
J1 CLOSED Disabled FS26 watchdog after power-up
J5 1-2 Select voltage level for FS26 DEBUG pin
J8 CLOSED External circuits powered from VDD_HV_B domain
J9 CLOSED External circuits powered from VDD_HV_A domain
J427 CLOSED The MCU peripherals powered from the VDD_HV_A domain
J15 CLOSED The MCU peripherals powered from the VDD_HV_B domain
J18 1-2 5 V for the VDD_HV_A domain
J13 1-2 3.3 V for the VDD_HV_B domain
J20 OPEN LIN1 Commander* mode
J22 1-2 5 V from FS26 SBC
J24 OPEN LIN2 Commander* mode
J26 CLOSED 3.3 V from FS26 SBC
J30 OPEN FS26 wake inputs
J31 1-2 V15 domain powered from FS26 SBC
J44 OPEN On-board debugger UART pins
J423 CLOSED 12 V from J14 connector
J424 CLOSED Connect 3.3 V voltage signal with 3.3 V MCU power domain option
*Commander in the LIN standard document.

Figure 22. S32K3X4EVB-Q172 Default Jumpers

Figure 22. S32K3X4EVB-Q172 Default Jumpers
S32K3X4EVB-Q172 Default Jumper Settings
Jumper State Notes
J1 CLOSED Disabled FS26 watchdog after power-up
J5 1-2 Select voltage level for FS26 DEBUG pin
J8 CLOSED External circuits powered from VDD_HV_B domain
J9 CLOSED External circuits powered from VDD_HV_A domain
J10 CLOSED The MCU peripherals powered from the VDD_HV_A domain
J18 1-2 5 V for the VDD_HV_A domain
J20 OPEN LIN1 Commander* mode
J22 1-2 5 V from FS26 SBC
J24 OPEN LIN2 Commander* mode
J26 CLOSED 3.3 V from FS26 SBC
J30 OPEN FS26 wake inputs
J44 OPEN On-board debugger UART pins
*Commander in the LIN standard document.

3.2 Set Up Jumpers in the DEVKIT-MOTORGD Evaluation Board

Reference the charts and diagrams below for set-up of the evaluation board jumpers.

Jumper Setting Option Description
J8 Short HALL/Encoder interface Voltage level for HALL/Encoder interface is 3.3 V
Open Voltage level for HALL/Encoder interface is 5.0 V (default)
J9/J10/J11 1-2 Motor Type Bidirectional 3-phase current sensing for PMSM FOC (sinusoidal) motor control
2-3 3-phase back-EMF voltage sensing for BLDC six-step (trapezoidal) sensorless motor control

Place DEVKIT-MOTORGD jumpers J9, J10 and J11 into position 1-2 for PMSM application or 2-3 for BLDC application. Jumper J8 stays open for 5 V HALL sensors.

Figure 23. J9-11 PMSM

Figure 23. J9-11 PMSM

Figure 24. J9-11 BLDC

Figure 24. J9-11 BLDC

Make sure that the potentiometer for overcurrent comparator is set in the correct position (approximately 8 - 10 A, slightly to the left from the middle).

Figure 25. Overcurrent Potentiometer

Figure 25. Overcurrent Potentiometer

3.3 Connect the Motor

Ensure that the motor phase wires are in the following order, from phase A to phase C:

A: Yellow

B: Green

C: Blue

Figure 26. Motor Phases

Figure 26. Motor Phases

3.4 Connect the Power Supply

Switch SW1 to the OFF position (fully to the left).

Figure 27. OFF

Figure 27. OFF

Connect the 12 V power supply adapter.

Figure 28. Plug Power

Figure 28. Plug Power

Switch SW1 to the ON position (fully to the right).

Figure 29. ON

Figure 29. ON

When power is applied to the EVB, four orange LEDs next to the voltage regulators indicate that the 12 V, 5 V, 3.3 V and 1.5 V supply voltages are present.

3.5 Connect the Debug Interface

Connect a micro-USB cable to the J40 connector to debug via the onboard S32K3 debugger.

Figure 30. USB cable

Figure 30. USB cable

4. Build the Application Project

Let's take your MCSTE1AK344 motor control kit for a test drive.

4.1 Select Application and MCU Programming

Select the appropriate PMSM or BLDC motor control application from the installed directory NXP\MC_DevKits\MCSPTE1AK344\sw.

To import the installed application software project in the S32 Design Studio IDE for S32 Platform:

  1. Launch S32DS for S32 Platform
  2. Go to File → Import then select General rarr; Existing Projects into Workspace
  3. Figure 31. Import Project

    Figure 31. Import Project
  4. Find the installed application directory: NXP\MC_DevKits\MCSPTE1AK344\sw and choose the corresponding project and click "OK". Then, click "Finish"

Figure 32. MCSPTE1AK344 Projects

Figure 32. MCSPTE1AK344 Projects

Figure 33. SW Project Nomenclature

Figure 33. SW Project Nomenclature

4.2 Use Configuration Tool

If you selected a project with low-level drivers (ll in project name), follow these steps:

  1. Expand the imported project folder in S32 Design Studio, such as MCSPTE1AK344_PMSM_FOC_2Sh_ll. Then, double-click the corresponding *.mex file to open the project configuration in the Configuration Tool
  2. Figure 34. MEX file

    Figure 34. MEX file
  3. After confirming that you configured the correct project, click "Update Code" button for generating configuration files
  4. Figure 35. Update Code

    Figure 35. Update Code

If you selected a project with AUTOSAR drivers (with as_tr in the project name), the S32DS project will contain a tresos folder with EB tresos configuration. Follow the following steps.

  1. Open EB tresos Studio and import the appropriate subfolder
  2. Figure 36. Import AUTOSAR tresos Project

    Figure 36. Import AUTOSAR tresos Project
  3. In EB tresos Studio, double-click on ECU (CORTEXM, S32K3XX) and generate the project (Menu → Project → Generate Project)

4.3 Upload Software and Debug

To upload the SW and debug, follow the following steps.

  1. In S32DS, return back to the C/C++ perspective
  2. Figure 37. C_Cpp perspective

    Figure 37. C_Cpp Perspective
  3. Go to the Debug Configuration menu and select the predefined debug configuration for building and uploading software onto the MCU
  4. Figure 38. Debug Menu

    Figure 38. Debug Menu

    Figure 39. Debug Configuration

    Figure 39. Debug Configuration
  5. The S32DS will switch into debug perspective. Click Resume or press F8 to run the code. Then, click Disconnect to avoid interference between the S32 Design Studio debugger and the FreeMASTER tool

Figure 40. Let Code Run

Figure 40. Let Code Run

Figure 41. Disconnect

Figure 41. Disconnect

4.4 Set Up the Debugging Tool

Launch the FreeMASTER application to set up the debugging tool. To open the FreeMASTER project, select File → Open Project, then browse to the FreeMASTER_control folder in the selected project directory and open the *.pmpx file.

Figure 42. FreeMASTER Project

Figure 42. FreeMASTER Project

To enable communication, access the FreeMASTER toolbar and click Go (or press Ctrl+G). You will know that communication has been successfully activated when you see the following at the bottom of the status bar:

RS-232; port=COMn; speed = 115200

Figure 43. FreeMASTER Start

Figure 43. FreeMASTER Start

Application Control

Application Setup (optional step)

If you run the MCSPTE1AK344 software on modified or custom hardware, you may need to edit hardware scales and fault triggers in the Motor Control Application Tuning (MCAT) tool.

Open the Application Setup page and edit the values on the left side of the page.

Figure 44. Application Setup

Figure 44. Application Setup

Once you finish, click "Save config" to generate a static configuration file. You may check file content at the "Output file" page.

Next, repeat the step from the Upload Software and Debug section to build the project and upload the code into MCU.

Motor parametrization and control loops autotuning (optional step)

In a case of motor change, you may benefit from new MCAT 2.0 motor parametrization and control loops autotuning features.

On the Motor Parameters page, enter the four basic motor parameters that cannot be detected automatically:

  • Number of pole pairs
  • Nominal Current
  • Nominal Speed
  • Maximum Speed

Click "Update Target" to start motor-parameter estimation and automatic control-loop tuning. The parameters are typically updated automatically in less than one minute.

Figure 45. Automated Motor Parametrization and Tuning

Figure 45. Automated Motor Parametrization and Tuning

Run the Motor

Open the "Speed Loop" page, then use the "Speed Control" tab to set the required speed and turn on the motor drive.

Figure 46. Speed Control

Figure 46. Speed Control

Select one of the predefined Scopes or Recorders in Project Tree to watch the application variables in real time.

For runtime debugging, you can create or modify scopes and recorders as needed.

Figure 47. Speed Scope

Figure 47. Speed Scope

Check Pending Faults

If there are pending faults and the red LED indicates a fault state, click "CLEAR" on the MCAT Control tab. You can also press SW5 and SW6 simultaneously on the board.

Figure 48. Pending Fault

Figure 48. Pending Fault

Start Application

Click "On/Off" on the control bar, or press SW5 or SW6 on the board, to start clockwise or counterclockwise rotor rotation. The blue LED indicates the running state.

Set Speed

Modify the "Required Speed" field on the control bar, or change the "Speed Required" value in the Variable Watch window. You can also control the speed by pressing SW5 or SW6 on the board.

Figure 49. Speed Modification

Figure 49. Speed Modification

Stop Application

Stop the motor by clicking "On/Off" on the MCAT control page, clearing the On/Off variable, or pressing and holding SW5 and SW6 on the S32K344EVB board. The green LED indicates the ready state.