1
Get Started2
Board features3
Configure the hardware4
Installing SPIGen on your computer5
Learn MoreSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through learning about how to set up the FRDMGD3100HBIEVM board.
The FRDMGD3100HBIEVM contents include:
Something went wrong! Please try again.
Something went wrong! Please try again.
The kit requires the following to function properly with the software:
Something went wrong! Please try again.
Refer to FRDMGD3100HBIEVM, Half-bridge evaluation board - User Guide for additional details.
Something went wrong! Please try again.
The FRDMGD3100HBIEVM is a half-bridge evaluation board populated with two GD3100 single-channel IGBT gate drive devices. The board supports connection to a FRDM-KL25Z microcontroller for SPI communication and programming, through the use of a logic translator board.
The evaluation board is designed to connect to a single phase of an Infineon HybridPACK™ Drive IGBT for evaluation of the GD3100 performance and capabilities driving a power device. The board includes DESAT circuitry for short-circuit detection and implementation of GD3100 IGBT shutdown protection capabilities.
Something went wrong! Please try again.
The FRDMGD3100HBIEVM consists of 3 boards as shown in the final assembly below.
Overview of the FRDMGD3100HBIEVM evaluation board
Something went wrong! Please try again.
The Freedom KL25Z is an ultra-low-cost development platform for Kinetis® L Series MCU built on Arm® Cortex®-M0+ processor.
Something went wrong! Please try again.
The FRDMGD3100HBIEVM includes a logic translator board, which provides simple isolation and is capable of level-shifting communication signals between the MCU and the GD3100 driver board. The driver board is exposed to high voltage and may require 3.3 V or 5.0 V logic, necessitating an interface board.
Something went wrong! Please try again.
Jumper, LED and additional board descriptions and images are available in the FRDMGD3100HBIEVM, Half-bridge evaluation board - User Guide user manual.
Something went wrong! Please try again.
FRDMGD3100HBIEVM is connected to any phase of an Infineon Hybrid PACK Drive module with SBE DC Link capacitor as shown in Figure 12. Double pulse and short-circuit testing can be conducted utilizing Windows-based PC with SPIGEN software.
Suggested equipment’s needed for testing:
Connect the micro-B end of the supplied USB cable into FRDM-GD3100EVM half-bridge evaluation board. Connect the other end of the cable to a host computer.
Something went wrong! Please try again.
Follow the step by step instructions to perform a basic double pulse test using SPIGEN with the FRDMGD3100HBIEVM board.
Something went wrong! Please try again.
Detailed configuration and images are available in the FRDMGD3100HBIEVM, Half-bridge evaluation board - User Guide.
Something went wrong! Please try again.
Software for FRDMGD3100HBIEVM is distributed with the SPIGen GUI tool (available on NXP.com). Necessary firmware comes pre-installed on the FRDM-KL25Z with the kit.
The latest version of SPIGen supports the GD3100 and is designed to run on any Windows 10, Windows 8, or Windows 7-based operating system. To install the software, do the following:
For additional information on microcode and FRDM-KL25Z configuration, refer to the user guide.
Something went wrong! Please try again.
In this video you will learn how to use the SPIGen software tool to configure and control the GD3100 evaluation board.
Something went wrong! Please try again.
The SPIGen graphical user interface is available from NXP.com as an evaluation tool demonstrating GD3100-specific functionality, configuration, and fault reporting. SPIGen also includes basic capacity for the FRDMGD3100HBIEVM to control an IGBT, enabling double-pulse or short-circuit testing.
Something went wrong! Please try again.
Something went wrong! Please try again.
Now start embedded application development.
The product summary page for GD3100 is located at http://www.nxp.com/GD3100.
Something went wrong! Please try again.
The overview section provides a description of the device, product features, a list of the kit contents, a list of (and links to) supported devices, list of (and links to) any related products and a Get Started section.
After downloading files, review each file, including the user guide which includes setup instructions.
Something went wrong! Please try again.
In addition to our GD3100: Advanced single-channel gate driver for Insulated Gate Bipolar Transistors (IGBTs) page you may also want to visit:
Something went wrong! Please try again.
FRDMGD3100HBIEVM, Half-bridge evaluation board.
Buy OptionsSomething went wrong! Please try again.
Board descriptions
Board Image
Kinetis KL25Z freedom board
Logic translator board
Additional board support
Evaluation board and system setup
Getting started with the FRDMGD3100HBIEVM board
Additional board support