Technical content and expertise to help jump start your design and get you to production faster.
Start your designDownload our latest development and embedded software solutions.
Expedite time-to-market with our extensive lineup of development kits.
Jump-start your design with proven hardware and software solutions.
Get the latest specifications in our technical documentation library.
Further your technical expertise with online and in-person instruction.
Get comprehensive paid support to fast-track your product development.
Design ideas, demo videos, quality answers. Connect with NXP professionals and other knowledgeable designers ready to help.
Software, documentation, evaluation tools. The resources to build comprehensive solutions and accelerate your time to market.
Access our design resource libraryWe're always looking for passionate and talented people to work with us.
Join our teamLet's take your MPC-LS-VNP-RDB for a test drive!
WARNING: The MPC-LS-VNP-RDB enclosure provides thermal management. Do not run the RDB with the enclosure open without proper cooling. Refer to the MPC-LS-VNP-RDB User Manual for cooling recommendations.
Execute the file and proceed with the default configurations that the installation wizard recommends.
Scroll down and click Documents. In the Software section, click “MCP2200/MCP2221 Windows Driver & Installer”.
Connect the power supply to the power jack of the MPC-LS-VNP-RDB board and the micro-B USB cable to the LS1043A USB3 console port. Make sure that the power status LED is glowing green on the board.
Select the COM port to which the USB3 console port is connected and click OK. Go to Setup > Serial Port and select 115200 as the baud rate. If no COM port is detected automatically, make sure that the MCP2221A driver is downloaded and installed correctly.
Press the reset button on the chassis back panel to reboot the board. The boot log appears in the console window.
After the boot completes, you will be prompted for a TinyDistro Login. Type “root” and then press enter. The getting started IPCF (InterPlatform Communications Framework) application is automatically executed on login.
Connect the power supply to the power jack of the MPC-LS-VNP-RDB board and the micro-B USB cable to the MPC5748G USB4 console port. Make sure that the power status LED is glowing green on the board.
Select the COM port to which the USB4 console port is connected and click OK. Go to Setup > Serial Port and select 115200 as the baud rate. If no COM port is detected automatically, make sure that the MCP2221A driver is downloaded and installed correctly.
Press the reset button on the chassis back panel to reboot the board. The boot log appears in the console window.
The getting started IPCF (InterPlatform Communications Framework) application is automatically executed on login.