Getting Started with FRDM-IMX93

Last Modified: 2024-11-29 11:56:00Supports FRDM i.MX 93 Development Platform

1. Out of the Box

The following section describes the steps to boot the FRDM-IMX93.

Development kit contains:

  • FRDM-IMX93 board with on-board u-blox MAYA-W27x with NXP’s Wi-Fi 6 Tri-radio IW612
  • Cable: Assembly, USB 2.0, Type-C male to Type-A male
  • Software: Linux BSP image Programmed in eMMC
  • Quick Start Guide

Get started developing your application on the FRDM-IMX93 with the out-of-the-box video. For more information please visit the i.MX 93 applications processor documentation.

1.1 Get Familiar With the Board

FRDM IMX93 Front

FRDM IMX93 Front

FRDM IMX93 Back

FRDM IMX93 Back

1.2 Boot from eMMC

The FRDM-IMX93 comes with a pre-built NXP Linux binary demo image flashed on the eMMC. Without modifying the binary inside, booting from the eMMC provides a default system with certain features for building other applications on top of Linux.

To understand more about NXP’s Embedded Linux®, continue reading the next sections.

1.3 Connect USB Debug Cable

Connect the supplied USB Type-C cable to the debug UART port P16, then connect the other end of the cable to a host computer.

Two UART connections will appear on the host computer. The first port is for Cortex-A55 core, and the second port is for Cortex-M33 core system debugging.

If you are unfamiliar with terminal applications, please view one of the following tutorials before continuing to step 1.4: Debug Terminal in Linux, Debug Terminal in Windows.

To debug under Linux, make sure CH342F Linux driver  is installed.

1.4 Connect the HDMI Cable

To experience the user interface provided with the image binary, connect a monitor via the HDMI connector P5.

1.5 Boot Switch Setup

See the next table to configure accordingly.

GS-FRDM-IMX93-IMG4

1.6 Connect Power Supply

Connect the power supply cable to the power connector P1.

The board has been set up to boot from eMMC by default. The processor starts executing the bootable image from eMMC. Then, the U-Boot execution should begin automatically.

Information is printed in the serial console for the Arm® Cortex®-A55. If you do not stop the U-Boot process, it continues to boot the kernel.

As the board boots up, you will see 2 penguins appear in the upper left-hand corner of the monitor, and then you will see the Linux terminal icon on the top left and timer on right top corner.

Congratulations, you are up and running.

1.7 Load Wi-Fi, Bluetooth and 802.15.4 Driver Modules

To login into the FRDM-IMX93, use “root” as the default login username for the i.MX Linux OS. There is no password. Use below command to load Wi-Fi and Bluetooth modules in the kernel.

root@imx93frdm:~# modprobe moal mod_para=nxp/wifi_mod_para.conf
root@imx93frdm:~# ifconfig mlan0 up
root@imx93frdm:~# modprobe btnxpuart
root@imx93frdm:~# hciconfig hci0 reset 

For more information on please visit FRDM-IMX93 Connectivity Training .

2. Get Software

The i.MX Linux Board Support Package (BSP) is a collection of binary files, source code and support files that are used to boot an Embedded Linux image on a specific i.MX development platform.

Current releases of Linux binary demo files can be found on FRDM i.MX 93 Development Board. Additional documentation is available in the i.MX Linux documentation bundle under the Linux sections of the i.MX Software and Development Tools.

2.1 Overview

FRDM-IMX93 support booting from eMMC and SD card.

This Getting Started guide only outlines a few methods of flashing the Linux BSP image to an SD card. Experienced Linux developers can explore other options if desired.

2.2 Download NXP Linux BSP Pre-Built Image

The latest pre-built images for the FRDM-IMX93 are available on the FRDM i.MX 93 Development Board.

The pre-built NXP Linux binary demo image provides a typical system and basic set of features for using and evaluating the processor. Without modifying the system, the users can evaluate hardware interfaces, test SoC features and run user space applications.

2.3 Burn NXP Linux BSP Image Using Universal Update Utility (UUU)

In addition to the connections from "Out of the Box" section, connect the USB1 (P2) to the host machine using the proper USB cable.

Unplug the power adapter. Refer to the "1.5 Boot Switch Setup" section and configure the board to boot on serial download protocol (SDP) mode.

Depending on the OS used in the host machine, the way to transfer the Linux BSP image onto an SD card can vary. Choose an option below for detailed instructions:

2.4 Optional: Use Common Torizon for a Simplified Linux Experience

Torizon is an easy-to-use industrial Linux platform, that simplifies the development and maintenance of Linux devices. Your FRDM-IMX93 is supported by the operating system Common Torizon: an open source minimal Embedded Linux image featuring, among other essential services, an optimal container runtime and components for secure offline and remote over-the-air (OTA) updates, device monitoring and remote access.

Download the Common Torizon binary  image.

Build Common Torizon from source using Yocto . You can download the Yocto layers, perform the build setup and start the build process.

Flash Common Torizon on FRDM-IMX93, please refer to the specific flashing steps .

After flashing, you will be able to log in via the terminal using the following credentials:

  • User: torizon
  • Password: torizon

After this, it is required that you create a password.

To evaluate some demo applications, you will be able to use Torizon Cloud . For this, you will need to create a Torizon Cloud account and provision your device to your account.

To learn how simple it is to do this, please check the next section.

2.5 Optional: Getting Started with Torizon Cloud

After successfully flashing Common Torizon on FRDM-iMX93, it is possible to start using Torizon Cloud, which allows for secure remote online and offline updates for both the OS and the applications, remote device monitoring, remote access, fleet management, and vulnerabilities monitoring, among other features.

To know more about Torizon , please refer to the Torizon documentation .

To start using Torizon Cloud, it is necessary to create an account  and add your FRDM-IMX93 with Common Torizon to your account.

Follow the step-by-step guide .

If you have questions about Torizon, feel free to reach out via the toradex community .

3. Build and Run

In the section, a brief guide of how to build Yocto BSP image for FRDM-IMX93 is introduced, along with how to add Matter support and how to build Debian release image

3.1 FRDM-IMX93 Yocto BSP

The FRDM-IMX93 BSP release is based on i.MX SW 2024 Q3 release with Yocto Project 5.0 (Scarthgap). To build FRDM-IMX93 image from source code, please first check i.MX Yocto Project User's Guide to get familiar with Yocto project and Yocto build. Then please follow below steps to build image for FRDM-IMX93.

  1. Download i.MX SW 2024 Q3 BSP Release:
  2. $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml 
    $ repo sync 
  3. Integrate FRDM-MX93 layer into Yocto code base:
    $ cd ${MY_YOCTO}/sources
    $ git clone https://github.com/nxp-imx-support/meta-imx-frdm.git
  4. Yocto Project Setup:
    $ MACHINE=imx93frdm DISTRO=fsl-imx-xwayland source sources/meta-imx-frdm/tools/imx-frdm-setup.sh -b frdm-imx93
  5. Build images:
    $ bitbake imx-image-full
  6. Flashing SD card image:
    $ zstdcat imx-image-full-imx93frdm.rootfs.wic.zst | sudo dd of=/dev/sdx bs=1M && sync

    Or using uuu to burn image into SD card:

    $ uuu -b sd_all imx-image-full-imx93frdm.rootfs.wic.zst
  7. Change boot switch SW1 to “0011” to select SD card boot, insert the SD card and power up the FRDM-IMX93 board.

3.2 FRDM-IMX93 Matter Support

FRDM-IMX93 has support for Matter. To include Matter support, please follow below steps to include Matter layer into Yocto build.

  1. Download i.MX SW 2024 Q3 BSP Release:
  2. $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml
    $ repo sync 
  3. Download i.MX Matter Yocto layer:
    $ cd ${MY_YOCTO}/sources/meta-nxp-connectivity
    $ git remote update
    $ git checkout imx_matter_2024_q3
  4. Integrate FRDM-MX93 layer into Yocto code base:
    $ cd ${MY_YOCTO}/sources
    $ git clone https://github.com/nxp-imx-support/meta-imx-frdm.git
  5. Yocto Project Setup:
    $ MACHINE=imx93frdm-iwxxx-matter DISTRO=fsl-imx-xwayland source sources/meta-imx-frdm/tools/imx-frdm-matter-setup.sh bld-xwayland-imx93
  6. Build images:
  7. $ bitbake imx-image-multimedia

3.3 FRDM-IMX93 Debian

FRDM-IMX93 has support for Debian 12 OS. i.MX Debian Linux SDK distribution is a combination of NXP-provided kernel and boot loaders with a Debian distro user-space image, which includes:

  • Debian-based rootfs
    1. Debian Base (basic packages)
    2. Debian Server (more packages without GUI Desktop)
    3. Debian Desktop (with GNOME GUI Desktop)
  • Linux kernel
  • BSP components
  • various applications (graphics, multimedia, networking, connectivity, security, and AI/ML)

For more details of NXP Debian Linux SDK Distribution, please check NXP Debian Linux SDK Distribution for i.MX and Layerscape.

Quick Start with Debian

To create an SD card with Debian for FRDM-IMX93, please follow below steps.

  1. Download flex-installer on the Linux host
  2. $ wget http://www.nxp.com/lgfiles/sdk/lsdk2412/flex-installer
    $ chmod +x flex-installer
    $ sudo mv flex-installer /usr/bin
  3. Plug the SD card into the Linux host and install the images as below
  4. # format SD card
    $ flex-installer -i pf -d /dev/sdb
    # automatically download and install images into SD card
    $ flex-installer -i auto -d /dev/mmcblk1 -m imx93frdm
  5. Plug the SD card into the FRDM-IMX93 board and install the extra packages as below
    1. setup Ethernet network interface by DHCP or setting it manually
    2. $ dhclient -i end0
    3. Set correct system time, for example
    4. $ date -s "22 Nov 2024 09:00:00"
    5. Install extra packages for GNOME GUI Desktop version
    6. $ debian-post-install-pkg desktop
    7. Or install extra packages for Server version without GUI Desktop
    8. $ debian-post-install-pkg server
    9. After finishing the installation, run the reboot command to boot up the Debian Desktop/Server system

Building Debian Images with Flexbuild

To build Debian image with Flexbuild for FRDM-IMX93, please follow below steps.

  1. Set up the build environment
    $ git clone https://github.com/nxp/flexbuild
    $ cd flexbuild && source setup.env
    #Continue to run commands below in case you need to build in Docker due to lack of Ubuntu 22.04 or Debian 12 host
    $ bld docker
    $ source setup.env
  2. Build image with Flexbuild
    $ bld -m imx93frdm
  3. Flexbuild usage:

    To build individual part of the image, please check below command list for Flexbuild usage

    $ bld uboot -m imx93frdm (compile u-boot image for imx93frdm)
    $ bld linux (compile linux kernel for all arm64 i.MX machines)
    $ bld bsp -m imx93frdm (generate BSP firmware)
    $ bld boot (generate boot partition tarball including kernel, dtb, modules, distro bootscript for iMX machines)
    $ bld multimedia (build multimedia components for i.MX platforms)
    $ bld rfs -r debian:server (generate Debian server rootfs)
    $ bld apps -r debian:server (compile apps against runtime dependencies of Debian server RootFS)
    $ bld merge-apps -r debian:server (merge iMX-specific apps into target Debian server RootFS)
    $ bld packrfs -r debian:server (pack and compress target debian server rootfs)

4. Developer Experience

To enable faster development for users of all skill levels, FRDM-IMX93 provides extensive example applications to showcase various features and capabilities of the FRDM-IMX93, especially on machine learning related use case accelerated by Neural-network Processing Unit (NPU) available in FRDM-IMX93.

Currently 9 example applications are available on FRDM-IMX93:

  • Image Classification
  • Object Detection
  • Selfie Segmenter
  • i.MX Smart Fitness
  • DMS (Driver Monitor System)
  • ML Benchmark Tool
  • Video Test Tool
  • i.MX Smart Kitchen
  • i.MX E-Bike VIT

The details of supported example applications are available in Application Code Hub (ACH) and GoPoint.

4.1 Application Code Hub

The Application Code Hub (ACH) repository enables engineers to easily find microcontroller and processor software examples, code snippets, application software packs and demos developed by NXP in-house experts. This space provides a quick, easy and consistent way to find microcontroller and processor applications.

ACH provides filter and search options to quickly find specific applications. With the support of Git capabilities, there is an easy way to import and use applications within user’s development environments.

To learn more details of Application Code Hub (ACH), please visit this link .

To find available example applications for FRDM-IMX93, please select “i.MX” in Device Families as shown below.

GS-FRDM-IMX93-IMG5

Select each example application to check for details.

GS-FRDM-IMX93-IMG6

To get the source code of each example application, click the “Visit on GitHub” button on the top to visit the code repository in NXP GitHub.

GS-FRDM-IMX93-IMG7

4.2 GoPoint for i.MX Applications Processors

The GoPoint for i.MX Application Processors is a user-friendly application launches pre-built applications packed with the Linux BSP, giving users an excellent out-of-the-box experience and hands-on experience with i.MX SoC's capabilities. GoPoint highlights advanced features while providing practical solutions for implementation, with source code and build recipes for the applications provided in GitHub .

To learn more details of GoPoint, please visit this link.

For FRDM-IMX93, GoPoint is included in the BSP release by default. To open the GoPoint GUI launcher, press the NXP logo displayed on the top left-hand corner of the screen after the FRDM-IMX93 boot up as shown below.

GS-FRDM-IMX93-IMG8

Available example applications are shown with icons of screenshot for each application. When selecting the example application, a brief description of this example application is shown on the right side. To launch the currently selected application, click the “Launch Demo” button. After an application is started, it can then be force-quit by clicking the “Stop Current Demo” button in the launcher (appears once the application is started).

For more details of the usage for each application, please refer to GoPoint for i.MX Applications Processors User's Guide.

GS-FRDM-IMX93-IMG9

Debug Terminal in Linux

Serial Communication Console Setup

The serial-to-USB drivers are available at CH342F Linux Drivers .

On the command prompt of the Linux host machine, run the following command to determine the port number:

ls /dev/ttyCH343USB*

The first number is for Arm® Cortex®-A55.

Minicom

Use the following commands to install and run the Minicom program:

  1. Install Minicom using Ubuntu package manager
  2. sudo apt-get install minicom
  3. Launch Minicom using a console window using the port number determined earlier
  4. sudo minicom /dev/ttyCH343USB * -s
GS-FRDM-IMX93-IMG3

Configure Minicom as show in Figure and Exit configure.

Debug Terminal in Windows

Serial Communication Console Setup

The WCH USB-serial chip on FRDM-IMX93 enumerates 2 serial ports. Assume that the ports are COM11,COM12. The first Port(COM11) is for the serial console communication from Arm® Cortex®-A55. The serial-to-USB drivers are available at CH342F Windows Driver .

Tera Term

Tera Term is an open source terminal emulation application. This program displays the information sent from the NXP development platform’s virtual serial port.

  1. Download Tera Term. After the download, run the installer and then return to this webpage to continue
  2. Launch TeraTerm. The first time it launches, it shows the following dialog. Select the Serial option. Assuming your board is plugged in, there should be a COM port automatically populated in the list
  3. Configure the serial port settings (using the COM port number identified earlier) to 115,200 baud rate, 8 data bits, no parity and 1 stop bit. To do this, go to Setup → Serial Port and change the settings
  4. Verify that the connection is open

PuTTY

PuTTY is a popular terminal-emulation application. This program displays the information sent from the NXP development platform's virtual serial port.

  1. Download PuTTY. After the download, run the installer and then return to this webpage to continue
  2. Launch PuTTY by either double clicking on the executable file you downloaded or from the Start menu, depending on the type of download you selected
  3. Configure In the window that launches. Select the Serial radio button and enter the COM port number that you determined earlier. Also enter the baud rate, in this case 115,200
  4. Click Open to open the serial connection. Assuming the board is connected, and you entered the correct COM port, the terminal window opens. If the configuration is not correct, PuTTY alerts you

Cortex M-33 Enablement

FRDM-IMX93 has one general-purpose Arm® Cortex®-M33 running up to 250 MHz, which can be used for real-time and low-power processing. In this section, developers can learn how to build program, run program and debug program for Cortex-M33 core.

Download SDK

The Cortex-M33 MCUXpresso SDK is distributed by the MCUXpresso Web Builder tool . The MCUXpresso SDK includes a flexible set of peripheral drivers designed to speed up and simplify development of embedded applications. Along with the peripheral drivers, the MCUXpresso SDK provides an extensive and rich set of example applications covering everything from basic peripheral use case examples to demo applications. The MCUXpresso SDK also contains optional RTOS integrations such as FreeRTOS and Azure RTOS, and device stack to support rapid development on devices.

To obtain the MCUXpresso SDK for FRDM-IMX93, please follow below steps.

  1. Visit MCUXpresso SDK Builder
  2. Click the “Select Development Board”
  3. GS-FRDM-IMX93-IMG11
  4. Search for “MIMX9352xxxxM” and select it
  5. GS-FRDM-IMX93-IMG12
  6. Choose the SDK release version 2.16 and press the “BUILD SDK” button
  7. GS-FRDM-IMX93-IMG13
  8. Choose the Host OS, Toolchain and middleware to be included in the SDK, then press the “BUILD SDK” button
  9. GS-FRDM-IMX93-IMG14
  10. After the SDK finish building, click “Download” in the Dashboard page
  11. GS-FRDM-IMX93-IMG15
  12. Download the SDK with documentation
  13. GS-FRDM-IMX93-IMG16
  14. After the SDK package is downloaded, unpack the package. Please check the release note and “Getting Started with MCUXpresso SDK for MCIMX93-EVK.pdf” document in the docs folder to learn more about Cortex-M33 MCUXpresso SDK

Build Cortex-M33 Program

Please refer to “Getting Started with MCUXpresso SDK for MCIMX93-EVK.pdf” document in the docs folder in the SDK package to learn how to setup toolchain and build cortex-M33 program.

Run Cortex-M33 Program

There are two methods to run compiled program on Cortex-M33: U-Boot bootaux and Linux remoteproc. After using bootaux or remoteproc to start the Cortex-M33 core, using remoteproc to stop the Cortex-M33 core is for debug purposes only. It is not recommended to stop the Cortex-M33 core from Linux OS in a production system.

Before starting the Cortex-M33 core, make sure the debug UART port of Cortex-M33 core is opened in the debug terminal.

  1. Using bootaux in U-Boot

    In this example, Cortex-M33 program is first loaded from SD card's partition 1 in U-Boot. Then Cortex-M33 core is booted by bootaux command. Finally, the Linux is booted on Cortex-A55 core by boot command. Please make sure the Cortex-M33 program binary is stored in the SD card's partition 1 with fat partition format. In this example, the binary file “imx93-11x11-evk_m33_TCM_power_mode_switch.bin” is used as an example.

    After the board is powered up, press any key in the Cortex-A55's debug terminal to enter U-Boot. Then use following command to start Cortex-M33 core.

    u-boot=> fatload mmc 1:1 ${loadaddr} imx93-11x11-evk_m33_TCM_power_mode_switch.bin
    19080 bytes read in 6 ms (3 MiB/s)
    u-boot=> cp.b ${loadaddr} 0x201e0000 ${filesize}
    u-boot=> bootaux 0x1ffe0000 0
    ## Starting auxiliary core addr = 0x1FFE0000...
    u-boot=> setenv mmcargs 'setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=${mmcroot} clk_ignore_unused'
    u-boot=> run prepare_mcore
    u-boot=> boot

    If the Cortex-M33 core boots successfully with this binary file, following log should be printed in the Cortex-M33 debug terminal:

    GS-FRDM-IMX93-IMG17
  2. Using remoteproc in Linux

    In this example, Cortex-M33 program is loaded from Linux's rootfs, and boots with remoteproc. The binary file “imx93-11x11-evk_m33_TCM_power_mode_switch.elf” is used here as an example.

    u-boot=> run prepare_mcore 
    u-boot=> boot 

    After Linux boots up, use following command in the Cortex-A55’s debug terminal to start Cortex-M33 core.

    root@imx93frdm:~# echo /lib/firmware/imx93-11x11-evk_m33_TCM_power_mode_switch.elf > /sys/class/remoteproc/remoteproc0/firmware
    root@imx93frdm:~# echo start > /sys/class/remoteproc/remoteproc0/state

    If the Cortex-M33 core boots successfully with this binary file, following log should be printed in the Cortex-M33 debug terminal.

    GS-FRDM-IMX93-IMG17

How to Debug

Please refer to application note AN14120 “Debugging Cortex-M with VS Code on i.MX 8M, i.MX 8ULP, and i.MX 93”.

Deploy ML models on NPU

Deploy ML models on NPU

FRDM-IMX93 has an Ethos-U65 NPU to accelerate neural-network machine learning inference. It runs at 1 GHz and provides 0.5 Tops computation power (256 MAC/cycle). For more details of the HW and SW architecture of Ethos-U65, please check i.MX Machine Learning User's Guide.

Model Quantization

To be accelerated by the Ethos-U65 NPU, the neural-network operators must be quantized to either 8-bit (unsigned or signed) or 16-bit (signed). For model quantization, please download latest eIQ toolkit and check the user guide.

Vela Compiling

To deploy the quantized neural network (NN) model on Ethos-U65, the first step is to use Vela to compile the prepared model. The Vela tool is used to compile a TensorFlow Lite NN model into an optimized version that can run on an embedded system containing an Arm Ethos-U NPU. The optimized model contains TFLite Custom operators for those parts of the model that can be accelerated by the Ethos-U NPU. Parts of the model that cannot be accelerated are left unchanged and run on CPU (Cortex-A or Cortex-M) using an appropriate kernel. After compilation, the optimized model can only be run on an Ethos-U NPU embedded system. The tool also generates performance estimates for the compiled model.

FRDM-IMX93 supports on target Vela compilation and offline Vela compilation. For on target Vela compilation, the Vela compiler is already installed in the Linux BSP by default. Developers can directly use following command on FRDM-IMX93 with Linux BSP to do on target vela compilation.

root@imx93frdm:~# vela YOUR_MODEL_NAME.tflite 

If running successfully, the vela compiled model YOUR_MODEL_NAME_vela.tflite is generated in the output folder.

For offline Vela compilation, please download latest eIQ toolkit and check the user guide.

Model Inference

To evaluate Vela compiled model’s performance on NPU, the simplest method is to use the benchmark_model tool in Linux BSP. It uses random data as input and gives average inference time for a given number of runs. Here is an example:

root@imx93frdm:~# /usr/bin/tensorflow-lite-2.16.2/examples/benchmark_model --graph=/root/mobilenet_v1_1.0_224_quant_vela.tflite --external_delegate_path=/usr/lib/libethosu_delegate.so 

If running successfully, the following log is printed in the debug terminal.

GS-FRDM-IMX93-IMG18

The benchmark_model tool can also provide operator profiling report by setting --enable_op_profiling=true in the command. For more usage of benchmark_model, please use --help to check.

For how to write code in c++ and python to run model inference on NPU, please refer to example applications in GoPoint.

Deploy PyTorch Model

Besides Tensorflow, PyTorch is also a popular deep learning frameworks to build NN models. But the Vela tool only support compilation for TensorFlow Lite NN models. For how to convert PyTorch models into TensorFlow Lite models, please check application note AN13769 “Deploy PyTorch Models to NXP Supported Inference Engines Using ONNX”.

Graphics

Graphics

FRDM-IMX93 has a Pixel Processing Pipeline (PXP) module that can be used to process graphics buffers or composite video and graphics data before sending to an LCD display or TV encoder. It is used to minimize the memory footprint required for the display pipeline and provide an area and performance optimized to both SDRAM-less and SRAM-based systems. The PXP combines scaling, color space conversion and rotation processing into a single processing engine.

For more details of PXP and how to use it, please check application note AN13829“How to Use PXP in GStreamer and Wayland”.

Security and Integrity

Security and Integrity

System security and integrity is always one of the most critical aspects to be considered in product development.

FRDM-IMX93 support secure boot feature and encrypted boot feature, helping to prevent unauthorized software execution during the device boot sequence and protect bootloader data from unauthorized access.

For more details of secure boot feature, please check application note AN12312 “Secure Boot on AHAB Supported Devices”.

For more details of encrypted boot feature, please check application note AN13994 “i.MX Encrypted Boot on AHAB-Enabled Devices”.

Fast Boot

Fast Boot

In certain use cases, there is requirement for the device boot time, which means the device needs to complete booting in a given time limit.

To optimize the boot time, FRDM-IMX93 supports falcon mode in U-Boot. Falcon mode is a feature in U-Boot that enables fast booting by allowing SPL to directly start the Linux kernel. It completely skips the U-Boot loading and initialization, with the effect of reducing the time spent in the bootloader.

For how to enable falcon mode and further optimize boot time, please check AN14093 “Fast Boot on i.MX 8M and i.MX 9 Using Falcon Mode and Kernel Optimizations”.