1
Plug It In2
Get Software3
Build, RunSign in to save your progress. Don't have an account? Create one.

Let's take your QN9090 board for a test drive, you have the choice of watching the sequence in a short video or following the detailed actions list below.
Something went wrong! Please try again.
Something went wrong! Please try again.
MCUXpresso SDK for the QN9090 integrates the MCUXpresso Software Development Kit with all the wireless connectivity stacks required to develop your solution with Bluetooth Low Energy.
Click below to download a pre-configured SDK release for the QN9090 that includes the wireless connectivity Bluetooth Low Energy stack for the QN9090.
Something went wrong! Please try again.
NXP offers a complimentary toolchain called MCUXpresso IDE.
No problem The MCUXpresso SDK includes support for other tools such as IAR .
Something went wrong! Please try again.
The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and also provides pin and clock tools to generate initialization C code for custom board support. This tool is integrated into MCUXpresso IDE, but if you are using a different IDE, you can download this tool below.
Something went wrong! Please try again.
Drivers for the debugger and virtual COM port also need to be installed. Ensure the QN9080DK board is connected to your computer, and then go to the drivers folder in the MCUXpresso IDE install directory (C:\NXP\MCUXpressoIDE_11.1.0_3209\Drivers
by default) double click on lpc_driver_installer.exe to install the drivers. Alternatively they are part of the LPCScrypt package, which can be download below.
Something went wrong! Please try again.
Configure your preferred terminal to 115200 baud rate, 8 data bits, no parity and 1 stop bit. To determine the port number of the QN9090’s virtual COM port, open the device manager and look under the "Ports" group.
Not sure how to use a terminal application? Try one of these tutorials: Tera Term Tutorial, PuTTY Tutorial.
Something went wrong! Please try again.
The QN9090 bootloader requires an image signature to verify the validity of a binary image. The image signing tool requires a Python install to exist on the PC. Download and the latest install Python 3.8 and add it to your system path. Then in a terminal window enter pip install pycryptodome to install the library.
Something went wrong! Please try again.
The QN9090 Wireless Connectivity Stack comes with a list of demo applications and driver examples ready to be compiled and run.
The QN9090 Wireless Connectivity Software package comes with a long list of BLE examples. To see what's available, browse to the 'wireless_examples' folder (\boards\QN9090cdk\wireless_examples\bluetooth).
If you are interested in running the preprogrammed example that comes with your board:
The demo application programmed out of the box for the QN9090 board is the Proximity Reporter demo. It implements a GATT server and the following profile and services.
Something went wrong! Please try again.
In order to use the Bluetooth Low Energy examples, the NXP IoT Toolbox needs to be installed on a smartphone. This application provides several examples that can be used in conjunction with the connectivity stack to connect your phone to the development board over BLE.
Something went wrong! Please try again.
You probably want to build and debug a demo by yourself. Use the guide below to learn how to build and debug an example application from the Wireless Connectivity Stacks in the MCUXpresso IDE or IAR Embedded Workbench IDE.


The following steps will guide you through opening the hybrid example. This project will be loaded to one board, while another project will be loaded on the 2nd board.

wireless_examples category, and then under the bluetooth category expand the heart_rate_sensor project and select the freertos version of project.
This particular project doesn’t make use of the UART, but for projects that do, select the “UART” option for the SDK Debug Console. Then, click on Finish
QN9090cdk_wireless_examples_bluetooth_heart_rate_sensor_freertos project name and then in the Quickstart Panel click on Build
J2 USB connector on the QN9090QN9090cdk_wireless_examples_bluetooth_heart_rate_sensor_freertos’ [Debug]

The following steps will guide you through compiling, flashing, and running a simple Heart Rate Sensor BLE application using the QN9090 board.
\boards\QN9090cdk\wireless_examples\bluetooth\heart_rate_sensor\freertos\iar) 









Something went wrong! Please try again.
Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
*.exe file you downloaded or from the Start menu, depending on the type of download you selected
| Documents and Videos | Description |
|---|---|
| AN12928 Bluetooth Low Energy Privacy and NXP QN9090 | Discusses the means that allow Bluetooth LE devices to preserve the identity of their users and how this relates to NXP QN9090 features, limitations, and applications. |
| Democratizing the Establishment of Secure Connections | Learn how NFC can be used along with the latest wireless MCUs to democratize secure connections. |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples for security are listed below.
A demonstration program that uses the KSDK software to encrypt plain text and decrypt it back using the AES algorithm.
Path:
<SDK_PATH>/boards/qn9090dk6/driver_examples/aes
A demonstration program that uses the KSDK software to generate SHA checksums.
Path:
<SDK_PATH>/boards/qn9090dk6/driver_examples/sha/
Several examples, demos and drivers are available within the SDK to help you get started. A common example for wired communications is listed below.
A number of driver examples exist within the SDK including I²C, SPI and USART.
Path:
<SDK_PATH>/boards/qn9090dk6/driver examples
| Documents and Videos | Description |
|---|---|
| AN2731 Compact Planar Antennas for 2.4 GHz Communication Features | Provides the basic insight on board layout and antenna design to improve the customer first pass success. |
| AN12610 QN9090 RF System Evaluation Report for BLE Applications | Provides RF evaluation test results of the QN9090 for BLE applications (2FSK modulation). It includes the test setup description and the tools used to perform the tests on your own. |
| AN12928 Bluetooth Low Energy Privacy and NXP QN9090 | Discusses the means that allow Bluetooth LE devices to preserve the identity of their users and how this relates to NXP QN9090 features, limitations, and applications. |
| AN1252 High Power Support | The QN9090 / QN9030 feature an integrated radio, which can be used with an external Front End. This application note is concerned with setting up the device for hardware designs that uses a FEM (FrontEnd module). |
| QN9090 Radio Certification Documents | Find certificate of declaration of conformity for the QN9090 as well as more on building a PCB right the first time. |
| Robust RF Designs for NXP’s K32W/QN Wireless MCUs with CEL Modules | The session will describe the features and performance of the NXP solution, show how combining NXP’s K32Wx/QN90x with CEL’s optimized wireless performance delivers a variety of key benefits. |
| Bluetooth Low Energy Application Developer’s Guide |
How to integrate the Bluetooth Low Energy Host Stack in an application and provides detailed explanation of the most used APIs and code examples.Path: <SDK_PATH>/docs/wireless/Bluetooth
|
| Bluetooth Low Energy Demo Applications User’s Guide |
Describes the Bluetooth® Low Energy stack enablement for the NXP development platforms. Path: <SDK_PATH>/docs/wireless/Bluetooth
|
| Bluetooth Low Energy Host Stack FSCI Reference Manual |
Provides a detailed description of the Bluetooth Low Energy Host Stack serial commands, communication packet structure, and usage of the Framework Serial Communication Interface (FSCI).Path: <SDK_PATH>/docs/wireless/Bluetooth
|
| Bluetooth Low Energy Host Stack API Reference Manual |
Presents all APIs, information and definitions relative to BLE configuration constants, Generic Access Profile (GAP), Generic Attribute Profile (GATT) and L2CAP procedures.Path: <SDK_PATH>/docs/wireless/Bluetooth
|
| Connectivity Framework Reference Manual |
An introduction to the Connectivity Framework software used to ensure portability across the ARM®-based MCU portfolio. Definitions and examples of framework services are included.Path: <SDK_PATH>/docs/wireless/Common
|
| Kinetis FSCI Host Application Programming |
Provides a detailed description for the Kinetis Wireless Host API implementing the Framework Serial Connectivity Interface (FSCI) on a peripheral port such as UART, USB or SPI.Path: <SDK_PATH>/docs/wireless/Common
|
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples for wireless connectivity are listed below.
The QN9090 SDK comes with a long list of BLE examples.
Path:
<SDK_PATH>/boards/qn9090dk6/wireless_examples/bluetooth
Examples show how to use the NTAG component in the context of a wireless application and how to transfer NFC data through the NTAG SRAM.
Path:
<SDK_PATH>/boards/qn9090dk6/wireless_examples/framework/nfc
QN9090(T) / QN9030(T) Bluetooth Low Energy Certification Tool User's Guide -Certification is mandatory for these kinds of RF product according to the regulatory of each region. The test is FCC/CE certification in US and EU areas. There are similar certification requirements in other areas.
Connectivity QTool -Connectivity QTool is a BLE PC Tools. It helps the developers to evaluate NXP's BLE devices. lt mainly includes following features: Advertising, Scanning and Connecting, Security Manager profile and other profiles such as DIS, OTAP, QPP and Wireless-UART.
Connectivity Tool Suite - Connectivity tools are a collection of applications that communicate with the NXP development boards via a serial interface. They help in the development and testing process of either 802.15.4 MAC, Simple MAC (SMAC), Thread, Bluetooth® Low Energy or Zigbee 3.0 based applications.
| Documents and Videos | Description |
|---|---|
| AN12902 QN9090/QN9030 Power Consumption Analysis | Provides information about the power consumption of QN9090 wireless MCU, how the hardware is designed and optimized for low-power operation, and how the software is configured to achieve the best low-power profile |
Several examples, demos and drivers are available within the SDK to help you get started. A common example for power management is listed below.
Allows each of the various low power modes to be selected using a simple user interface via the serial port.
Path:
<SDK_PATH>/boards/qn9090dk6/driver_examples/power_api
Several examples, demos and drivers are available within the SDK to help you get started. A common example for device management and secure OTA is listed below.
Determines if an OTA has occurred. It also determines if an application (image) is valid and whether to load a particular application or not.
Path:
<SDK_PATH>/qn9090dk6/wireless_examples/ssbl
Connect with other engineers and get expert advice on designing with the QN9090 on one of our community sites.
Get Started With QN9090 Development Platform - How To
Attach the USB Cable
Run the Out-of-Box Demo
Download MCUXpresso SDK with Connectivity Software
Install Your Toolchain
MCUXpresso Config Tools
QN9090 Drivers
Terminal Configuration
Install Python 3.8