UCODE: Built for Ecosystem Flexibility

Open Standards, Built to Scale

Open standards (GS1 EPC Gen2v2) help keep RAIN RFID interoperable across tags, readers and software as deployments scale. The Gen2 specification was developed over many years through industry-wide consensus, bringing together leading technology providers and end users alike. This collaborative foundation has enabled the industry to scale to its current level and continues to underpin future innovation. For solution designers scaling across sites, suppliers, and regions, open standards preserve choice as deployments grow.

Why Open Standards Matter as RAIN RFID Scales

As item-level tagging expands across retail, logistics, healthcare and industrial use cases, system behavior must stay predictable across vendors and over time. End users require the flexibility to change suppliers, and system integrators must avoid reader protocols that fragment deployments. True scalability depends on interoperability. Open standards keep innovation additive—new capabilities can be introduced without breaking existing deployments, while supporting long-term resilience and global compatibility.

Ecosystem collaboration

across vendors, geographies, and rollouts.

Interoperability by design

for stable, predictable RAIN RFID performance.

Scalable foundation

as item‑level tagging volumes expand.

Performance Without Compromise:
Standards-Based vs Proprietary Approaches

UCODE X delivers industry-leading performance within GS1 EPC Gen2v2. With high read sensitivity and strong write sensitivity, it supports robust reads and efficient encoding in demanding environments. That matters because Gen2v2 compliance helps ensure interoperability across standards-based RAIN RFID infrastructure—so system designers can select components based on performance, availability and cost, rather than proprietary constraints.

No proprietary air-protocol

required to achieve top-tier performance.

Standards-based interoperability

across multi-vendor infrastructure.

No closed ecosystem

that limits multi-vendor choice.

Standards‑based (Gen2v2) Proprietary Protocol
Tag chip choice Multiple vendors Single controlling company
Reader compatibility Reader‑agnostic License dependent
Mixed‑tag reads Predictable behaviour Protocol switching / priority targeting
Future expansion Additive and iterative Hardware redesign often required

Risk with proprietary protocols

They can create dependency on a single company’s licensed approach and reduce flexibility which can limit the ability to add new tag types, new suppliers, or new geographies without redesign. High performance does not require proprietary air protocols, relying on them increases long-term strategic risk and reduces the pool from which innovation can draw.