Getting Started with MCSPTR2AK396 Development Kit

Last Modified: 2025-09-30 15:59:00Supports S32K396 BLDC/PMSM Development Kit

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Software
  • 3

    Plug It In
  • 4

    Build, Run

1. Out of the Box

NXP's MCSPTR2AK396 Low-Voltage Motor Control Development Kit is designed for development of low-voltage motor control applications using the S32K396 automotive microcontroller.

This guide will walk you through the process of setting up and using the 3-Phase Permanent Magnet Synchronous Motor Control Development Kit with S32K396 (MCSPTR2AK396).

This guide also covers software (SW) installation for MCSPTR2AK396 motor control application software MCSPTR2AK396-SW.exe in revision 2.0. For MCSPTR2AK396-SW version 2.0, please refer to the MCSPTR2AK396 Getting Started webpage for software set.

1.1 MCSPTR2AK396 Overview

This section will familiarize you with the contents of this development kit.

MCSPTR2AK396 Development Kit
  • S32K396-Peripheral Component Interconnect Express (PCIe) controller board
  • 3-phase permanent magnet synchronous motor/brushless direct current
  • PMSM/BLDC low-voltage power stage based on the MC33937A pre-driver integrated circuit
  • Micro USB cable
  • +24 VDC power supply
  • Universal adapter
  • PSE power cord
  • 3 phase PMSM motor with resolver, 30 V per phase, 3000 RPM, 0.32 Nm, 95 W, 5.2 A
MCSPTR2AK396 Callouts MCSPTR2AK396 Motor Control Application Block Diagram

1.2 Get Familiar with the Boards

MCPTR2AK396 Controller Board MCPTR2AK396 Power Stage Board

2. Get Software

Sign in at nxp.com with your credentials.

2.1 Select SW packages from Automotive Software Package Manager

Open Automotive Software Package Manager and select S32K3 device.

S32DS3.5 Download 1

Unfold the FRDM Automotive Board Installation Package bundle and check S32 Design Studio, Real-Time Drivers and FreeMASTER software. Other SW packages are optional.

S32DS3.5 Download 2

Click on the Generate Bundle Installer button at the end of the page.

GS-MCSPTR2AK396-IMG51.1.

Follow the wizard instructions for Export Control and SW License Agreement (need to scroll whole text down before accepting). After that, you may close the window. Installer and Installer User Manual download will start automatically in a few moments.

GS-MCSPTR2AK396-IMG51.2

The FRDM Automotive Board Installation Package bundle allows to enable automatic installation and configuration sw without any interaction. That simplifies the installation procedure.

GS-MCSPTR2AK396-IMG51.3

2.2 Add GCC Toolchain Version 10.2

Latest version of the S32 Design Studio contains GCC toolchain only in version 11.4. For full compatibility with RTD, you need to install GCC also in version 10.2.

In S32 Design Studio, go to Help → S32DS Extensions and Updates from the top menu to open the S32DS Extensions and Updates dialogue where you may install it.

S32K3 RTD Download 1 S32K3 RTD Download 2

2.3 Download eTPU SW

Download S32K3 ETPU SW RFP 2.0.1.

Add Update Site file Install S32K3 RTD GS-MCSPTR2AK396-IMG54.1

2.4 Install eTPU SW

In S32DS, go to Help → S32DS Extensions and Updates from the top menu to open the S32DS Extensions and Updates dialogue.

Click Add Update Sites and browse for downloaded eTPU SW updatesite file or use the drag&drop option - drag downloaded updatesite file and drop on S32DS Extensions and Updates menu. Added sw package will also be automatically selected for following installation.

S32K3 RTD Download 2 eTPU SW Download 2

2.5 Get FreeMASTER Application Tool for Real-Time Debugging

Download and install the FreeMASTER application tool for real-time debugging.

Add Update Site file

2.6 Get Automotive Math and motor Control Library (AMMCLib) Set

Download and install AMMCLib for S32K3xx.

GS-MCSPTR2AK396-IMG59.1N GS-MCSPTR2AK396-IMG59N.1.

2.7 Download the Development Kit Application Software

Download and install the MCSTR2AK396 motor control application software package.

Get AMMCLib for S32K3 GS-MCSPTR2AK396-IMG60.1N

3. Plug It In

3.1 Check Default Jumper Positions

Check the default jumper positions at the 3PHLVPWBRDPCIE power stage board

3PHLVPWBRDPCIE Jumpers

3PHLVPWBRDPCIE Jumpers
3PHLVPWBRDPCIE Default Jumper Settings
Jumper State Notes
J5 2-3 Resolver S4 output routed to operational amplifier
J6 2-3 Resolver S3 output routed to operational amplifier
J7 2-3 Resolver excitation signal from TM5 signal at PCIe connector
J9 1-2 DC BUS current sensing signal measured via operation amplifier
J10 2-3 VREF as voltage source for overcurrent threshold potentiometer
J11 1-2 External overcurrent fault comparator
J16 OPEN Zero-Cross detection disconnected
J17 OPEN Zero-Cross detection disconnected
J18 OPEN Zero-Cross detection disconnected
J19 1-2 Phase A current signal routed to AN1 signal at PCIe connector
J20 1-2 Phase B current signal routed to AN3 signal at PCIe connector
J21 1-2 Phase C current signal routed to AN5 signal at PCIe connector

Check the default jumper positions at the S32K396-PCIE-MC controller board

S32K396-PCIE-MC Jumpers

S32K396-PCIE-MC Jumpers
S32K396-PCIE-MC Default Jumper Settings
Jumper State Notes
J11 2-3 CAN0 Transceiver STB signal pulled down
J13 OPEN FS26_VDEBUG signal generated - FS26 starts in debug mode
J14 CLOSED FS26_VDEBUG signal derived from VBOS signal
J15 CLOSED RESET SW2 connected to RESET_B signal
J16 CLOSED External wake-up signal connected to MCU
J17 2-3 CAN3 Transceiver STB signal pulled down
J18 1-2, 3-4 CAN0_TX and CAN0_RX signals routed to on-board CAN transceiver
J19 CLOSED Functional Safety signals FS0B and FS1B connected
J20 1-2, 3-4 CAN3_TX and CAN0_RX signals routed to on-board CAN transceiver
J22 CLOSED RESET_B signal connected as wake-up signal to FS26
J23 2-3 VHREF_H voltage connected to VDD_HV_A
J24 CLOSED RESET_B signal connected to 20-pin JTAG connector
J26 CLOSED VDD_JTAG signal present at 20-pin JTAG connector
J28 2-3, 5-6, 8-9, 11-12 JTAG signals routed to S32K3 on-board debugger
J29 OPEN External RESET signal pins
J30 CLOSED LPUART2_TX signal connected to S32K3 on-board debugger
J31 1-2 LPUART2_RX signal connected to S32K3 on-board debugger
J32 1-2 Sine Wave Generator 1 routed to TM5 signal at PCIe connector
J33 2-3 V15 voltage regulated by external NMOS transistor
J35 CLOSED PTB11 connected to TM3 signal at PCIe connector
J37 OPEN CAN0 Transceiver STB signal not connected to MCU
J38 1-2 CAN3 Transceiver STB signal not connected to MCU

In case of using an external JTAG debug probe via J20 connector, change the settings of J28 to 1-2, 4-5, 7-8, 10-11.

External Debugger

External Debugger

3.2 Assemble the Boards

To assemble the controller board to the power stage board, connect the board to the PC with a micro USB cable

S32K396 Motor Control Kit

S32K396 Motor Control Kit

Optionally use the support column for improving mechanical robustness

S32K396 Motor Control Kit

S32K396 Motor Control Kit

3.3 Connect USB and Power Supply

  1. Connect the board with PC by micro-USB cable
  2. Connect the kit USB and Power Supply

    Connect the kit USB and Power Supply
  3. Plug a 24 V power supply to the power stage board
  4. Connect the kit USB and Power Supply

    Connect the kit USB and Power Supply

4. Build, Run

Let's take your MCSTR2AK396 motor control kit for a test drive.

4.1 Select Application and MCU Programing

Select the appropriate PMSM or BLDC motor control application from the installed directory NXP\MC_DevKits\MCSPTR2AK396\sw .

To import the installed application software project in the S32 Design Studio IDE for S32 Platform:

  1. Launch S32DS for S32 Platform
  2. Go to File > Import, then select General > Existing Projects into Workspace
  3. Import Project
  4. Navigate to the installed application directory: NXP\MC_DevKits\MCSPTR2AK396\sw and choose appropriate project and click OK. Then, click Finish
  5. Import MCSPTR2AK396 Project

4.2 Use Configuration Tool

  • Unfold the structure of the M7_0_0 project and double-click on *.mex file to open the project configuration in S32 Configuration Tool
  • Mex File
  • Ensure that you are configuring the M7_0_0 project, and click Update Code button for generating configuration files. Next, in the S32 Configuration Tool, click the pop down button next to the project name and choose *.mex file for the M7_0_2 project. Click the Update Code accordingly
  • Update Code

4.3 Upload Software and Debug

  1. In S32DS, return back to the C/C++ perspective
  2. C_Cpp Perspective
  3. Use the Debug Configuration menu for uploading software into the MCU
  4. Debug Menu
  5. Next, expand Launch Group and click the first launch configuration. This configuration will upload both the M7_0_0 and M7_0_2 projects to the MCU. Click Debug for building and uploading software into MCU
  6. Debug Configuration
  7. The S32DS will switch into debug perspective where you may let the code run by clicking Resume (or press F8)
  8. Resume
  9. Click Disconnect to avoid interference between the S32DS IDE debugger and the FreeMASTER tool
  10. Confirm Perspective Switch

4.4 Set Up the Debugging Tool

Launch the FreeMASTER application.

To open the *.pmpx FreeMASTER project \FreeMASTER_control, click File > Open Project.

FreeMASTER Project

To enable communication, in the FreeMASTER toolbar, click Go (or press Ctrl+G). Successful communication displays in the status bar at the bottom as:

RS-232; port=COMn; speed = 115200

FM Start

Application Control

Application Setup (Optional Step)

If you run MCSPTR2AK396 sw on a modified or own hardware platform, you may need to edit hardware scales and fault triggers. In the Motor Control Application Tuning (MCAT) Tool switch to the Application Setup page and edit values on the left side.

GS-MCSPTR2AK396-IMG6.1

Once you finish, click Save config to generate a static configuration file. You may check file content at the Output file page.

Now, repeat step from the Upload Software and Debug section to build the project and upload the code into MCU.

Motor Parametrization and Control Loops Autotuning

In a case of motor change, you may benefit from new MCAT 2.0 motor parametrization and control loops autotuning features.

At Motor Parameters page, fill four basic motor parameters that cannot be detected automatically:

  • Number of pole pairs
  • Nominal Current
  • Nominal Speed
  • Maximum Speed

Click Update target button and start the motor parameters estimation and automating tuning for control loops. Parameters are automatically updated typically in less than a minute.

GS-MCSPTR2AK396-IMG6.2

For more information about the automatic motor parametrization and control loops autotuning please read AN15061 Application Note in MCSPTR2AK396\doc folder. Default path: c:\NXP\MC_DevKits\MCSPTR2 AK396\doc\ApplicationNotes\AN15061 MCAT 2.0 - Motor Control Application Tuning Tool for PMSM FOC.pdf.

Spin the Motor

Switch, for example, to the Speed Loop page. Under the Speed control tab, configure the required speed and turn on the motor drive.

GS-MCSPTR2AK396-IMG6.3

Select one of the predefined Scopes or Recorders in Project Tree to watch the application variables in real-time. For comfortable run-time debugging you may create or modify any of scopes or recorders.

GS-MCSPTR2AK396-IMG6.4
  • Check pending faults
  • In case of pending faults, click the CLEAR button at MCAT control tab or alternatively press simultaneously SW2 and SW3 on the board.

    GS-MCSPTR2AK396-IMG6.5 GS-MCSPTR2AK396-IMG6.6
  • Start application
  • Click On/Off on the control bar or press SW2/SW3 on the board to initiate clockwise/counterclockwise spinning of the rotor.

  • Set Speed
  • Modify Required Speed field on the control bar or change Speed Required in the Variable Watch window. Alternatively control speed by pressing SW2 or SW3 switches.

    GS-MCSPTR2AK396-IMG6.7
  • Stop Application
  • Stop the motor by clicking the On/Off button on the MCAT control page, Clear On/Off variable or use the On/Off switch on the 3PHLVPWBRDPCIE board.