Getting Started with the FRDM-AUD10 Development Board

Last Modified: Oct 9, 2026 new Supports FRDM-AUD10, HiFi 5 audio DSPs, Arm Cortex-M7 MCU

Contents of this document

  • 1

    Out of The Box
  • 2

    Get Software
  • 3

    Run And Install
  • 4

    Programming
  • 5

    Build And Run
  • 6

    Audio Software

1. Out of The Box

The development kit includes:

  • FRDM-AUD10 evaluation board
  • Quick Start Guide

The user needs to prepare two USB-Type C cables and one RJ45 Ethernet cable.

To begin developing the user’s application on the AUD10 follow the detailed instructions provided below.

1.1 Get Familiar With The Board

FRDM-AUD10 Board Top View Showing Main Components

1.2 Board Cable Connections

Connect a USB-Type C cable to the USB-Type C power connector (J16) to provide 5 V power.

The user can use the GUI to control the AUD10 via MCU-Link and/or Ethernet.

Control AUD10 via MCU-Link: Connect a USB-Type C cable to the USB-Type C debug connector (J10), then connect the other end of the cable to the PC.

Control AUD10 via Ethernet: Connect the FRDM-AUD10 board to the PC using an RJ45 Ethernet cable. Please note that a direct connection is required. Do not connect through a network switch, as network switches are currently not supported.

FRDM-AUD10 Board Cable Connections

1.3 Bootstrap Modes

The GPIO0 and GPIO1 of the AUD10 are designated as the bootstrap pins.

The following table specifies the bootstrap selection for the AUD10.

GPIO[1…0] Boot mode description
00 Boot image download from external flash using SPI-M interfacing
01 Boot image send to the system via host using PCIe interface or SPI interface, host assisted boot mode. PCIe clock 100 MHz(External)
10 Boot image send to the system via host using PCIe interface or SPI interface, host assisted boot mode. PCIe clock 125 MHz(External)
11 Boot image sends to the system via host using PCIe interface or SPI interface, host assisted boot mode. PCIe clock 124.8 MHz(Internal)

On the FRDM-AUD10 board, J21 pin pairs 23-24 and 21-22 are used to set the GPIO0 and GPIO1 levels of the AUD10. Placing a jumper cap sets the corresponding GPIO level to 0, while removing it sets the level to 1.

J21 pin pair 23-24: To set the GPIO0 level.

J21 pin pair 21-22: To set the GPIO1 level.

Boot Strap Mode Selection

Select Boot From Flash Mode For The AUD10

Place jumper caps on J21 pin pairs 23-24 and 21-22 to set both GPIO0 and GPIO1 of the AUD10 to logic 0. GPIO[1…0] = 00, boot from flash mode is selected by the AUD10.

  • GPIO0 = 0
  • GPIO1 = 0
Select Boot from Flash Mode

Select Host Assisted Boot Mode For The AUD10

Remove the jumper caps from J21 pin pairs 23-24 and 21-22 to set both GPIO0 and GPIO1 of the AUD10 to logic 1. GPIO[1…0] = 11, boot from flash mode is selected by the AUD10. The user can also choose to set GPIO[1..0] to 01 or 10.

  • GPIO0 = 1
  • GPIO1 = 1
Select Host Assisted Boot Mode with GPIO[1…0] = 11

2. Get Software

2.1 Recommended PC Configuration For GUI Installation

AUD10 GUI is designed to run on general-purpose, moderately powerful desktop PCs or laptops. The following is the recommended PC configuration:

Operating System Windows 10 and Above
RAM 4 GB
Hard Disk SSD SSD, with a minimum of 2 GB of free space
Text size 150%
Display Resolution 1920x1080

Users may experience intermittent disappearance of certain GUI elements (for example: combo boxes, checkboxes, radio buttons) when changing screen resolution or display scaling, particularly on systems using Intel integrated graphics. This behavior is associated with known rendering issues in some Intel GPU drivers when used with Qt-based applications.

Recommended Actions:

  1. Avoid changing screen resolution, switching displays or adjusting display scaling while the application is running
  2. If the issue occurs, restart the application to restore normal GUI behavior

2.2 Installation Prerequisites On PC

Before using the GUI, the following software must be downloaded to the user’s PC.

class="metadata">Table 3. Software Overview

Sr No. Software Name Package Name Description
1 AUD10 GUI installer exe SAF9X00_GUI_R<x.y.z_yyyymmdd>_Setup.exe Windows OS installer package for AUD10 GUI.
2 AUD10 firmware binaries SAF910X_101_SBL_v<x.y.z>_rel_secure.bin AUD10 firmware binaries would be available in the package, which needs to be loaded on the device
SAF910X_101_CKC_S<abcd>_secure.bin
SAF910X_101_SC_QA-FRDM1.0_<x.y.z>_secure.bin
SAF910X_101_CAP_v<x.y.z>_rel_secure.bin
SAF910X_101_APP_<ABCD>_QA-FRDM1.0_<yyyymmdd-HHMMSS>_rel_secure.bin

2.3 GUI Installation

Start installing AUD10 GUI by double-clicking SAF9X00_GUI_R<x.y.z_yyyymmdd>_Setup.exe.

Follow the on-screen instructions to complete the installation process.

  1. Welcome window Welcome Window
  2. Click the "Browse..." button to select another installation folder path if needed Installation Folder Selection
  3. Installation Progress Installation Progress
  4. Click the "Finish" button to complete the installation Installation Completion

Click the Windows "Start" menu button, look for the application SAF9X00_GUI_R[version], click the AUD10 GUI Application as shown in the Figure

Launching the GUI from Windows Start

The following screen appears on a successful launch.

Successful GUI Launch

Users can verify the installed GUI version from the title bar of the GUI.

If any earlier version of the AUD10 GUI is installed on the system, a pop-up will appear, requesting the user to press OK to uninstall the earlier version or press Cancel to install without uninstalling the earlier version.

Uninstall the Earlier Version

Configure The PC’s Ethernet Adapter IP Address

To control the AUD10 via Ethernet, the PC's Ethernet adapter must be configured with an IP address on the same subnet as the AUD10.

The AUD10 uses the static IP address 192.168.1.80. assigns the PC an unused IP address in the 192.168.1.x subnet (for example, 192.168.1.100) and ensures that there are no IP address conflicts on the network.

Configure the PC's Ethernet Adapter Edit IP Settings

2.4 TCP Server

Run quantum-tcp-server.exe print in a Command Prompt window on the PC.

The TCP Server IP address will be displayed in the Command Prompt window.

For example:

Run the TCP Server

3. Run And Install

3.1 Boot The AUD10 via MCU-Link

The following steps describe how to use the GUI to boot the AUD10 via MCU-Link.

  1. Refer to Section 1.3.2 to select Host Assisted Boot Mode for the AUD10
  2. Refer to Section 2.2 to run the TCP Server and obtain its IP address
  3. Open the GUI, enter the TCP Server IP address and Port number (12345), then click the "Connect" button. Check if the GUI is connected to TCP Server successfully Connect the GUI to the TCP Server Connect the GUI to the TCP Server
  4. In the Settings tab, set Board to FRDM Board, Port to SPI_1, and Boot mode to Host assisted boot. Set File Selection to Binary files, then select the following firmware binaries in order:
    • SBL
    • CKC
    • SoftConfig
    • CAP
    • Binary (NEEE)
    • AWE or AOC Binary

    Next, click the "Boot" button to boot the AUD10.

    Settings to Boot the AUD10 with NEEE Binary
  5. Check if boot is completed successfully Successful Boot
  6. Refer to Section 5 to control the AUD10 via Ethernet

4. Programming

4.1 Flash Programming

The following steps describe how to use the GUI to program the flash of the AUD10 via MCU-Link.

  1. Refer to Section 1.3.2 to select Host Assisted Boot Mode for the AUD10
  2. Refer to Section 2.2 to run the TCP Server and obtain its IP address
  3. Open the GUI, enter the TCP Server IP address and Port number (12345), then click the "Connect" button. Check if the GUI is connected to the TCP Server successfully
  4. In the Settings tab, set Board to FRDM Board, Port to SPI_1, and Boot mode to Host assisted boot. Set File Selection to Binary files, then select the following firmware binaries in order:
    • SBL
    • CKC
    • SoftConfig
    • CAP
    • Binary (FEEE)

    Next, click the "Boot" button to boot the AUD10.

    Settings to Boot the AUD10 with FEEE Binary
  5. Check if the boot is completed successfully
  6. Click the "Sync" button of the GUI, a green “LED” should show up at the bottom of the window indicating the CMD subsystem is up CMD Subsystem is Active
  7. In Setting > Flash Programming, select the appropriate flash binary, either AOC or AWE. Click the "Program Flash" button Program the Flash
  8. Check if flash programming is completed successfully Successful Flash Programming
  9. Close the TCP Server and the GUI, power off the board. Refer to Section 1.3.1 and select Boot from Flash Mode for the AUD10. Then power the board back on. After the board boots up, verify connectivity by pinging the AUD10 at IP address 192.168.1.80.
  10. Run the TCP Server and the GUI, enter the TCP Server IP address and Port number (12345) to connect the GUI to the TCP Server
  11. Refer to Section 5 to control the AUD10 via Ethernet

5. Build And Run

5.1 Connect The GUI To The AUD10 via Ethernet

In the Settings tab, set Board to FRDM Board, Port to Ethernet. Enter the AUD10 IP address 192.168.1.80 and port number 12345, then click the "Connect" button. Check if the GUI is connected to the AUD10 successfully.

Connect the GUI to the AUD10 via Ethernet

5.2 AOC Demonstration

Early Audio is output through the Line Out (J2) and Headphone Out (J3) immediately after the AUD10 starts.

In the Commander Sender tab of the GUI, send Ethernet commands to configure the AWE input and output.

For example, after sending the following two Ethernet commands, the audio signal received on Stereo3 In (J7) is processed by AWE and output through IIS0 out. The user can hear the processed audio through Line Out (J2) or Headphone Out (J3).

Send Ethernet Commands to AWE

To tune the AWE project using Audio Weaver, send the following command in the GUI to enable AWE.

Enable AEW

Open Audio Weaver (Version 8.D.2.6).

In AWE Server, click Target > Change Connection.

In the Change Connection window, select TCP/IP from the Connection drop-down list and enter 127.0.0.1 in the IP Address field. Then, click the "Change" button.

Connection Configuration in AWE Server Connection Configuration in AWE Server

In AWE Designer, click File > Open.

Open the awd file in AWE Designer

Select the desired awd project and then click the Run button.

Run the awd file in AWE Designer

The user can double-click the desired module and adjust the parameters as needed. The sound effect will be applied immediately.

Parameter Settings in AWE Designer

Audio Software

6.1 Audio SDK

The AUD10 Audio SDK enables users to develop applications that run on the HiFi 5 core.

Please refer to the AUD10 Audio SDK documentation for more details: ~\hifi5\aoc-frdm-sdk-1.9.0\docs\index.html

AUD10 Audio SDK Documentation

Design Resources

Board Information

Chip Information