1
Plug It In2
Get Software3
Run Sensor Demos4
EvaluateSign in to save your progress. Don't have an account? Create one.

FRDM-K64-AGM01 demonstration kit as an exampleSomething went wrong! Please try again.
Connect the "Sensor Demonstration Kit" to the PC via the USB cable between the OpenSDA USB port on the board and the USB connector on the PC.
Something went wrong! Please try again.
All the standard sensor demonstration kits should work out of box with the STB-CE software. These standard kits do not require any jumper changes. In case of custom sensor kits, there are a few jumper modifications recommended.
Find the complete list of all the sensor demo kits with the appropriate jumper settings here.
Something went wrong! Please try again.
Kinetis FRDM MCU boards are supplied with OpenSDA firmware pre-loaded. For a smooth out of box sensor demonstration with STB-CE, make sure that the latest version of the default OpenSDA bootloader and firmware application is on the FRDM development board. This allows debugging, flash programming and serial communication over a USB cable.
The default OpenSDA firmwares for all FRDM based sensor demonstration kits used with STB-CE are as follows:
FRDM-K22F, FRDM-K64F, FRDM-KW41Z, FRDM-KE15Z, RD-KL25-AGMP01FRDM-KL25Z, FRDM-KL27ZObtain the latest OpenSDA drivers for FRDM boards from OpenSDA Update to the FRDM boards.
Locate the section "Download – OpenSDA Bootloader and Application" and select your FRDM Board from the dropdown list. Strictly follow the provided instructions to program the board.
For Windows 10 systems, the older versions of the OpenSDA drivers could get corrupted when
the board is plugged on a Windows 10 machine. As a result, many boards might get not
detected as an MSD or a COM port on Windows 10. The latest versions of the OpenSDA software are
compatible with Windows 10 and can be obtained from the link above. The current FRDM-K64F,
FRDM-K22F, FRDM-KL25Z and RD-KL25-AGMP01 boards come with an older version of OpenSDA
drivers from the factory and require a mandatory OpenSDA update.
Something went wrong! Please try again.
The output data from the provided example applications is provided over the MCU UART. This requires that the driver for the board's virtual COM port is installed on the PC. The board MUST be plugged into the PC before the driver installer is run.
If you have not installed already an ARM IDE toolchain, download and install the Windows drivers corresponding to the default OpenSDA application selected above:
PEmicro Windows Serial Driver mbed Windows Serial Driver
Once the Windows Serial Port Drivers are installed on the PC, determine the port number of the board's virtual COM port by opening the device manager and looking under the "Ports" group.
The demonstration kit is now ready to communicate with the PC.
Something went wrong! Please try again.
Download and install NXP Sensor Toolbox - CE (STB-CE) v2.5 from the download button on the Overview tab. If needed, please see the User Guide for more detailed instructions.
Something went wrong! Please try again.
STB-CE enables "Out of Box Sensor Demonstrations and Evaluations" on all the available NXP sensor demonstration kits. The ISSDK firmware and the GUI project are auto loaded providing a plug-and-play experience.
Click on the Sensor Toolbox-CE icon on your desktop. Once the window opens, click on "Out of Box Sensor Demonstrations".
Something went wrong! Please try again.
On following the prompts accurately, the appropriate ISSDK firmware will be auto loaded (if required) to the MCU and the corresponding sensor GUI will auto load.
For the chosen example demonstration kit FRDM-K64-AGM01, the AGM01 sensor board
has a 6-axis (Accel, Mag) FXOS8700 sensor and 3-axis FXAS21002 gyroscope sensor. STB-CE
currently provides one out of box demonstrations for each sensor.
Take the FXOS8700 6-Axis (Accel, Mag) demo as an example.
On following appropriate prompts, the ISSDK firmware for FXOS8700 demo will get loaded to the K64F MCU and the appropriate GUI will launch. If the demo kit already has the appropriate firmware, the FXOS8700 6-axis (Accel, Mag) demo will automatically launch without any firmware download.
Something went wrong! Please try again.
The GUI project window comprises two different screens - form(s) and the "Register" screens. Therefore, the user will see multiple tabs on launching the GUI, as shown in the images below.
For the FXOS8700 demo example, the forms comprise the accelerometer and the magnetometer GUI as shown below:
Here are some key things that can be observed from the above sensor demonstration with STB-CE:
Similarly, all the other available out of box sensor demos provide demo features like Streaming, Logging and Sensor Event detection.
Something went wrong! Please try again.
Apart from sensor demonstrations at pre-configured firmware settings, each GUI in this tool allows a user to make sensor configuration changes conveniently.
This feature allows a user to make sensor configuration changes in the form(s) in a GUI. This enables a user to make quick changes to critical sensor settings and then stream or log data to see the updated results.
As shown in the image below, in the FXOS8700 demo, the user has the facility to change the power modes, range, ODR and enable/disable events (once in Standby mode) and see the updated results. For example, the streaming data would have an observable noise difference in a "High-Resolution" mode as compared to the "Low Power" mode of the sensor.
Something went wrong! Please try again.
With complete access to the sensor register map with descriptions, this tool provides an easy and intuitive interface for detailed register level evaluation. It enables quick read and writes to single/multiple registers or parameters with ease. It also allows saving user-specific register configurations and loading it later for use. The register operations include:
The image below shows the register screen for the FXOS8700 demo:
Something went wrong! Please try again.
Apart from out of box sensor demonstrations, this tool also supports running standalone STB-CE GUI projects. A standalone project is provided by NXP as a separate package (.stbpkg). To successfully run the custom GUI project, the MCU must have the appropriate firmware loaded.
For more details, please find the User Guide in the Documentation tab.
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with the FRDM Sensor Toolbox on our community site.