1
Installing MCU-Link Pro and updating firmware2
Using MCU-Link Pro with MCUXpresso IDE3
Setting up MCU-Link Pro with 3rd party IDEs4
Using other serial terminal programsSign in to save your progress. Don't have an account? Create one.
Setting up your MCU-Link Pro is very simple. The first step is to download the installer, which installs host side drivers and includes a utility to update the firmware. Note that MCUXpresso IDE 11.4.1 or later will automatically install the driver information files. You can either watch the video below for Windows installation, or follow the steps to install MCU-Link Pro:
First step is to download the MCU-LINK installer package for your chosen host operating system. After downloading, run the installer.
Something went wrong! Please try again.
Although MCU-Link Pro comes with firmware installed, this should be updated to the latest version. To perform the update:
program_CMSIS.cmd
script. Follow the on-screen instructions
Note: program_JLINK.cmd
may be used if the J-Link option is desired, but this firmware does not support energy measurement or USB bridging.
Note: Review the Readme.txt for other OS-specific setup.
Something went wrong! Please try again.
MCU-Link Pro will enumerate 4 devices when fully installed -a CMSIS-DAP device and Trace port under HID devices, plus a VCOM port under Ports:
Image 1. MCU-Link Pro Ports
Inage 2. MCU-Link Pro Ports
Something went wrong! Please try again.
MCUXpresso IDE will automatically detect MCU-Link Pro, just as it does with other supported probes (note version 11.4.1 or later should be used). The MCU-Link Pro VCOM feature is independent of the IDE, but the built-in Serial terminal feature of MCUXpresso IDE can be used with it. See this short tutorial video for an overview of using MCU-Link Pro with MCUXpresso IDE:
Something went wrong! Please try again.
MCU-Link Pro can be used with IDEs from our partners, such as Arm Keil uVISION and IAR Embedded Workbench. Set up is straightforward, as with any other CMSIS-DAP probe:
Install the latest version IAR available. The version must be at least, IAR Embedded Workbench IDE for Arm 8.40.2.
With your project workspace open, right mouse click on the project:
Something went wrong! Please try again.
MCU-Link Pro's VCOM feature can be used with serial terminal emulation programs such as PuTTY and TeraTerm. Set up is as with similar VCOM devices. Most MCUXpresso SDK examples will use a configuration of 115200 baud rate, 8 data bits, no parity and 1 stop bit. To determine the port number of the MCU-Link Pro virtual COM port, open the device manager and look under the "Ports" group (as shown earlier). Check the following tutorials: Tera Term Tutorial, PuTTY Tutorial.
Something went wrong! Please try again.
Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
Learn more about the MCU-Link with design tips, training documents, and the NXP Community. If you need additional help, contact NXP Support.
Connect with other engineers and get expert advice on designing with the MCU-Link on one of our community sites.