Getting Started with the SEN-SPI-BOX Evaluation Board

Last Modified: 2021-10-04 15:23:09Supports SEN-SPI-BOX: Evaluation Tool for Automotive Sensors

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Install Software
  • 4

    Use the Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the SEN-SPI-BOX board.

1.1 Kit Contents/Packing List

The SEN-SPI-BOX contents include:

  • One Sensor SPI Master Kit (SEN-SPI-BOX)
  • One USB Type A USB cable
  • One NXP MDI ribbon cable (16-pin)
  • One Beagle ribbon cable (10-pin)
  • One debug cable
  • One 8 GB microSD card
  • One microSD to PC adapter
GS-SEN-SPI-BOX-IMG1

1.2 Additional Hardware

The SEN-SPI-BOX kit can be coupled with SEN-GEN6-SKT.

The following figure shows how to couple the SEN-SPI-BOX with a SEN-GEN6-SKT board for the FXLS9xxxx evaluation.

GS-SEN-SPI-BOX-IMG2

1.3 System Requirements

NXP Sensor FFV Tool software is compatible with Window-based computer. Win10 (x86, x64) is recommended. Older version of Window Microsoft OS could work but have not been tested and are not supported.

2. Get Hardware

2.1 Board Description

The NXP SEN-SPI-BOX kit provides a full-solution of built-in functionalities to communicate with any SPI/I2C sensor. The kit graphs real-time data, executes custom scripts, and verifies sensor status. The NXP FFV tool which works with the SEN-SPIBOX can graph real-time data, execute custom scripts, and verify sensor status.

The software currently supports FXLS90xxx, FXLS93xxx, FXLS8962, MMA69xx, MMA65xx, MMA68xx NXP automotive sensors.

2.2 Board Features

  • Board based on an NXP Cortex M4 microcontroller (M4MK64FN1M0VLQ12)
  • USB connectivity to communicate with any Win10 based machine
  • Built-in SD Card boot loader to allow firmware upgrades
  • Two separate terminals to connect any sensor board using a ribbon cable or the debug cable included in the kit
  • Supports 3.3 V and 5.0 V sensors
  • Auxiliary output supplies: 10.5 V, 13.5 V
  • SPI interface, up to 12 MHz, supports 8, 16, 24, and 32-bit transfers
  • I2C interface: up to 1 MHz

2.2 Board Components

Overview of the SEN-SPI-BOX board.

SEN-SPI-BOX components SEN-SPI-BOX components

The kit contains an NXP SEN-SPI-BOX evaluation board, three different cables compatible with dedicated NXP sensor boards, a microSD card for built-in boot loading capability, and a USB Type-B cable to connect the kit to a computer.

The kit is powered by an NXP Kinetis® K64F Cortex M4 Microcontroller.

3. Install Software

Go to SEN-SPI-BOX: Evaluation tool for Automotive Sensors and download the software.

Double-click the downloaded .msi file and follow the instructions.

4. Use the Hardware

  1. Connect the FFV kit via the USB Type-B cable included in the kit
  2. Launch the software
  3. Select a predefined sensor package
  4. GS-SEN-SPI-BOX-IMG5
  5. After the software detects the kit, enable and select the voltage for the power supplies as needed
  6. GS-SEN-SPI-BOX-IMG6
  7. Connect the sensor board to the SEN-SPI-BOX kit using a ribbon cable (NXP MDI or Beagle terminal) or the debug cable
  8. GS-SEN-SPI-BOX-IMG7 GS-SEN-SPI-BOX-IMG8
  9. In the Sensor First Field Verification Tool window, click Scan
  10. GS-SEN-SPI-BOX-IMG9
  11. Click Select to confirm the sensor selection from the device list
  12. Play the demo

Support

Forums

Connect with other engineers and get expert advice on designing with the SEN-SPI-BOX on one of our community sites.