1
Out of the Box2
Plug It In3
Get Software4
Build, Run5
TroubleshootingSign in to save your progress. Don't have an account? Create one.

The Trimension SR250 development board offers a flexible platform for integrating ultra-wideband (UWB) ranging and radar into consumer and industrial IoT solutions. It enables an easy integration of Trimension SR250 for presence, location and motion detection, helping improve efficiency and safety.
This page will guide you through the setup and operation of the Trimension SR250 development board.
The kit contents include:
Something went wrong! Please try again.
In addition to the kit contents, you will also need the following hardware.
FRDM-RW612 Development Board Some minor rework is necessary to route the API interface pins to the Arduino headers for proper communication with SR250-ARD board.
In order to allow the SR250-ARD shield to communicate with the FRDM-RW612 board via SPI, a small rework is required to expose the SPI signals on the Arduino headers.
Alternatively you could simply interconnect FRMD-RW612 Arduino compatible header pins D0 to D11 and D1 to D12 via jumper wires.
Something went wrong! Please try again.
In the first step, you will assemble the boards together through the Arduino headers:
Make sure both USB-C ports of the FRDM-RW612 board are connected to the laptop.
For additional guidance, please refer to the SR250 UWB Plug-and-Play Application .
Something went wrong! Please try again.
When setting up the development environment, you will need the following software:
Python 3.8 or later.
And the following dependencies:
# Install Python dependencies
pip3 install west ninja# Verify installations
python3 --version
cmake --version
ninja --version
west --versionSomething went wrong! Please try again.
The following steps below will guide you through setting up the build environment for Zephyr-based projects.
# Download SR250 Software to working directory
git clone https://github.com/nxp-uwb/sr250-uwbiot-zephyr.git# Initialize west workspace
cd ~/sr250-uwbiot-zephyr
west init -l --mf west.yml uwbiot-top# Download Zephyr OS and all dependencies
west update# Install Zephyr Python dependencies
pip install -r zephyr/scripts/requirements.txt# Set the environment (required for each new terminal session)# Windows:
zephyr\zephyr-env.cmd# Linux:
source zephyr/zephyr-env.shBuilding Demo Application
# Example: Build ranging controller demo
west build -b frdm_rw612 -p auto uwbiot-top/demos/common/demo_ranging_controller/zephyr# Example: Build radar demo
west build -b frdm_rw612 -p auto uwbiot-top/demos/radar/demo_radar/zephyrReplace the demo path with the specific demo that you want to build.
Note: To ensure that the SR250 firmware and calibration parameters are up to date, it is recommended to run the following before running other demos:
uwbiot-top/demos/SR2xx/demo_sr2xx_fw_updateuwbiot-top/demos/SR2xx/demo_device_calibration# Flash built application using west flashOpen your serial terminal application and connect to the FRDM-RW612 HS-USB interface through Virtual COM port set to the following configurations:
After resetting the FRDM-RW612 board, the demo application will display initialization messages, status updates and operational logs in the terminal window.
In this step, you will ensure that MS Visual Studio (VS) Code is properly installed.
Follow these steps to install the needed VS Code extensions for Zephyr development:
Step 1: Open Extensions View
Ctrl+Shift+X or Cmd+Shift+X on macOS)Step 2: Install the Required Extensions
To set up VS Code, you will install the following extensions:
Step 3: Install MCUXpresso Zephyr Dependencies
During the setup, the Zephyr integrated development environment (IDE) extension will prompt you to install the required dependencies for MCUXpresso Zephyr development.
Open MCUXpresso Installer
Note: If the MCUXpresso Secure Provisioning Tool (SEC) or FreeMASTER fails to install, you can move forward without these components.
Part 1: Zephyr Dependencies Installation
During the first part of installing Zephyr dependencies, the image below is what will appear on your screen.
Part 2: Zephyr Dependencies Installation
During the second part of installing Zephyr dependencies, the image below is what will appear on your screen.
Note: The dependency installation may take several minutes depending on your Internet connection.
Import the FRDM-RW612 Zephyr Repository
Ctrl+Shift+P or Cmd+Shift+P on macOS)
Understanding the Project Structure
The FRDM-RW612 Zephyr project is CMake-based, which provides:
Import the CMake Project
In the following steps, you will complete the import of CMake.
Note: Set the App type to Repository application.
Important: Ensure that the CMake Tools extension is properly installed before attempting to import the project.
In the following steps, you will build and flash the application.
Select Build Configuration
Build the Application
Build button in the status bar or open Command Palette and select CMake: BuildBuild Output Location
The compiled binaries will be generated in the build directory that corresponds to your selected configuration:
build/Debug/ (for Debug builds)build/Release/ (for Release builds)Note: The build process may take a few minutes on the first run as dependencies are compiled.
In the following steps, you will debug your development environment.
Configure Debug Settings
Ctrl+Shift+D)
Hardware Connection Checklist
Before you begin debugging, verify that the:
Start Debugging
F5 or click the green play button in the Run and Debug viewSomething went wrong! Please try again.
This section covers common issues for both VS Code and command line builds.
West Command Not Found (Linux)
# Install west via pip
pip install --user west
export PATH=$PATH:~/.local/binBuild Fails (“No Such File or Directory”)
# Ensure west update completed successfully
west update# Try a pristine build
west build -b frdm_rw612 -p always Windows: File Not Found Errors for Existing Files
Symptom:
You may encounter errors (as shown below) even though the files do exist in your workspace:
fatal error: : No such file or directory CMake Error: Cannot find source file: Error: The system cannot find the path specifiedCause:
Windows has a default MAX_PATH limit of 260 characters. When file paths exceed the character limit, Windows cannot access them, resulting in “file not found” errors.
Solution:
To locate the files, either use shorter workspace paths (such as C:\uwb) or enable long path support by using one of the following methods:
# first method: in registry editor
1. Press Win + R, type "regedit" and press Enter
2. Go to: HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\FileSystem
3. Find or create a DWORD value: LongPathsEnabled
4. Set value to: 1
5. Restart your computer# Second method: in Group policy editor
1. Press Win + R, type "gpedit.msc" and press Enter
2. Navigate to: Computer Configuration > Administrative Templates > System > Filesystem
3. Enable "Enable Win32 long paths"
4. Restart your computer# Third method: via PowerShell command (to be run as Administrator)
New-ItemProperty -Path "HKLM:\SYSTEM\CurrentControlSet\Control\FileSystem" -Name "LongPathsEnabled" -Value 1 -PropertyType DWORD -ForceWindows: Use WSL2 (Recommended Alternative)
When encountering compatibility issues, try the Windows Subsystem for Linux (see below).
# Install WSL2 from PowerShell (Administrator)
wsl --install# Then work within WSL2 Ubuntu environment# Follow Linux instructions from thereCMake Error (“fatal error: opening dependency file” or “No such file or directory”)
The above errors occur when CMake cannot find generated dependency files, often due to:
Error Example
With CMake, you may encounter the following:
fatal error: opening dependency file modules\psa_crypto_driver\...
\mcuxClPsaDriver_generate_ecp_key.c.obj.d: No such file or directoryfatal error: opening dependency file build/CMakeFiles/myproject.dir/src/
main.c.obj.d: No such file or directoryThis happens due to any of the following issues:
Solutions
Below are suggestions for resolving CMake errors.
# 1. Clean build directory completely
rm -rf build/
# 2. Re-run west update to ensure all dependencies are fetched
west update
# 3. Try pristine build
west build -b frdm_rw612 -p always
# 4. If still failing, check if all modules are present
west list
# 5. Verify CMake can find the toolchain
cmake --version Python Version Mismatch
If you encounter a Python mismatch, refer to the following:
# Ensure Python 3.8 or later
python --version
# Upgrade if needed
sudo apt install python3.10 # LinuxMultiple Python Versions Conflict
If you encounter a conflict related to multiple versions of Python, refer to the following:
# Use virtual environment
python -m venv ~/Myvenv
source ~/Myvenv/bin/activate
# Then proceed with setupCMake Version Is Too Old
To rule out the CMake version being out of date, refer to the following:
# Check version
cmake --version
# Upgrade via pip
pip install --upgrade cmake
# Or install from official source
# Linux: https://cmake.org/download/
# macOS: brew install cmakeNinja Not Found
If Ninja is not found, refer to the following:
# Install Ninja
pip install ninja
# Or via package manager
sudo apt install ninja-build # Linux
brew install ninja # macOSZephyr SDK Not Found (Linux)
When the SDK is not found, refer to the following:
# Set environment variable
export ZEPHYR_SDK_INSTALL_DIR=~/zephyr-sdk-0.16.5
# Add to ~/.bashrc for persistence
echo 'export ZEPHYR_SDK_INSTALL_DIR=~/zephyr-sdk-0.16.5' >> ~/.bashrcOut of Memory During Build
If the system indicates that it is out of memory, refer to the following:
# Limit parallel jobs
west build -b frdm_rw612 -p auto -- -j2
# Or set in environment (Linux)
export CMAKE_BUILD_PARALLEL_LEVEL=2 Disk Space Issues
If you encounter a disk space error, refer to the following:
# Check available space
df -h .
# Clean old builds
rm -rf build/
# Clean west cache (if needed)
rm -rf ~/.west/Module Import Errors in Python
If you encounter module import errors, refer to the following:
# Reinstall requirements
pip install -r zephyr/scripts/requirements.txt --force-reinstall
# Clear pip cache
pip cache purgeUseful Debug Commands
The following are additional commands to assist with the debugging process:
# Verbose build
west build -b frdm_rw612 -p auto -v # Show west configuration
west config# List all projects and their status
west list# Show build system info
west build -b frdm_rw612 -p auto -- --trace # Check environment variables
env | grep ZEPHYRGetting Help
If issues persist, consult these additional resources:
Something went wrong! Please try again.
Permission Denied When Flashing (Linux)
If you are denied permission when flashing, refer to the following:
sudo usermod -a -G dialout $USER
# Log out and log back inFlash Fails/Device Not Found
If flashing fails due to the device not being found, refer to the following:
# Check if device is connected
# Check J-Link connection
JLinkExe # Should detect device (Linux)Board Not Found Error
If you encounter an error that the board is not found, refer to the following:
# List available boards
west boards
# Ensure you're using the correct board name
# For FRDM-RW612: frdm_rw612SR250 Firmware (FW) Version Error
While running the demo application, if you encounter the following error (shown below) in the logs, this indicates a mismatch between SR250 FW version and UWBIOT MW version.
Running the demo application uwbiot-top/demos/SR2xx/demo_sr2xx_fw_update will allow SR250 FW to update.
Something went wrong! Please try again.