GoldBox 3 for Fast Vehicle Networks

Last Modified: 2023-02-23 12:39:00Supports GoldBox 3 Vehicle Networking Development Platform

1. Out of the Box

1.1 Get to Know the S32G-VNP-GLDBOX-3 Board for Vehicle Networking

GLDBOX3+RDB3

GLDBOX3+RDB3

1.2 Main Hardware Components

RDB3-GOLDBOX-COMPONENTS

2. Get Software

Learn how to use the Automotive Software Package Manager

2.1 Install a Terminal Emulator for Console

Install any terminal emulator familiar to you, such as Tera Term, Putty and other.

We recommend to use the Tera Term 2.3. Tera Term is open source free software terminal emulator supporting UTF-8 protocol. Now TTSSH supports SSH2 protocol (original version supports SSH1).

Download Tera Term

2.2 Install FTDI CDM WHQL Driver

FTDI CDM v2.12.28 WHQL driver for serial configuration from FTDI chip.

Download FTDI CDM driver

3. Plug It In

3.1 Plug in the SD Card

The SD card has pre-loaded Linux BSP image in the factory, you just need to plug SD card into the respective slot in your NXP GoldBox.

3.2 Plug in the UART Cable

Use the Micro-AB interface of the UART cable to connect the NXP GoldBox UART0 port. Use the typeA interface of the UART cable to connect to the PC.

GS-S32G-VNP-GLDBOX_3.2

4. Run

4.1 Setup Console

  1. Open your terminal emulators for console
  2. Select the serial port to which can be found in “Device Manager” of the PC and click OK
  3. Go to Setupial Port select 115200 as the baud rate

4.2 Power On the S32G-VNP-GLDBOX-3

Connect 12V power supply to the 12V DC port on your GoldBox.

GS-S32G-VNP-GLDBOX_4.2

4.3 Run Linux BSP

The Linux BSP is automatically executed from the SD card.

The console display on Tera Term show the running logs of Linux BSP.

Integrate LLCE CAN/LIN MCAL Driver

High-level Code Structures

Providing an easy way to integrate Low Latency Communication Engine (LLCE) CAN/LIN MCAL driver into S32DS as LLCE 1.0.0 driver does not integrate to S32DS 3.4 environment.

The software package structure:

LLCE-CAN-LIN-MCAL-demo-01

Hardware and Software Requirements

Host PC with Windows OS with serial console
S32G-VNP-RDB2 REV C/D

-

LLCE demo code

DOWNLOAD LLCE DEMO CODE

Real-Time Drivers (RTD) 1.0.0

DOWNLOAD RTD

Low Latency Communication Engine (LLCE) 1.0.0

DOWNLOAD LLCE

S32 Design Studio for S32 Platform (Building LLCE project)

DOWNLOAD S32DS

S32 Design Studio for S32 Platform (MCAL configuration for LLCE)

GET EB tresos

S32G-VNP-RDB2 Connection

Plug LLCE CAN/LIN and UART0 connectors, also power your S32G-VNP-RDB2.

LLCE-CAN-LIN-MCAL-demo-02

Create a new project in S32DS

Set your S32G-VNP-RDB2 to serial boot mode by turning both SW9 [0:1] and SW10 [0:1] to OFF:OFF

Power the board on, and open the s32ft.exe flash tool under the S32DS 3.4 installation folder:

LLCE-CAN-LIN-MCAL-demo-19

Upload the LLCE_CAN_LIN_M7_0_IVT.bin into the QSPI NOR Flash by using Flash tool
Target : S32Gxxx. Algorithm: MX25UW51245G
COM: Please check the com number on the HOST PC for UART0

LLCE-CAN-LIN-MCAL-demo-20a

Click Upload target and algorithm to hardware to initialize the hardware.
Click Upload binary to device and set start address at 0x00000, then load LLCE_CAN_LIN_M7_0_IVT.bin into QSPI and click OK

LLCE-CAN-LIN-MCAL-demo-20b

Set your S32G-VNPRDB2 to QSPI boot mode by turning SW9 [0:1] to OFF:OFF and SW10 [0:1] to ON:OFF (for BOOT from RCON) plus SW4 [6:8] to OFF:OFF:OFF (to boot from QSPI Flash)

Connect LLCE CAN0 to LLCE CAN1 and connect LLCE LIN2 (leader) to LLCE LIN3 (follower)

Open serial console (e.g: Tera Term) for UART0 on Host PC, set bitrate as 9600.
Power on the board and wait for console printings:

LLCE-CAN-LIN-MCAL-demo-21

LCCE CAN/LIN test

PFE Ethernet Interface with LWIP and FreeRTOS

An example project that enable Packet Forwarding Engine (PFE) Ethernet interface with a lwIP (lightweight IP) stack and FreeRTOS on the S32G’s M7 core. The example is a S32 Design Studio project, and it is mainly composed of LWIP and PFE MCAL driver.

PFE-Ethernet-interface-01

Hardware and Software Requirements

Host PC with Windows OS with serial console
S32G-VNP-RDB2 REV C/D

-

PFE demo code

DOWNLOAD PFE DEMO CODE


Enabling PFE Ethernet Interface

Launch S32 Design Studio for S32 platform and import the example project using the Existing Projects into Workspace option:

PFE-Ethernet-interface-02

Once loaded, click the Build Project option. Get the results once the built is complete:

PFE-Ethernet-interface-03

Make and IVT image by selecting the dcd_sram_init.bin DCD file for clearing SRAM.

PFE-Ethernet-interface-04

Set RAM start pointer as 0x34000000 and RAM entry pointer as 0x34001000 for application boot image.
Then write a final blob image to the SD card for testing.

PFE-Ethernet-interface-05

S32G-VNP-RDB2 Setup for Testing

Connect corresponding ports according to which PFE interface is used, then power up the board for test.

PFE-Ethernet-interface-06

Do a ping test to confirm conection:

PFE-Ethernet-interface-07

Extract the serdes folder and add to project directory. Right click folder in Project Explorer and select Build path > Add to > Debug_RAM to include serdes source code to project:

PFE-Ethernet-interface-08

Change the initialization parameters of serdes according to board setup:

PFE-Ethernet-interface-09

Call serdes_init() before Eth_43_PFE_init()


  serdes_init();
  oal_mm_init(NULL);
  Eth_43_PFE_Init(NULL_PTR);
  

Linux BSP Running Logs


  U-Boot 2019.04+ga53a9fa1e9 (Aug 31 2020 - 05:07:39 +0000)

  CPU:    NXP S32G274A rev. 2.1.0
  Reset cause: Power-On Reset
  Model: NXP S32G27x
  Board:  NXP S32G274A-RDB
  DRAM:  512 MiB
  CA53 core 1 running.
  CA53 core 2 running.
  CA53 core 3 running.
  All (4) cores are up.
  MMC:   FSL_SDHC: 0
  Loading Environment from MMC... OK
  Using external clock for PCIe0
  Configuring PCIe0 as RootComplex(x2)
  Using external clock for PCIe1
  Frequency 125Mhz configured for PCIe1
  Configuring PCIe1 as SGMII(x2) [XPCS0 2.5G, XPCS1 OFF]
  PCIe0: Failed to get link up
  Pcie0: LINK_DBG_1: 0x00000000, LINK_DBG_2: 0x00000800 (expected 0x000000d1)
  DEBUG_R0: 0x0052a300, DEBUG_R1: 0x08200000
  PCIe1: Not configuring PCIe, PHY not configured
  In:    serial
  Out:   serial
  Err:   serial
  Net:   EQOS phy: rgmii fixed-link
                                  
  Warning: eth_eqos (eth0) using random MAC address - 8a:54:02:e5:1f:1a
  eth0: eth_eqos PFE: emac0: sgmii emac1: none emac2: rgmii
                                  
  Warning: eth_pfeng using MAC address from ROM
  , eth1: eth_pfeng
  Hit any key to stop autoboot:  0
  PFE: emac0: sgmii emac1: none emac2: rgmii
  PFE: emac0: sgmii emac1: none emac2: rgmii
  switch to partitions #0, OK
  mmc0 is current device
  9158664 bytes read in 400 ms (21.8 MiB/s)
  Booting from mmc ...
  9158664 bytes read in 385 ms (22.7 MiB/s)
  27786 bytes read in 7 ms (3.8 MiB/s)
  ## Flattened Device Tree blob at 83e00000
     Booting using the fdt blob at 0x83e00000
     Loading Device Tree to 000000009fafa000, end 000000009fb03c89 ... OK
  Reserving 2048k off the top of [c0000000-dfffffff] for protected RAM
  DT: Enabling PFE
  DT: Enabling PFE_EMAC_0
  DT: pfe0 set to 00:01:be:be:ef:11
  DT: Disabling PFE_EMAC_1
  DT: Enabling PFE_EMAC_2
  DT: pfe2 set to 00:01:be:be:ef:33
  DT: Enabling GMAC
                                  
  Starting kernel ...
                                  
  [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
  [    0.000000] Linux version 4.19.59-rt24+ged566620fe59 (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Tue Aug 25 10:01:34 UTC 2020
  [    0.000000] Machine model: Freescale S32G275
  [    0.000000] earlycon: linflex0 at MMIO 0x00000000401c8000 (options '115200n8')
  [    0.000000] bootconsole [linflex0] enabled
  [    0.000000] cma: Reserved 256 MiB at 0x00000000cfc00000
  [    0.000000] random: get_random_bytes called from start_kernel+0x94/0x3f0 with crng_init=0
  [    0.000000] percpu: Embedded 21 pages/cpu s48920 r8192 d28904 u86016
  [    0.000000] Detected VIPT I-cache on CPU0
  [    0.000000] CPU features: enabling workaround for ARM erratum 845719
  [    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
  [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 900415
  [    0.000000] Kernel command line: console=ttyLF0,115200 root=/dev/mmcblk0p2 rootwait rw earlycon nohz=off coherent_pool=64M
  [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
  [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
  [    0.000000] software IO TLB: mapped [mem 0xcbc00000-0xcfc00000] (64MB)
  [    0.000000] Memory: 3151736K/3651584K available (6078K kernel code, 368K rwdata, 2024K rodata, 448K init, 215K bss, 237704K reserved, 262144K cma-reserved)
  [    0.000000] rcu: Preemptible hierarchical RCU implementation.
  [    0.000000]  Tasks RCU enabled.
  [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
  [    0.000000] GICv3: Distributor has no Range Selector support
  [    0.000000] GICv3: no VLPI support, no direct LPI support
  [    0.000000] ITS: No ITS available, not enabling LPIs
  [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000050880000
  [    0.000000] arch_timer: cp15 timer(s) running at 5.00MHz (virt).
  [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x127350b88, max_idle_ns: 440795202120 ns
  [    0.000005] sched_clock: 56 bits at 5MHz, resolution 200ns, wraps every 4398046511100ns
  [    0.008351] Console: colour dummy device 80x25
  [    0.012468] Calibrating delay loop (skipped), value calculated using timer frequency.. 10.00 BogoMIPS (lpj=20000)
  [    0.022689] pid_max: default: 32768 minimum: 301
  [    0.027433] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
  [    0.033989] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
  [    0.065168] ASID allocator initialised with 32768 entries
  [    0.078243] rcu: Hierarchical SRCU implementation.
  [    0.106732] smp: Bringing up secondary CPUs ...
  [    0.151077] Detected VIPT I-cache on CPU1
  [    0.151111] GICv3: CPU1: found redistributor 1 region 0:0x00000000508a0000
  [    0.151147] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
  [    0.191123] Detected VIPT I-cache on CPU2
  [    0.191151] GICv3: CPU2: found redistributor 100 region 0:0x00000000508c0000
  [    0.191179] CPU2: Booted secondary processor 0x0000000100 [0x410fd034]
  [    0.231190] Detected VIPT I-cache on CPU3
  [    0.231209] GICv3: CPU3: found redistributor 101 region 0:0x00000000508e0000
  [    0.231225] CPU3: Booted secondary processor 0x0000000101 [0x410fd034]
  [    0.231310] smp: Brought up 1 node, 4 CPUs
  [    0.287500] SMP: Total of 4 processors activated.
  [    0.292184] CPU features: detected: GIC system register CPU interface
  [    0.298610] CPU features: detected: 32-bit EL0 Support
  [    0.306755] CPU: All CPU(s) started at EL1
  [    0.310521] alternatives: patching kernel code
  [    0.315555] devtmpfs: initialized
  [    0.322790] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
  [    0.332215] futex hash table entries: 1024 (order: 4, 65536 bytes)
  [    0.344747] pinctrl core: initialized pinctrl subsystem
  [    0.350441] NET: Registered protocol family 16
  [    0.355564] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____))
  [    0.392905] DMA: preallocated 65536 KiB pool for atomic allocations
  [    0.398961] Serial: AMBA PL011 UART driver
  [    0.418631] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
  [    0.430451] vgaarb: loaded
  [    0.433060] SCSI subsystem initialized
  [    0.436769] usbcore: registered new interface driver usbfs
  [    0.442312] usbcore: registered new interface driver hub
  [    0.447384] usbcore: registered new device driver usb
  [    0.453176] pps_core: LinuxPPS API ver. 1 registered
  [    0.457793] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
  [    0.467201] PTP clock support registered
  [    0.471596] clocksource: Switched to clocksource arch_sys_counter
  [    0.484113] NET: Registered protocol family 2
  [    0.488818] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes)
  [    0.496354] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
  [    0.503842] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
  [    0.510687] TCP: Hash tables configured (established 32768 bind 32768)
  [    0.517015] UDP hash table entries: 2048 (order: 4, 65536 bytes)
  [    0.522981] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
  [    0.529527] NET: Registered protocol family 1
  [    0.533974] RPC: Registered named UNIX socket transport module.
  [    0.539558] RPC: Registered udp transport module.
  [    0.544245] RPC: Registered tcp transport module.
  [    0.548927] RPC: Registered tcp NFSv4.1 backchannel transport module.
  [    0.555533] Unpacking initramfs...
  [    0.558752] Initramfs unpacking failed: junk in compressed archive
  [    0.608954] Freeing initrd memory: 98304K
  [    0.614005] workingset: timestamp_bits=62 max_order=20 bucket_order=0
  [    0.620989] fuse init (API version 7.27)
  [    0.625222] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 250)
  [    0.632285] io scheduler noop registered
  [    0.636187] io scheduler deadline registered
  [    0.640470] io scheduler cfq registered (default)
  [    0.645129] io scheduler mq-deadline registered
  [    0.649637] io scheduler kyber registered
  [    0.654050] s32g275-siul2-pinctrl 4009c240.siul2-pinctrl0: initialized s32 pinctrl driver
  [    0.662296] s32g275-siul2-pinctrl 44010400.siul2-pinctrl1: initialized s32 pinctrl driver
  [    0.677252] s32gen1-pcie 40400000.pcie: Configuring as RootComplex
  [    0.683162] s32gen1-pcie 40400000.pcie: Allocated line 0 for interrupt 66 (msi)
  [    0.690394] s32gen1-pcie 40400000.pcie: host bridge /pcie@40400000 ranges:
  [    0.697258] s32gen1-pcie 40400000.pcie:    IO 0x5800003000..0x5800012fff -> 0x00000000
  [    0.705159] s32gen1-pcie 40400000.pcie:   MEM 0x5800013000..0x5840012fff -> 0x00013000
  [    1.711594] s32gen1-pcie 40400000.pcie: Phy link never came up
  [    2.715593] s32gen1-pcie 40400000.pcie: Phy link never came up
  [    2.721209] s32gen1-pcie 40400000.pcie: PCI host bridge to bus 0000:00
  [    2.727606] pci_bus 0000:00: root bus resource [bus 00-ff]
  [    2.733071] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
  [    2.739231] pci_bus 0000:00: root bus resource [mem 0x5800013000-0x5840012fff] (bus address [0x00013000-0x40012fff])
  [    2.753103] pci 0000:00:00.0: BAR 0: assigned [mem 0x5800100000-0x58001fffff 64bit pref]
  [    2.760871] pci 0000:00:00.0: BAR 6: assigned [mem 0x5800020000-0x580002ffff pref]
  [    2.768409] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
  [    2.773976] pcieport 0000:00:00.0: Signaling PME with IRQ 92
  [    2.779439] pcieport 0000:00:00.0: AER enabled with IRQ 92
  [    2.785178] s32gen1-pcie 44100000.pcie: u-boot did not initialize PCIE PHY; is u-boot compiled with PCIE support?
  [    2.796282] 401c8000.serial: ttyLF0 at MMIO 0x401c8000 (irq = 30, base_baud = 7812500) is a FSL_LINFLEX
  [    2.807429] console [ttyLF0] enabled
  [    2.807429] console [ttyLF0] enabled
  [    2.814711] bootconsole [linflex0] disabled
  [    2.814711] bootconsole [linflex0] disabled
  [    2.823540] 401cc000.serial: ttyLF1 at MMIO 0x401cc000 (irq = 31, base_baud = 7812500) is a FSL_LINFLEX
  [    2.833381] 402bc000.serial: ttyLF2 at MMIO 0x402bc000 (irq = 57, base_baud = 7812500) is a FSL_LINFLEX
  [    2.847880] libphy: Fixed MDIO Bus: probed
  [    2.852463] vcan: Virtual CAN interface driver
  [    2.857005] slcan: serial line CAN interface driver
  [    2.861981] slcan: 10 dynamic interface channels.
  [    2.866780] CAN device driver interface
  [    2.871567] flexcan 401b4000.flexcan: device registered (reg_base=(____ptrval____), irq(s):
  [    2.880094] flexcan 401b4000.flexcan:  26
  [    2.884186] flexcan 401b4000.flexcan:  27
  [    2.888282] flexcan 401b4000.flexcan:  28
  [    2.892373] flexcan 401b4000.flexcan:  29
  [    2.896464] flexcan 401b4000.flexcan: )
  [    2.901043] flexcan 402a8000.flexcan: device registered (reg_base=(____ptrval____), irq(s):
  [    2.909570] flexcan 402a8000.flexcan:  49
  [    2.913662] flexcan 402a8000.flexcan:  50
  [    2.917758] flexcan 402a8000.flexcan:  51
  [    2.921849] flexcan 402a8000.flexcan:  52
  [    2.925943] flexcan 402a8000.flexcan: )
  [    2.930403] flexcan 402b2000.flexcan: device registered (reg_base=(____ptrval____), irq(s):
  [    2.938925] flexcan 402b2000.flexcan:  53
  [    2.943017] flexcan 402b2000.flexcan:  54
  [    2.947112] flexcan 402b2000.flexcan:  55
  [    2.951202] flexcan 402b2000.flexcan:  56
  [    2.955296] flexcan 402b2000.flexcan: )
  [    2.959458] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
  [    2.965411] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
  [    2.972162] s32cc-dwmac 4033c000.ethernet: PTP uses main clock
  [    2.978119] s32cc-dwmac 4033c000.ethernet: no reset control found
  [    2.984348] s32cc-dwmac 4033c000.ethernet: phy mode set to RGMII
  [    2.990598] s32cc-dwmac 4033c000.ethernet: User ID: 0x10, Synopsys ID: 0x51
  [    2.997708] s32cc-dwmac 4033c000.ethernet:   DWMAC4/5
  [    3.002776] s32cc-dwmac 4033c000.ethernet: DMA HW capability register supported
  [    3.010231] s32cc-dwmac 4033c000.ethernet: RX Checksum Offload Engine supported
  [    3.017681] s32cc-dwmac 4033c000.ethernet: TX Checksum insertion supported
  [    3.024693] s32cc-dwmac 4033c000.ethernet: Wake-Up On Lan supported
  [    3.031111] s32cc-dwmac 4033c000.ethernet: Enabled workarounds for s32g274a platform
  [    3.039012] s32cc-dwmac 4033c000.ethernet: Enable RX Mitigation via HW Watchdog Timer
  [    3.047005] s32cc-dwmac 4033c000.ethernet (unnamed net_device) (uninitialized): device MAC address b2:87:c5:05:03:51
  [    3.057732] s32cc-dwmac 4033c000.ethernet: Enabling HW TC (entries=256, max_off=256)
  [    3.065723] libphy: stmmac: probed
  [    3.069942] mdio_bus stmmac-0: MDIO device at address 4 is missing.
  [    3.076566] mdio_bus stmmac-0: MDIO device at address 5 is missing.
  [    3.083183] mdio_bus stmmac-0: MDIO device at address 6 is missing.
  [    3.089805] mdio_bus stmmac-0: MDIO device at address 7 is missing.
  [    3.096702] usbcore: registered new interface driver asix
  [    3.102259] usbcore: registered new interface driver ax88179_178a
  [    3.108505] usbcore: registered new interface driver cdc_ether
  [    3.114488] usbcore: registered new interface driver net1080
  [    3.120294] usbcore: registered new interface driver cdc_subset
  [    3.126368] usbcore: registered new interface driver zaurus
  [    3.132096] usbcore: registered new interface driver cdc_ncm
  [    3.137903] usbcore: registered new interface driver qmi_wwan
  [    3.143961] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
  [    3.150624] ehci-pci: EHCI PCI platform driver
  [    3.155231] usbcore: registered new interface driver cdc_wdm
  [    3.161037] usbcore: registered new interface driver uas
  [    3.166502] usbcore: registered new interface driver usb-storage
  [    3.172716] usbcore: registered new interface driver option
  [    3.178429] usbserial: USB Serial support registered for GSM modem (1-port)
  [    3.199421] ci_hdrc ci_hdrc.0: EHCI Host Controller
  [    3.204545] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
  [    3.231610] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
  [    3.237248] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
  [    3.245680] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
  [    3.253045] usb usb1: Product: EHCI Host Controller
  [    3.258024] usb usb1: Manufacturer: Linux 4.19.59-rt24+ged566620fe59 ehci_hcd
  [    3.265299] usb usb1: SerialNumber: ci_hdrc.0
  [    3.270158] hub 1-0:1.0: USB hub found
  [    3.274009] hub 1-0:1.0: 1 port detected
  [    3.279363] s32gen1-rtc 40060000.rtc: rtc core: registered s32gen1_rtc as rtc0
  [    3.287677] sdhci: Secure Digital Host Controller Interface driver
  [    3.293980] sdhci: Copyright(c) Pierre Ossman
  [    3.298424] sdhci-pltfm: SDHCI platform and OF driver helper
  [    3.335639] mmc0: SDHCI controller on 402f0000.usdhc [402f0000.usdhc] using ADMA
  [    3.343511] usbcore: registered new interface driver usbhid
  [    3.350217] usbhid: USB HID core driver
  [    3.354483] NET: Registered protocol family 10
  [    3.360292] Segment Routing with IPv6
  [    3.364089] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
  [    3.370606] NET: Registered protocol family 17
  [    3.375154] can: controller area network core (rev 20170425 abi 9)
  [    3.381881] NET: Registered protocol family 29
  [    3.386451] can: raw protocol (rev 20170425)
  [    3.390809] can: broadcast manager protocol (rev 20170425 t)
  [    3.396588] can: netlink gateway (rev 20170425) max_hops=1
  [    3.396646] mmc0: new high speed SDHC card at address 5048
  [    3.408886] mmcblk0: mmc0:5048 SD16G 14.4 GiB
  [    3.413449] s32gen1-rtc 40060000.rtc: setting system clock to 2018-08-10 18:00:00 UTC (1533924000)
  [    3.424338]  mmcblk0: p1 p2
  [    3.432587] EXT4-fs (mmcblk0p2): mounting ext3 file system using the ext4 subsystem
  [    3.564012] EXT4-fs (mmcblk0p2): recovery complete
  [    3.572759] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
  [    3.580548] VFS: Mounted root (ext3 filesystem) on device 179:2.
  [    3.586575] devtmpfs: mounted
  [    3.589629] Freeing unused kernel memory: 448K
  [    3.593954] Run /sbin/init as init process
  INIT: version 2.88 booting
  [    3.712010] random: fast init done
  Starting udev
  [    3.999267] udevd[797]: starting version 3.2.8
  [    4.008995] random: udevd: uninitialized urandom read (16 bytes read)
  [    4.016322] random: udevd: uninitialized urandom read (16 bytes read)
  [    4.022469] random: udevd: uninitialized urandom read (16 bytes read)
  [    4.057252] udevd[798]: starting eudev-3.2.8
  [    4.608718] pfeng: loading out-of-tree module taints kernel.
  [    4.639285] pfeng 46000000.pfe: pfeng, ethernet driver loading ...
  [    4.645189] pfeng 46000000.pfe: Found reserved memory at p0x83400000 size 0xc00000
  [    4.652905] pfeng 46000000.pfe: Cbus addr 0x46000000 size 0x1000000
  [    4.658939] pfeng 46000000.pfe: firmware-name: s32g_pfe_class.fw
  [    4.665015] pfeng 46000000.pfe: HIF channel 0 in SC mode
  [    4.670227] pfeng 46000000.pfe: pfe0 linked to EMAC 0
  [    4.675259] pfeng 46000000.pfe: HIF channel 2 in SC mode
  [    4.680547] pfeng 46000000.pfe: pfe2 linked to EMAC 2
  [    4.685586] pfeng 46000000.pfe: TX clocks for interface pfe2 installed
  [    4.692086] pfeng 46000000.pfe: HIF channels mask: 0x0005
  [    4.697477] pfeng 46000000.pfe: Interface selected: EMAC0: 0x4 EMAC1: 0xffffffed EMAC2: 0x8
  [    4.718907] pfeng 46000000.pfe: Firmware: s32g_pfe_class.fw [size: 166088 bytes]
  [    4.725991] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:2718] INF: PFE CBUS p0x(____ptrval____) mapped @ v0x(____ptrval____)
  [    4.744578] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:2769] INF: Detected per block IRQ mode (S32G)
  [    4.756488] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:1381] INF: BMU1 buffer base: p0x(____ptrval____)
  [    4.770845] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:1428] INF: BMU2 buffer base: p0x(____ptrval____) (2097152 bytes)
  [    4.786777] [/usr/src/debug/pfe/0.8.0-r0/git/sw/oal/.//src/oal_irq_linux.c:156] INF: register IRQ 85 by name 'PFE BMU IRQ'
  [    4.797626] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_bmu_csr.c:117] INF: BMU_EMPTY_INT (BMU @ p0x(____ptrval____)). Pool ready.
  [    4.810671] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_bmu_csr.c:117] INF: BMU_EMPTY_INT (BMU @ p0x(____ptrval____)). Pool ready.
  [    4.894305] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:1779] INF: Firmware .elf detected
  [    4.905177] [/usr/src/debug/pfe/0.8.0-r0/git/sw/elf/src/elf.c:1379] INF: ELF_Open: File format: Elf32
  [    4.914375] [/usr/src/debug/pfe/0.8.0-r0/git/sw/elf/src/elf.c:1380] INF: ELF_Open: File endian: Alien (Big)
  [    4.924123] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:1788] INF: Uploading CLASS firmware
  [    4.935472] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1480] INF: pfe_ct.h file version"d6aa29e94e07a9cfbf1ccebb03994057"
  [    4.950316] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1480] INF: pfe_ct.h file version"d6aa29e94e07a9cfbf1ccebb03994057"
  [    4.964705] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1480] INF: pfe_ct.h file version"d6aa29e94e07a9cfbf1ccebb03994057"
  [    4.979092] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1480] INF: pfe_ct.h file version"d6aa29e94e07a9cfbf1ccebb03994057"
  [    4.993477] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1480] INF: pfe_ct.h file version"d6aa29e94e07a9cfbf1ccebb03994057"
  [    5.007866] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1480] INF: pfe_ct.h file version"d6aa29e94e07a9cfbf1ccebb03994057"
  [    5.022273] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1480] INF: pfe_ct.h file version"d6aa29e94e07a9cfbf1ccebb03994057"
  [    5.036663] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1480] INF: pfe_ct.h file version"d6aa29e94e07a9cfbf1ccebb03994057"
  [    5.051046] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1738] INF: [FW VERSION] 0.8.0, Build: Mar 31 2020, 11:41:35 (c768f3e), ID: 0x31454650
  [    5.064955] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_pe.c:1747] INF: [PE 0 MMAP]
  [    5.064955]                          DMEM Heap Base: 0x20001150 (11952 bytes)
  [    5.064955]                          PHY IF Base   : 0x20000aac (288 bytes)
  [    5.084143] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_emac_csr.c:308] INF: The PHY mode selection is done using a HW interface. See the 'phy_intf_sel' signal.
  [    5.100102] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_emac_csr.c:308] INF: The PHY mode selection is done using a HW interface. See the 'phy_intf_sel' signal.
  [    5.115924] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_emac_csr.c:308] INF: The PHY mode selection is done using a HW interface. See the 'phy_intf_sel' signal.
  [    5.131597] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:2149] INF: SAFETY instance created
  [    5.142830] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:2163] INF: Watchdog instance created
  [    5.155192] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:1913] INF: Routing table created, Hash Table @ p(____ptrval____), (____ptrval____) (65536 bytes)
  [    5.280190] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/src/pfe_l2br.c:643] INF: Fall-back bridge domain @ 0x20000a98 (class)
  [    5.293618] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_platform/hw/s32g/pfe_platform_master.c:2913] INF: Enabling the CLASS block
  [    5.364627] pfeng 46000000.pfe pfe0 (uninitialized): setting MAC addr: 00:01:be:be:ef:11
  [    5.372937] pfeng 46000000.pfe pfe0: registered
  [    5.400167] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_hif_drv/src/pfe_hif_drv_sc.c:320] INF: Attempt to register HIF client: pfe0
  [    5.411299] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_hif_drv/src/pfe_hif_drv_sc.c:385] INF: HIF client pfe0 id 0 registered
  [    5.422440] pfeng 46000000.pfe pfe0: Register HIF client pfe0 for logif (____ptrval____)
  [    5.430444] pfeng 46000000.pfe pfe2 (uninitialized): setting MAC addr: 00:01:be:be:ef:33
  [    5.438896] pfeng 46000000.pfe pfe2: registered
  [    5.468519] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_hif_drv/src/pfe_hif_drv_sc.c:320] INF: Attempt to register HIF client: pfe2
  [    5.479651] [/usr/src/debug/pfe/0.8.0-r0/git/sw/pfe_hif_drv/src/pfe_hif_drv_sc.c:385] INF: HIF client pfe2 id 1 registered
  [    5.490788] pfeng 46000000.pfe pfe2: Register HIF client pfe2 for logif (____ptrval____)
  [    5.498865] libphy: PFEng Ethernet MDIO: probed
  [    5.503428] mdio_bus PFEng Ethernet MDIO.pfe2: MDIO device at address 1 is missing.
  [    5.511055] mdio_bus PFEng Ethernet MDIO.pfe2: MDIO device at address 2 is missing.
  [    5.579136] loading NXP PHY driver: [autonomous mode]
  [    5.677591] sja1105pqrs spi1.0: Loading SJA1105P SPI driver
  [    5.682940] sja1105pqrs spi1.0: Detected device id is invalid: ffffffff
  [    5.689435] sja1105pqrs spi1.0: SJA1105P SPI Failed to read Device Id
  [    5.712578] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
  Fri Aug 28 01:21:01 UTC 2020
  [    5.995835] urandom_read: 3 callbacks suppressed
  [    5.995844] random: dd: uninitialized urandom read (512 bytes read)
  INIT: Entering runlevel: 5
  Configuring network interfaces... ifup: don't have all variables for eth0/inet
  Starting syslogd/klogd: done
  Starting random number generator daemon[    6.197407] random: rngd: uninitialized urandom read (4 bytes read)
  [    6.203438] random: rngd: uninitialized urandom read (4 bytes read)
  .
  [    6.211508] random: crng init done
  [    6.214604] random: 1 urandom warning(s) missed due to ratelimiting
  Starting OpenBSD Secure Shell server: sshd
  done.
                                  
  Auto Linux BSP 1.0 s32g274ardb /dev/ttyLF0
                                  
  s32g274ardb login:

Open S32G-VNP-GLDBOX-3 Enclosure

To open the S32G-VNP-GLDBOX-3 enclosure:

  1. Prepare the hex key provided in the kit package:

  2. GS-S32G-VNP-GLDBOX_PT-2a
  3. Find the screws at the bottom and use the hex key to unscrew it:

  4. GS-S32G-VNP-GLDBOX_PT-2b
  5. Pull up the bottom board:

  6. GS-S32G-VNP-GLDBOX_PT-2c
  7. Check the view of GoldBox 3 with open enclosure:

  8. GS-S32G-VNP-GLDBOX_PT-2d