NFC Eval Board Setup Guides

Last Modified: Dec 4, 2023Supports P3T1035xUK Arduino® Shield Evaluation Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get to Know the Hardware
  • 3

    Install Software
  • 4

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the P3T1035XUK-ARD board.

1.1 Kit Contents and Packing List

The P3T1035XUK-ARD kit contents include:

  • Assembled and tested evaluation board in an antistatic bag

1.2 Assumptions

Familiarity with the SPI-bus is helpful but not required.

1.3 Static Handling Requirements

1.4 Minimum System Requirements

  • PC Pentium processor (or equivalent)
  • One USB port (either 3.0 or 2.0 or 1.1 compatible)
  • Windows 7, 8, or 10
  • OM13089 MCU board (from www.nxp.com)

1.5 Power Requirements

The MIMXRT685-EVK MCU board obtains power from the PC USB port. Two USB parts can be connected to the MIMXRT685-EVK MCU board simultaneously. Use an external power supply option if exceeding the USB port current capabilities.

2. Get to Know the Hardware

2.1 Board Features

  • A complete evaluation platform for the P3T1035XUK I³C, I²C-bus, 0.5 °C accuracy, digital temperature sensor
  • Easy to use GUI based software demonstrates the capabilities of the P3T1035XUK
  • On-board temperature sensor for system thermal management experiments
  • Convenient test points for easy scope measurements and signal access
  • USB interface to the host PC
  • Power supply from USB port (x2) or external power supply can be used to power P3T1035XUK-ARD evaluation board

2.2 Board Description

The P3T1035XUK-ARD evaluation board features an I³C, I²C-bus, 0.5 °C accuracy, digital temperature sensor. A graphical interface allows the user to easily explore the different functions of the driver. The board can be connected in parallel with other I²C-bus demo boards to create an evaluation system

2.3 Board Components

Figure 1. P3T1035XUK-ARD evaluation board

Figure 1. P3T1035XUK-ARD evaluation board
Device Description Location
P3T1035XUK I³C, I²C-bus, 0.5 °C accuracy, digital temperature sensor U2
TPS71701DCKT Adjustable output voltage LDO U1
NTS0304EPWJ 4-bit dual supply translating transceiver U6
Green LED Power supply on LED D1

3. Install Software

3.1 Install P3T1035XUK-ARD Demo GUI

  • Double click on “setup.exe” to install P3T1035XUK-ARD demo GUI
  • Click “Next” button three times to complete installation GS-P3T1035XUK-ARD-IMG

3.2 Run Makalu6 Temperature Sensors GUI on Windows 7,8,10 PC

  1. Double click on “Makalu6 Temperature Sensors” icon to start GUI. GS-P3T1035XUK-ARD-IMG
  2. Select proper COM port (last COM port normally) and click “Connect” button to connect MIMXRT685-EVK board. GS-P3T1035XUK-ARD-IMG
  3. Use Setting tab to select I²C and I³C-bus speed, and click on the “Set Speed” button. GS-P3T1035XUK-ARD-IMG
  4. Click on “Scan” button to discover any NXP temperature sensor target address on the evaluation board. GS-P3T1035XUK-ARD-IMG
  5. Use Sensor Type to select which temperature sensor to be tested on the evaluation board. GS-P3T1035XUK-ARD-IMG
  6. Read/Write configuration register in the temperature sensor device control tab. GS-P3T1035XUK-ARD-IMG
  7. Read/Set THIGH (high limit) and TLOW (low limit) registers in the temperature sensor device control tab. GS-P3T1035XUK-ARD-IMG
  8. Perform one-shot or polling temperature read in the temperature sensor device control tab. GS-P3T1035XUK-ARD-IMG
  9. Read internal registers into a file or read a file into the internal registers in the in the temperature sensor device control tab. GS-P3T1035XUK-ARD-IMG
  10. Perform I³C general tests in the I³C tab. GS-P3T1035XUK-ARD-IMG
  11. Perform I²C general tests in the I²C tab. GS-P3T1035XUK-ARD-IMG

4. Configure Hardware

4.1 Configure the Hardware

P3T1035XUK-ARD EV board and MIMXRT685-EVK MCU board connection

P3T1035XUK-ARD evaluation board is connected to the MIMXRT685-EVK MCU board using four connectors (J1/J2/J3/J4 on P3T1035XUK-ARD board and J27/J28/J29/J30 on MIMXRT685-EVK board) for I²C-bus and power supply, and one connector (J9 on P3T1035XUK-ARD board and J18 on MIMXRT685-EVK board) for I³C-bus.

The MIMXRT685-EVK MCU board communicates with P3T1035XUK demo GUI through PC USB port and uses I²C or I³C-bus to communicate to P3T1035XUK.

Figure 1. P3T1035XUK-ARD evaluation board

Figure 1. P3T1035XUK-ARD evaluation board

Figure 2. MIMXRT685-EVKMCU evaluation board

Figure 2. MIMXRT685-EVKMCU evaluation board

Figure 3. P3T1035XUK-ARD evaluation board connecting to the MIMXRT685-EVK MCU board

Figure 3. P3T1035XUK-ARD evaluation board connecting to the MIMXRT685-EVK MCU board