PCA9420 Power Solutions Quick Guide

Last Modified: 2019-10-08 09:31:56Supports PCA9420UK-EVM

Contents of this document

  • 1

    Get Software
  • 2

    Build
  • 3

    Create

Get Software

1.1 PCA9420 GUI Software Installation

Unzip the provided PCA9420 Evaluation Kit GUI installation execution file, follow the step by step instruction on the screen.

During the installation process, the FTDI interface cable driver will also be installed, please refer to the screen capture for the reference. When correctly installed, the figure shown below on the right pop up on the screen. Click “Finish” button to continue.

PCA9420-IMG-1

Once the installation finished, the GUI will be automatically launched. Please note that since the standalone evaluation board has not been powered up, no communication channel is established between the computer (GUI) via the interface cable to the evaluation board, and it shows “Disconnected” at the bottom left of the GUI.

PCA9420-IMG-2

1.2 GUI Panels

When the GUI is launched, it looks for a PCA9420UK/PCA9420BS target board connected via the USB cable. If connected, the GUI panels display “Connected” on the bottom left.

Build

2.1 Board Description

Following figures describe the main elements on the board.

PCA9420-IMG-4

PCA9420-IMG-4

PCA9420-IMG-5

PCA9420-IMG-5

Number Name Description
1 USB Input USB power supply for the PCA9420UK
2 Logic pin for
MODESEL1 and 2
Logic high or low for MODESEL1 and 2 pins
3 VBAT-TS TS selection pin for either 10k or 100k
4 System Node Electronic load for system
5 U1 PCA9420UK PMIC
6 VBAT_BKUP Coil cell battery for back-up purpose
7 VBAT Connect a Li-ion battery cell
8 SW2_OUT BUCK2 output
9 SW1_OUT BUCK1 output
10 LDO2_OUT LDO2 output
11 LDO1_OUT LDO1 output
12 INT-PU Interrupt pull-up to either LDO2 output or an external
LDO output
13 PMIC-OUT All regulators’ output
14 SW1 Button connected to ON pin
15 I²C-PU Logic voltage selection for I²C
16 MODE-PU Logic voltage selection for MODESEL0 and 1 function
17 FTDI-CTRL I²C interface
18 VREG_IN Input selection for an external LDO between VBAT and
USB input

2.2 Jumper and Switch Definitions

Following figures show the location of jumpers and switch on the evaluation board.

PCA9420-IMG-6

PCA9420-IMG-6

PCA9420-IMG-7

PCA9420-IMG-7

The next table describes the function and settings for each jumper and switch.

Jumper/
Switch
Description Setting Connection/Result
SW1 ON Open Connect ON pin to ground when
pressed. Causes wake-up event of
PMIC
J5 FTDI-CTRL I²C interface connection with FTDI cable.
Orange color for SCL, Yellow and Green
color for SDA
J6 Voltage monitor Measure voltages for PCA9420UK
1: VBAT
2: BUCK2 output
3: BUCK1 output
4: LDO2 output
5: LDO1 output
Measure voltages for PCA9420BS
1: BUCK1 output
3: VBAT
5: LDO2 output
7: LDO1 output
9: BUCK2 output
J7 Logic configuration for
MODESEL0
[1-2] Logic high
[2-3] Logic low
J8 Pullup configuration for
MODE function
[1-2] Pullup to external LDO output
[2-3] Pullup to LDO2 output
J9 Logic configuration for
MODESEL1
[1-2] Logic high
[2-3] Logic low
J10 Pullup configuration for I/O
voltage
[1-2] Pullup to external LDO output
[2-3] Pullup to LDO2 output
J11 Logic voltage configuration
for INTB
[1-2] Pullup to external LDO output
[2-3] Pullup to LDO2 output
J13 VDD configuration for
external LDO
[1-2] Pullup to USB input
[2-3] Pullup to VBAT
J14 NTC configuration [1-2] Pulldown to 100k
[2-3] Pulldown to 10k

PCA9420-IMG-8

PCA9420-IMG-8

2.3 Connections

Connect wires on the following pins as shown in the next figure, and make sure the power supply is turned off during the wiring stage:

  • A Li-ion battery – Connect to VBAT test point
  • VIN Input – Powered by USB Micro B connector
  • FTDI Connector – Connect to FTDI USB to I²C cable (Yellow/Green to SDA, Orange to SCL, and Black to GND)

Create

3.1 The GUI Quick Guide

As shown in the next Figure, the GUI is a user-friendly tool which allows access to the on-chip registers to perform write/read commands manually or automatically (depending on GUI setting). Below is a quick guide of the key blocks that the GUI provides.

PCA9420-IMG-3

PCA9420-IMG-3

  1. Write All Registers: Click the write button on the GUI to perform a “write” command to all registers on PCA9420UK/PCA9420BS based on the current GUI setting. It is recommended to disable auto refresh before clicking the write all command, since some of settings might be updated by the auto refresh if turned on
  2. Read All Registers: Click the read button on the GUI to perform a “read” command and update all the register values reflected on the GUI
  3. Reset: N.A
  4. Functional View: By default, the GUI shows the “functional view”
  5. Register Map View: Click this button to select the Register map view
  6. Auto Refresh: Sets the auto refresh timer for the Interrupts and Status registers

    By choosing different options from the drop-down menu, the GUI performs the backend automatic read and refresh functions accordingly.

    • 1/second – Read all registers 1 time per second (1Hz)
    • 2/second – Read all registers 2 times per second (2Hz)
    • 4/second – Read all registers 4 times per second (4Hz)
    • Disabled – Disable the auto read
  7. Device information: It shows the device ID, device revision and its follower address information. Note that the GUI selects the follower address configured on the evaluation automatically
  8. Function Selection Tab: All function related registers are grouped into eight different tabs including "Top level control", "Interrupts", "Charging Control", "Charging Status", and "Group A-D setting". Click the tab to access the related registers
  9. Set/Read Setting: Set/Read the registers on the selected function tab
  10. Interrupts: Related to register 0x01 (TOP_INT), 0x02 (SUB_INT0), 0x04 (SUB_INT1) and 0x06 (SUB_INT2). When related events happen, the unmasked interrupt bits are set and the GUI highlights the checkboxes and changes the background color to RED
  11. Clear Interrupt: Related to register 0x02 (SUB_INT0), 0x04 (SUB_INT1) and 0x06 (SUB_INT2). The clear interrupt button is used to CLEAR the interrupt bits. In the case multiple interrupts bits are set at the same time, the button clears all set interrupts bits
  12. Regulator Status: Indicates the regulator status
  13. PMIC Status: Indicates current PMIC Status, including selected output group, regulators output voltage setting and the linear charging status
  14. Connections Status: When valid communication between GUI and the hardware is established, it shows "connected", otherwise it shows "disconnected". The cable used is also shown at the right side of the connection status bar