Quick Start Guide for S32K3X4EVB Board

Last Modified: 2021-10-06 10:29:00Supports S32K3x4-Q172 General-Purpose Development Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Software
  • 3

    Plug It In
  • 4

    Build, Run

1. Out of the Box

1.1 Get to Know the S32K344EVB-Q172 Evaluation Board

S32K3X4EVB-Q172 Evaluation board - Hero Specs

S32K3X4EVB-Q172 Evaluation board - Hero Specs

1.2 Block Diagram Features

S32K3X4EVB-Q172 Block Diagram

2. Get Software

You can watch the video or follow the below step-by-step guide to set up your S32K3X4EVB-Q172 Evaluation Board:

2.1 Get the Integrated Development Environment (IDE)

Download and Install S32 Design Studio IDE for S32 Platform.

Download the S32DS IDE

2.2 Install the S32K3xx Development Package

Go to Help → S32DS Extensions and Updates from the top menu to open the S32DS Extensions and Updates. Navigate to the S32K3xx development package and install it.

S32K3X4EVB-Q172-GS-S32DS-SW-IMG1

Continue with the installation of the Real-Time Drivers for S32K3xx:

S32K3X4EVB-Q172-GS-S32DS-SW-IMG2

2.3 Download and Install Elektrobit Tresos Studio and Real-Time Drivers (Only AUTOSAR® Users)

Download and install Elektrobit Tresos Studio / AUTOSAR Configuration Tool from S32K3 Standard Software Package.

S32DS Tresos Installer

Download and install the .exe file of the S32K3 Real-Time Drivers for Cortex-M from the S32K3 Standard Software Package.

S32K3X4EVB-Q172-GS-S32DS-RTD-IMG

The installer will ask for the EB Tresos installation directory on your disk, saving time in configuration.

S32K3X4EVB-Q172-GS-LINK-IMG

2.4 Get the Run-Time Debugging Tool

S32K3X4EVB-Q172 performs better when using the FreeMASTER Run-Time Debugging Tool.

Download

The FreeMASTER communication driver for S32K3 microcontrollers is also needed; download it from the Automotive SW - S32K3 - S32 FreeMASTER link in the S32K3 Standard Software Package.

3. Plug It In

3.1 Set Up Jumpers in the S32K3X4EVB-Q172 Evaluation Board

S32K3X4EVB-Q127 JUMPERS IMG

S32K3X4EVB-Q127 JUMPERS IMG
Default Jumper settings
Jumper State Notes
J1 CLOSED Disabled FS26 watchdog after power-up
J5 1-2 Select voltage level for FS26 DEBUG pin
J8 CLOSED External circuits powered from VDD_HV_B domain
J9 CLOSED External circuits powered from VDD_HV_A domain
J10 CLOSED The MCU peripherals powered from the VDD_HV_A domain
J15 CLOSED The MCU peripherals powered from the VDD_HV_B domain
J18 1-2 5 V for the VDD_HV_A domain
J19 1-2 3.3 V for the VDD_HV_B domain
J20 OPEN LIN1 Controller mode
J22 1-2 5 V from FS26 SBC
J24 OPEN LIN2 Controller mode
J26 CLOSED 3.3 V from FS26 SBC
J30 OPEN FS26 wake inputs
J31 1-2 V15 domain powered from FS26 SBC
J44 OPEN Onboard debugger UART pins

3.2 Plug in the Power Supply

Switch SW1 to the OFF position (fully to the right).

S32K3X4EVB-Q172-OFF-GS-IMG

Connect the 12 V power supply adapter and switch SW10 to the ON position (fully to the left).

S32K3X4EVB-Q172-ON-GS-IMG

This power-up procedure manages that SBC starts with the disabled watchdog. Four orange LEDs indicate the active 12 V, 5 V, 3.3 V and 1.5 V power supply domains.

3.3 Connect the Debugger Cable

Connect a micro-USB cable to the J40 connector to debug via the onboard S32K3 debugger.

S32K3X4EVB-Q172-USB-GS-IMG

Or use one of the available JTAG connectors to debug via the external S32K3 debugger.

S32K3X4EVB-Q172-JTAG-GS-IMG

4. Build, Run

Let's take your S32K3X4EVB-Q172 Evaluation Board for a test drive.

4.1 Create a S32DS Project from Example

Open S32DS and from the menu, go to: File → New → S32DS Project from Example. Select one of the RTD example codes. You may choose between examples with a high-level API or with a low-level API. For example: Port_example_K344.

S32DS Project from Example

4.2 Using the Configuration Tool

Double-click on the .mex project file.

S32K3X4EVB-Q172-GS-MEX-IMG

Please ensure that you configure the appropriate project and click on "Update Code" button for generating configuration files.

S32K3X4EVB-Q172-GS-UPDATE-CODE-IMG

4.3 Upload Software and Debug

Return back to the C/C++ perspective.

S32K3X4EVB-Q172-GS-CC-IMG

Use the Debug Configuration menu and select one of the predefined debug configurations for building and uploading software into MCU.

S32K3X4EVB-Q172-GS-DEBUG-IMG S32K3X4EVB-Q172-GS-DEBUG-MENU-IMG

The S32DS will switch into Debug perspective where you may let the code run.

S32K3X4EVB-Q172-GS-RUN-IMG

The red LED will now blink for approximately 10 seconds.