1
Plug It In2
Get Software3
Build, Run4
CreateSign in to save your progress. Don't have an account? Create one.

Go to Sensor Evaluation Boards and select the desired Demonstration Kit.
Something went wrong! Please try again.
Connect the Sensor Demonstration Kit to the PC via the USB cable between the OpenSDA USB port on the board and the USB connector on the PC.
Something went wrong! Please try again.
Kinetis Freedom MCU boards are supplied with OpenSDA firmware pre-loaded. For a smooth 'Out of Box Sensor Demonstration' with STB-CE, make sure that the latest version of the default OpenSDA bootloader and firmware application is on the Freedom development board. This allows debugging, flash programming and serial communication over a USB cable.
The default OpenSDA firmware for all Freedom based sensor demonstration kits used with STB-CE are as follows:
Obtain the latest OpenSDA drivers for FRDM boards from the link below.
Locate the section "Download – OpenSDA Bootloader and Application" and select your FRDM Board from the dropdown list. Strictly follow the provided instructions to program the board.
Note: For Windows 10 systems, the older versions of the OpenSDA drivers could get corrupted when the board is plugged on a Windows 10 machine. As a result, many boards might get not detected as an MSD or a COM port on Win 10. The latest versions of the OpenSDA software are compatible with Windows 10 and can be obtained from the link above. The current FRDM-K64F, FRDM-K22F, FRDM-KL25Z and RD-KL25-AGMP01 boards come with an older version of OpenSDA drivers from the factory and require a mandatory OpenSDA update.
Something went wrong! Please try again.
The output data from the provided example applications is provided over the MCU UART. This requires that the driver for the board’s virtual COM port is installed on the PC. The board MUST be plugged into the PC before the driver installer is run.
If you have not installed already an ARM IDE toolchain, download and install the Windows drivers corresponding to the default OpenSDA Application selected above:
Once the Windows Serial Port Drivers are installed on the PC, determine the port number of the board’s virtual COM port by opening the device manager and looking under the "Ports" group.
The demonstration kit is now ready to communicate with the PC.
Something went wrong! Please try again.
Available in both online and desktop editions, MCUXpresso SDK Builder creates a custom SDK for Kinetis, LPC and i.MXRT microcontrollers.
Something went wrong! Please try again.
This builds the SDK package for the demonstration kit. A request is sent to the build server. Requests for SDK packages are served in the order they are received. Notification is provided when the package is ready. The package is provided as a zip file. When notified, download the package (zip file) to the local PC
Note: ISSDK must be one of the Optional Middleware selections to develop an embedded sensor application. ISSDK provides the complete framework for sensor application development.
Something went wrong! Please try again.
NXP offers a complimentary toolchain called MCUXpresso IDE.
No problem. The MCUXpresso SDK includes support for other tools such as: IAR , Keil , command-line GCC .
Something went wrong! Please try again.
The sensor output of ISSDK example applications can be directly visualized on terminal applications like RealTerm , Tera Term , or PuTTY .
ISSDK also enables sensor visualization and data analysis on the FreeMASTER Sensor Tool.
Something went wrong! Please try again.
Explore the SDK Package.

Something went wrong! Please try again.
The CMSIS, devices, docs, rtos and tools directories are unchanged from the standard MCUXpresso SDK deployments. The ISSDK folder appears as frdmk22f_a8974 in the "/boards" directory.
As shown above, ISSDK provides out-of-box example projects for the FXLS8974CF sensor. In addition, ISSDK includes algorithms such as Pedometer. These sensor out-of-box example projects are ready to build and run with the FRDM-K22F-A8974 Demonstration Kit.
In addition, a new middleware folder for ISSDK is created containing the ISSDK drivers, algorithms and other support files as follows:
Something went wrong! Please try again.
If one or more of the demo applications sounds interesting, you're probably wanting to know how you can build and run yourself. Let us take "fxls8974cf_interrupt" out-of-box example available as part of the downloaded SDK package and try running it with our chosen IDE: MCUXpresso.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Note: Once, the ISSDK example is imported successfully, the MCUXpresso IDE automatically creates the corresponding standalone project in your workspace.
Something went wrong! Please try again.
For the firmware to be loaded successfully, review Steps 1.3 and 1.4 to be sure that the MCU board has the latest OpenSDA FW and the PC has the appropriate Windows Serial Drivers
Something went wrong! Please try again.
Terminal applications, such as Realterm, TeraTerm, or PuTTY, can be used to view the sensor output from the board. Refer to the readme.txt file in your workspace (standalone project) to configure the serial terminal correctly for successful communication with the Demonstration Kit. When the demonstration runs successfully, gyroscope output samples can be seen on the terminal window.
Something went wrong! Please try again.
The MCUXpresso IDE creates a standalone project folder for the chosen project under your workspace folder:
Something went wrong! Please try again.
Now, start your embedded application development, open the project from the folder with the desired IDE and start developing a custom application.
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with the IOT-SENSING-SDK on our community site.
Go to MCUXpresso Configuration Tools
Build FRDM-K22F-A8974 Kit Configuration
Install the Toolchain
Install Visualization