1
Out of Box2
Get Software3
Plug It InSign in to save your progress. Don't have an account? Create one.

Something went wrong! Please try again.
Something went wrong! Please try again.
Sign in at NXP.com with your credentials.
Open Automotive Software Package Manager and select S32K3 device - contains software also compatible with S32M27x.
Unfold the FRDM Automotive Board Installation Package bundle and check S32 Design Studio, Real-Time Drivers and FreeMASTER software. Other SW packages are optional.
Click on Generate Bundle Installer button at end of the page.
Follow the wizard instructions for Export Control and SW License Agreement (need to scroll whole text down before accepting). After that, you may close wizard window. Installer and Installer User Manual download will start automatically in a few moments.
Note: NXP Multi Installer is generated and works only for limited time window. Please start with installation right after installer download.
The FRDM Automotive Board Installation Package bundle allows to enable automatic installation and configuration sw without any interaction. That simplifies the installation procedure.
Something went wrong! Please try again.
Latest versions of the S32 Design Studio contain GCC toolchain only in version 11.4. For full compatibility with RTD, you need to install GCC also in version 10.2.
In S32 Design Studio, go to Help → S32DS Extensions and Updates from the top menu to open the S32DS Extensions and Updates dialogue where you may install it.
Something went wrong! Please try again.
Download updatesite file with FreeMASTER Communication Driver for S32M2.
In S32 Design Studio, go to Help → S32DS Extensions and Updates from the top menu to open the S32DS Extensions and Updates dialogue where you click on Add Update Sites and install it.
Note: Any other optional sw might be downloaded from S32M2 Standard Software Package or S32M2 Reference Software Package. Use the same way with Add Update Sites link or use drag and drop option - drag downloaded updatesite file and drop on S32DS Extensions and Updates menu. Added sw package will be also automatically selected for following installation.
Something went wrong! Please try again.
Download and install FreeMASTER application tool for real-time debugging.
Note: for this setup you may even skip the Lite service installation (for which the activation code is required).
Something went wrong! Please try again.
Download and install AMMCLib for S32M27x.
Note: Required is version 1.1.45 or newer
Note: If possible, install AMMCLib in their default path location for easy later path modification.
Something went wrong! Please try again.
Download and install FRDM-A-S32M276 motor control application software package.
Note: S32M27xEVB is an older name for FRDM-A-S32M276. SW installer keeps the S32M27xEVB name for backward compatibility.
Note: The installation process will also ask you to download the latest version of the Automotive Math and Motor Control Library (AMMCLib) set and installer will test minimum required version in next step.
Something went wrong! Please try again.
The recommended accessory kit for FRDM-A-S32M276 board is NXP BLDC_KIT (sw developed and tuned for given motor), however you may use any suitable 3 ph motor and 12 V power supply instead.
BLDC_KIT Content:
Table 1. FRDM-A-S32M276 Default Jumper Settings
| Jumper | State | Notes |
|---|---|---|
J1 |
CLOSED | VSUP_MCU is routed to VSUP input of MCU |
J2 |
1-2 | VBAT is routed to VSUP. Boost Converter disconnected |
J7 |
CLOSED | Power domains LED Indicators enabled |
J23 |
CLOSED | VDD_MCU is connected to the VDD_MCU_PERH |
J26 |
OPEN | [1] High Voltage Input, [2] GND |
J35 |
OPEN | [1] LPUART0_RX, [2] LPUART0_TX |
J51 |
CLOSED | LIN Commander* mode |
J55 |
OPEN | ADC Potentiometer disabled |
J61 |
CLOSED | VSUP is routed to VSUP_PERH |
J201 |
OPEN | Current shunt voltage, not populated |
*Master in the LIN standard document.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Let's take your FRDM-A-S32M276 motor control evaluation board for a test drive.
Select the appropriate PMSM or BLDC motor control application from the installed directory NXP\MC_DevKits\S32M27xEVB\sw
Note: S32M27xEVB is an older name for FRDM-A-S32M276. SW projects keep S32M27xEVB name for backward compatibility.
To import the installed application software project in the S32 Design Studio IDE for S32 Platform:
NXP\MC_DevKits\S32M27xEVB\sw and choose appropriate project and click OK. Then, click FinishNote: Check the box for the option Copy projects into workspace.
*.mex file to open the project configuration in Configuration Tool
Launch the FreeMASTER application.
To open the *.pmpx FreeMASTER project <selected project>\FreeMASTER_control, click File > Open Project.
Note: You can also start it by double clicking directly in the S32DS project folder.
To enable communication, in the FreeMASTER tool bar, click Go (or press Ctrl+G).
Successful communication displays in the status bar at the bottom as:
RS-232; port=COMn; speed = 115200
If you run FRDM-A-S32M276 sw on modified or own hardware platform, you may need to edit hardware scales and fault triggers. In the Motor Control Application Tuning (MCAT) Tool switch to Application Setup page and edit values on left side.
Once you finish, click on Save config to generate static configuration file. You may check file content at Output file page.
Now, repeat step from Upload Software and Debug section to build the project and upload the code into MCU.
Note: MCU will go to reset, FreeMASTER reconnecting might be needed (Ctrl+K, Ctrl+G).
In a case of motor change, you may benefit from new MCAT 2.0 motor parametrization and control loops autotuning features.
At Motor Parameters page, fill four basic motor parameters that cannot be detected automatically:
Click on Update target button and start the motor parameters estimation and automating tuning for control loops. Parameters are automatically updated typically in less than a minute.
For more information about the automatic motor parametrization and control loops autotuning please read AN15061 Application Note in S32M27xEVB\doc folder. Default path: c:\NXP\MC_DevKits\S32M27XEVB\doc\ApplicationNotes\AN15061 MCAT 2.0 - Motor Control Application Tuning Tool for PMSM FOC.pdf
Switch for example to Speed Loop page. Under Speed control tab, configure Required speed and turn on the motor drive.
Select one of predefined Scopes or Recorders in Project Tree to watch the application variables real-time.
For comfortable run-time debugging you may create or modify any of scopes or recorders.
In case of pending faults (fault state - fast blinking USER_LED01), click the CLEAR button at MCAT control tab or alternatively press simultaneously SW2 and SW3 on the board.
Click On/Off on the control bar or press SW2/SW3 on the board to initiate clockwise/counterclockwise spinning of the rotor. Run state is signalized by slowly blinking USER_LED01.
Modify Required speed field on the Speed control bar or change Speed Required in Variable Watch window. Alternatively control speed by pressing SW2 or SW3 switches on the board.
Stop the motor by clicking On/Off button on the MCAT control page, clear On/Off variable or simultaneously press and hold SW2 and SW3 on the FRDM-A-S32M276 board. Ready state is signalized by steadily light at both USER_LED01 and USER_LED02.
Note: For more information about MCAT tool please read AN15061 Application Note in S32M27xEVB\doc folder. Default path: c:\NXP\MC_DevKits\S32M27xEVB\doc\ApplicationNotes\AN15061 MCAT 2.0 - Motor Control Application Tuning Tool for PMSM FOC.pdf
Connect with other engineers and get expert advice on designing with the FRDM-A-S32M276 Reference Design Board using our community sites.
Select SW Packages from Automotive Software Package Manager
Add GCC Toolchain Version 10.2
Add FreeMASTER Communication Driver for S32M27x
Get FreeMASTER Application Tool for Real-Time Debugging
Get Automotive Math and Motor Control Library (AMMCLib) Set
Download the Development Kit Application Software
Check the Default Jumper Positions at the FRDM-A-S32M276 Evaluation Board
Plug the Motor
Optionally Plug the Encoder/HALL Sensors (Only for Sensor-Based SW Application
Plug the Power Supply and USB Debug Interface
Optionally to Previous Step Plug the JTAG Debug Interface and UART Interface