GS-IMX91QSB: Getting Started with IMX91QSB

Last Modified: Sep 2, 2025Supports i.MX 91 Quick Start Evaluation Kit

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Software
  • 3

    Build, Run
  • 4

    Developer Experience

1. Out of the Box

The following section lists the steps to boot the i.MX 91QSB.

The development kit contains:

  • i.MX 91 QSB along with M.2 module with NXP’s Wi-Fi 6 Tri-radio IW610
  • Power supply: USB-Type C 45 W power delivery supply, 5 V/3 A; 9 V/3 A; 15 V/3 A; 20 V/2.25 A supported
  • Cable: Assembly, USB 2.0, Type-C male to Type-A male
  • Software: Linux board support package (BSP) image programmed in embedded MultiMediaCard (eMMC)
  • Quick start guide

Get started developing your application on the i.MX 91 QSB with the out-of-the-box video. For more information, please see the i.MX 91 applications processor Documentation.

1.1 Get Familiar With the Board

GS-IMX91QSB-IMG1

GS-IMX91QSB

GS-IMX91QSB-IMG2

GS-IMX91QSB

1.2 Boot Option

The i.MX 91 QSB comes with a prebuilt NXP Linux binary demo image flashed on the eMMC. Without modifying the binary inside, booting from the eMMC provides a default system with certain features for building other applications on top of Linux.

To understand more about NXP's Embedded Linux®, continue reading the next sections.

1.3 Connect USB Debug Cable

Connect the supplied USB-Type C cable to the debug universal asynchronous receiver-transmitter (UART) port J11, then connect the other end of the cable to a host computer.

Four UART connections will appear on the host computer. The third port is for A55 core system debugging. If you are unfamiliar with terminal applications, please view one of the following tutorials before continuing to the next section: Minicom Tutorial, Tera Term Tutorial, PuTTY Tutorial.

To understand more about NXP's Embedded Linux®, continue reading the next sections.

1.4 Boot Switch Setup

SW3 [1-4] is the boot configuration switch. By default, the boot device is eMMC/uSDHC1.

1.5 Board Boot Up

  1. Connect the power supply cable to the power connector J13
  2. Power the board by flipping the switch SW5

The processor will start executing from the on-chip ROM code. With the default boot switch setup, the code reads the fuses to define the media where it is expected to have a bootable image. After it finds a bootable image, the U-Boot execution should begin automatically.

Information is printed in the serial console for the Arm® Cortex®-A55. If you do not stop the U-Boot process, it continues to boot the kernel.

Once the board boots up, the serial port begins to print log information to the PC as the board boots up. Congratulations, you are up and running.

2. Get Software

The i.MX Linux board support package (BSP) is a collection of binary files, source code and support files that are used to boot an Embedded Linux image on a specific i.MX development platform.

Current releases of Linux binary demo files can be found on Linux download page. Additional documentation is available in the i.MX Linux documentation bundle under the Linux sections of the i.MX Software and Development Tools.

2.1 Overview

i.MX 91 QSB support booting from eMMC and SD card.

This Getting Started guide only outlines a few methods of flashing the Linux BSP image to an SD card. Experienced Linux developers can explore other options if desired.

2.2 Download NXP Linux BSP Pre-Built Image

The latest prebuilt images for the i.MX 91 QSB are available on the Linux download page.

The prebuilt NXP Linux binary demo image provides a typical system and basic set of features for using and evaluating the processor. Without modifying the system, the users can evaluate hardware interfaces, test system-on-chip (SoC) features and run user space applications.

2.3 Burn NXP Linux BSP Image Using Universal Update Utility (UUU)

In addition to the connections from the "Out of the Box" section, connect the USB1 (J12) to the host machine using the proper USB cable.

Now turn off the board. Refer to the "1.4 Boot Switch setup" section and configure the board to boot in the serial download protocol (SDP) mode.

Depending on the OS used in the host machine, how the Linux BSP image transfers onto an SD card varies. Choose from the options below for detailed instructions:

3. Build, Run

The section provides, a brief guide on how to build a Yocto board support package (BSP) image for i.MX 91 QSB is introduced, along with how to add Matter support.

3.1 i.MX 91 QSB Yocto BSP

The i.MX 91 QSB BSP release is based on i.MX SW 2025 Q2 release with Yocto Project 5.2 (Walnascar). To build i.MX 91 QSB BSP image from source code, please first check i.MX Yocto Project user guide  to get familiar with Yocto project and Yocto build. Next, you will please follow the below steps below to build your image for i.MX 91 QSB.

  1. Download i.MX SW 2025 Q2 BSP release:
  2. $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-walnascar -m
    imx-6.12.20-2.0.0.xml
    $ repo sync
  3. Yocto project Setup:
  4. $ MACHINE=imx91-9x9-lpddr4-qsb DISTRO=fsl-imx-xwayland source imx-setup-release.sh -b
    bld-xwayland-imx91qsb
  5. Flashing SD card image:
  6. 1$ zstdcat imx-image-full-imx91qsb.rootfs.wic.zst | sudo dd of=/dev/sdx bs=1M && sync

    Or using uuu to burn image into SD card:

    $ uuu -b sd_all imx-image-full-imx91qsb.rootfs.wic.zst
  7. Change boot switch SW1[1:4] to “0011” to select SD card boot by inserting the SD card, then power up the i.MX 91 QSB

3.2 i.MX 91 QSB Matter Support

To include support for Matter for the i.MX94QSB, please follow below steps to include Matter layer into Yocto build.

  1. Download i.MX SW 2025 Q2 BSP release:
  2. $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-walnascar -m imx-6.12.20-2.0.0.xml
    $ repo sync
  3. Download i.MX Matter Yocto layer:
  4. 1$ cd ${MY_YOCTO}/sources/meta-nxp-connectivity
    $ git remote update
    $ git checkout imx_matter_2025_q2
  5. Yocto project Setup:
  6. 1$ cd ${MY_YOCTO}
    $ MACHINE=imx91qsb-iwxxx-matter DISTRO=fsl-imx-xwayland source sources/meta-nxp-connectivity/tools/imx-matter-setup.sh bld-xwayland-imx91qsb
  7. Build images:
  8. $ bitbake imx-image-multimedia

4. Developer Experience

To enable faster development for users of all skill levels, NXP provides extensive example applications that showcase the various features and capabilities of the platform.

4.1 Application Code Hub

The Application Code Hub (ACH)  repository enables engineers to easily find microcontroller and processor software examples, code snippets, application software packs and demos developed by NXP's in-house experts. This environment provides a quick, easy and consistent way to find microcontroller and processor applications.

The ACH provides filter and search options to quickly find specific applications. With the support of Git capabilities, you have an easy way to import and use applications within the user’s development environments.

Learn more about the Application Code Hub (ACH).

4.2 GoPoint for i.MX Applications Processors

The GoPoint for i.MX Application Processors is a user-friendly application that launches prebuilt applications packed with the Linux BSP, giving users an excellent out-of-the-box experience and hands-on experience with i.MX's system-on-chip (SoC) capabilities. GoPoint highlights advanced features while providing practical solutions for implementation, with source code and build recipes for the applications provided in GitHub .

Learn more about GoPoint for i.MX Application Processors

Debug Terminal Setup

Debug Terminal in Linux

Serial Communication Console Setup

On the command prompt of the Linux host machine, run the following command to determine the port number:

1$ ls /dev/ttyUSB*

The third port is for Arm® Cortex®-A55.

Debug Terminal in Windows

Serial Communication Console Setup

The FTDI USB-serial chip on i.MX 91 QSB enumerates 4 serial ports. Assume that the ports are COM11, COM12, COM13, COM14. The third port (COM13) is for the serial console communication from Arm® Cortex®-A55. The serial-to-USB drivers are available at FTD Chip Drivers .

Support

Troubleshooting

Security and Integrity

System security and integrity is always one of the most critical aspects to be considered in product development.

i.MX 91 QSB support secure boot feature and encrypted boot feature, helping to prevent unauthorized software execution during the device boot sequence and protect bootloader data from unauthorized access.

For more details of secure boot feature, please check application note Secure Boot on AHAB Supported Devices.

For more details of encrypted boot feature, please check application note i.MX Encrypted Boot on AHAB-Enabled Devices.

Fast Boot

In certain use cases, there is requirement for the device boot time, which means the device needs to complete booting in a given time limit.

To optimize the boot time, i.MX 91 QSB supports falcon mode in U-Boot. Falcon mode is a feature in U-Boot that enables fast booting by allowing SPL to directly start the Linux kernel. It completely skips the U-Boot loading and initialization, with the effect of reducing the time spent in the bootloader.

For how to enable falcon mode and further optimize boot time, please check Application Note Fast Boot on i.MX 8M and i.MX 9 Using Falcon Mode and Kernel Optimizations .