1
Plug It In2
Get Software3
Build and Run4
Create5
MCUXpresso Developer ExperienceSign in to save your progress. Don't have an account? Create one.

Let's take your RDM board for a test drive! You have the choice of watching the sequence in a short video or following the detailed actions listed below.
The MCXW236B-EVK-BB board comes along with the MCXW236BHN-RDM board which is pre-programmed with a health care IoT demo. This program serves as a sanity check to verify that the device is working as expected out of the box.
Something went wrong! Please try again.
Connect the MCXW236BHN-RDM board to the MCXW236B-EVK-BB by aligning the conector pins from the RDM board connector J6 and J7 to J8 and J12 respectively, before plugging the board make sure to set up the correct jumper settings on the MCXW236B-EVK-BB.
The image below serves a reference on the jumpers setting for a connection between the MCXW236BHN-RDM board to the MCXW236B-EVK-BB.
For more information on jumper settings for the MCXW236B-EVK-BB to the MCXW23xByy-RDM or MCXW23xAyy-RDM please refer to the [MCXW23-EVK-BB User Manual]
Something went wrong! Please try again.
Connect a type-C USB cable from connector J33 to a host computer or power supply to power up the board and run the demo program.
Follow the steps shown in the video above to connect and interact with the demo with the NXP's IoT ToolBox.
If a password is required to connect to the device use 999999.
Something went wrong! Please try again.
NXP offers a toolchain called MCUXpresso for VS Code. Please download MCUXpresso for VS Code v25.06 or newer.
Learn how to install VS Code for your host PC with the following tutorial.
Something went wrong! Please try again.
The NXP extension adds tools to help add software repositories into the Visual Studio Code workspace. The software repository can be provided from three sources:
This section will import the MCUXpresso SDK using the remote git repository option. For the remote git repository option follow these steps.
Something went wrong! Please try again.
The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and also provides pin and clock tools to generate initialization C code for custom board support. It is fully integrated as a part of MCUXpresso IDE and also as a separate tool if using a different IDE.
Click the Get MCUXpresso Config Tools below to get the Config Tools installer.
Something went wrong! Please try again.
The MCUXpresso Secure Provisioning (SEC) Tool is a GUI-based application provided to simplify the generation and provisioning of bootable executables on NXP MCU devices. We recommend all users to begin with the MCUXpresso Secure Provisioning (SEC) tool for trial run and mass production use. It supports secure programming and device provisioning on NXP's microcontrollers at the production stage.
After downloading the tool, you can find the user guide under the ‘Help’ tab. Follow the instructions for your board in the ‘Processor-specific workflow’ chapter.
Note: For advanced users that need a more customizable set-up we also offer a command-line tool that is useful when interfacing with a custom or partner programming tool. The Secure Provisioning SDK (SPSDK) is an open source development kit with its source code released on GitHub and PyPI.
Something went wrong! Please try again.
The following steps will guide you through the health care IoT demo application using MCUXpresso for vs code extension for the Cortex-M33 application. The MCUXpresso extension for vs code installation and the SDK for the MCXW-Series can be found at the Get Software section of this Getting Started guide.
The following tab will open on the editor screen
J33 ‘MCU-LINK’ port
SW3 label as "Wake_up" to start running the example
Something went wrong! Please try again.
The following steps will guide you through the manipulation of the general-purpose outputs. The example sets up a GPIO to set up a signal to toggle an LED.
Something went wrong! Please try again.
Note: Previously, you had to import an SDK project like shown in the previous step.
Note: If your imported example project does not have the .mex files present, please follow the [Working with MCUXpresso config tools guide]. The pins tool should now display the pin configuration for the led_blinky project
Something went wrong! Please try again.
SW4 buttonSW4 button, search for PIO0_18 and click the checkbox under the PIN column to enable it
Note: The clocks and other files may also be tagged as being updated since the header has been changed.


SW4 GPIO pin
SW4 the LED will toggle from its current stateSomething went wrong! Please try again.
Check out each of the following sections to learn about the ecosystem provided for flexible protyping and development. In the video below, we will introduce you to the FRDM platform, the full-featured EVK and the compatible shields for extended capabilities. In addition we will walk you through our Application Code Hub portal where we provide numerous application examples through NXP's Github.
For quick prototyping platforms, we offer both the low-cost FRDM platform and the full-featured EVK.
FRDM development boards come with standard form factor and headers, easy access to MCU I/Os, on-board MCU-Link debugger and a USB-C cable. Our full featured evaluation kits include extended I/O and interface access, extendibility with WiFi and additional MCU-Link features. There are also many compatible Click Boards and/or Arduino shields. For those that are supported with an Open CMSIS Pack examples may be available on ACH, but if not, many of them are easy to use via serial interface like I²C, SPI and UART, for which we provide drivers with examples in the MCUXpresso SDK.
Something went wrong! Please try again.
The Application Code Hub further enhances our MCUXpresso Developer Experience by giving developers an interactive dashboard to quickly locate software. Visit the ACH today to start exploring or discover additional details and benefits of the new interactive Application Code Hub.
Software accessible from Application Code Hub is located in NXP’s GitHub repository so it can be easily accessed and cloned from that location directly.
Something went wrong! Please try again.
The following demo walks us through importing a project from ACH using a system based on the FRDM platform with a motor control shield and a low cost LCD. Although your evaluation board may differ from this system, the following steps can be replicated and used for all supported platforms.
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with the MCXW236BHN-RDM on one of our community sites.