Getting Started with MCXW236BUK-RDM

Last Modified: Sep 16, 2025Supports MCXW236BUK-RDM Radio Device Module

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build and Run
  • 4

    Create
  • 5

    MCUXpresso Developer Experience

1. Plug It In

Let's take your EVK board for a test drive! You have the choice of watching the sequence in a short video or following the detailed actions listed below.

1.1 Get Familiar with the Board

The MCXW236B-EVK-BB board comes along with the MCXW236BUK-RDM board which is pre-programmed with a health care IoT demo. This program serves as a sanity check to verify that the device is working as expected out of the box.

Figure 1. MCXW23-EVK Callouts

Figure 1. MCXW23-EVK Callouts

1.2 Set Up the Boards

Connect the MCXW236BUK-RDM board to the MCXW236B-EVK-BB by aligning the conector pins from the RDM board connector J6 and J7 to J8 and J12 respectively, before plugging the board make sure to set up the correct jumper settings on the MCXW236B-EVK-BB.

The image below serves a reference on the jumpers setting for a connection between the MCXW236BUK-RDM board to the MCXW236B-EVK-BB.

Figure 2. MCXW23-EVK Callouts

Figure 2. MCXW23-EVK Callouts

For more information on jumper settings for the MCXW236B-EVK-BB to the MCXW23xByy-RDM or MCXW23xAyy-RDM please refer to the [MCXW23-EVK-BB User Manual]

1.3 Plug In the Board

Connect a type-C USB cable from connector J33 to a host computer or power supply to power up the board and run the demo program. Follow the steps shown in the video above to connect and interact with the demo with the NXP's IoT ToolBox.

If a password is required to connect to the device use 999999.

Figure 3. MCXW23-EVK Plug in the Board

Figure 3. MCXW23-EVK Plug in the Board

2. Get Software

2.1 Install Your Toolchain

NXP offers a toolchain called MCUXpresso for VS Code. Please download MCUXpresso for VS Code v25.06 or newer.

Visual Studio Code

Get VS Code.

Learn how to install VS Code for your host PC with the following tutorial.

2.2 Jump Start Your Design with the MCUXpresso SDK

The NXP extension adds tools to help add software repositories into the Visual Studio Code workspace. The software repository can be provided from three sources:

  • Remote git URL
  • NXP MCUXpresso SDK archive file
  • Existing git folder

This section will import the MCUXpresso SDK using the remote git repository option. For the remote git repository option follow these steps.

  1. Click on the MCUXpresso extension Icon
  2. Click on the “QUICKSTART PANEL” tab and then click on the "Import repositoty" button. After pressing that button a new import window will appear on your IDE
  3. MCUXpresso SDK Step 1
  4. Select the “Remote” option to import the provided SDK files
  5. Browse to the Repository options by clicking on the arrow button and search for "MCUXpresso SDK - 24.12 or newer" option
  6. Browse to the Revision options by clicking on the arrow button and search for version "v25.09.00" or newer
  7. Browse to a folder to be a common “Destination” to store SDKs. (i.e. C:\VS_CODE_SDKs ) Enter a name for the new SDK, in this case \mcux_sdk_v25_09_00_pvw1
  8. Click on Import button and wait for the installation
  9. MCUXpresso SDK Step 2

2.3 MCUXpresso Config Tools

The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and also provides pin and clock tools to generate initialization C code for custom board support. It is fully integrated as a part of MCUXpresso IDE and also as a separate tool if using a different IDE.

Click the Get MCUXpresso Config Tools below to get the Config Tools installer.

MCUXpresso Config Tools

Get MCUXpresso Config Tools

2.4 Programming and Provisioning Tools

The MCUXpresso Secure Provisioning (SEC) Tool is a GUI-based application provided to simplify the generation and provisioning of bootable executables on NXP MCU devices. We recommend all users to begin with the MCUXpresso Secure Provisioning (SEC) tool for trial run and mass production use. It supports secure programming and device provisioning on NXP's microcontrollers at the production stage.

After downloading the tool, you can find the user guide under the ‘Help’ tab. Follow the instructions for your board in the ‘Processor-specific workflow’ chapter.

SEC

SEC Installation

3. Build and Run

The following steps will guide you through the health care IoT demo application using MCUXpresso for vs code extension for the Cortex-M33 application. The MCUXpresso extension for vs code installation and the SDK for the MCXW-Series can be found at the Get Software section of this Getting Started guide.

3.1 Build and Flash an Application Using MCUXpresso IDE

  1. Find the activity bar in the left-hand bar and click it to open it. Once it's open go to the explorer and open the project tab
  2. Build and flash application using MCUXpresso IDE - fig 1
  3. Then click Import example from repository Build and flash application using MCUXpresso IDE - fig 2
The following tab will open on the editor screen
  4. Build and flash application using MCUXpresso IDE - fig 3
  5. Click the arrow button on the repository tab to choose your previously downloaded the MCXW-Series board SDK to select an example that can run on that board, and then click Next
  6. Build and flash application using MCUXpresso IDE - fig 4
  7. Select the toolchain according to the SDK version, both SDK and toolchain must match to avoid problems. Then select the board
  8. Build and flash application using MCUXpresso IDE - fig 5
  9. Use the arrow button to expand the Template tab, and then select the "wireless_examples/reference_design/health_care_iot_peripheral_bm" to use it as a template for the project. Then, click import button
  10. Build and flash application using MCUXpresso IDE - fig 6
  11. Expand the project, go to the MCU tab and expand it. Search for the Package tab and make sure Package: MCXW236BIHNAR is selected, if not in the MCU tab in the right end click the "Change package" icon button and set MCXW236BIHNAR for the project
  12. Build and flash application using MCUXpresso IDE - fig 7
  13. Select the project and build it by either clicking the “build icon” in the shortcuts provided above or by doing a right click and select the "Build" option
  14. Build and flash application using MCUXpresso IDE - fig 8
  15. The project should build without presenting any errors or warnings in the console
  16. Build and flash application using MCUXpresso IDE - fig 9
  17. Connect the board to your computer with the micro-USB to J33 ‘MCU-LINK’ port
  18. Build and flash application using MCUXpresso IDE - fig 10
  19. Download the application to your board by either clicking the “debug” icon above or by doing a right click and select the "Debug" option
  20. Build and flash application using MCUXpresso IDE - fig 11
  21. Open up a serial terminal to be able to see the application’s output. Select the port corresponding to the MCULINK probe to your board “MCULink-VCOM” window. Set your terminal to baud rate or speed to "460800", 8-bit data, no parity and 1 stop bit and connect to that port
  22. Build and flash application using MCUXpresso IDE - fig 12
Build and flash application using MCUXpresso IDE - fig 13
  23. Run the application by pressing the “run” icon. See the output printed on the terminal
  24. Build and flash application using MCUXpresso IDE - fig 14
Build and flash application using MCUXpresso IDE - fig 15
  25. Press on board SW3 label as "Wake_up" to start running the example
  26. Build and flash application using MCUXpresso IDE - fig 16
  27. See the output printed on the terminal
  28. Build and flash application using MCUXpresso IDE - fig 17
  29. You can connect the demo to the IoT Toolbox app by following the steps shown in the Plug it in video from section 1

4. Create

4.1 Clone an Example Project from MCUXpresso for VS Code

The following steps will guide you through the manipulation of the general-purpose outputs. The example sets up a GPIO to set up a signal to toggle an LED.

  1. Find the activity bar in the left-hand bar and click it to open it. Once it's open you can either go to the explorer and open the project tab and click import example application from an imported repository, click the import repository icon or go to the Quickstart panel and click Import Example from Repository button
  2. Modify an Example Project from MCUXpresso for VS Code - fig 1
  3. Click and select the repository for the MCXW23-EVK board to select the corresponding toolchain that matches the SDK version
  4. Modify an Example Project from MCUXpresso for VS Code - fig 2
  5. Use the arrow button to expand the template category, then search for "demo_apps/led_blinky_lpc", click the line that matches this text to select it. Then, click import
  6. Modify an Example Project from MCUXpresso for VS Code - fig 3
  7. Expand the "mcxw23evk_led_blinky_lpc" project, go to the MCU tab and expand it. Search for the Package tab and make sure Package: MCXW236BIHNAR is selected, if not in the MCU tab in the right end click the "Change package" icon button and set MCXW236BIHNAR for the project
  8. Modify an Example Project from MCUXpresso for VS Code - fig 4
  9. Click the “mcxw23evk_led_blinky_lpc” project in the side bar and, compile, and run the demo as described in the previous section
  10. Modify an Example Project from MCUXpresso for VS Code - fig 5
  11. You should see the RED LED changing back and forth
  12. Terminate the debug session

4.2 Use MCUXpresso IDE Pins Tools

  1. Open the pins tool by right clicking the project, then selecting the selecting “Open with MCUXpressoConfigTools” button
  2. Use MCUXpresso IDE Pins Tools - fig 1
  3. The pins tool should now display the start developing window, now you should search for the .mex file of the project and select it. If this file is included in your project you can search search for it in the path/mcux/mcuxsdk\examples\_boards\mcxw23evk\\ For example, in the picture I've selected from my sdk path on the type of project the as project to select the .mex file, this file has the configuration for the project and then click next and finish
  4. Use MCUXpresso IDE Pins Tools - fig 2
  5. Use MCUXpresso IDE Pins Tools - fig 3

4.3 Use MCUXpresso Config Tools

  1. We’ll use MCUXpresso Config tools to edit the pin configuration for this project, in th "Pins" view deselect “Show dedicated pins” and “Show no routed pins” checkboxes to see only the routed pins. Routed pins have a check in a green box next to the pin name. The functions selected for each routed pin are highlighted in green
  2. Use MCUXpresso Config tools - fig 1
  3. In the current configuration, PIO0_19 is routed as the output of the GPIO to toggle the LED. Let’s add the pin configuration to enable the SW4 button
  4. Select “Show no routed pins” to see the other options. To enable the SW4 button, search for PIO0_18 and click the checkbox under the PIN column to enable it
  5. Use MCUXpresso Config tools - fig 2
Use MCUXpresso Config tools - fig 3
  6. After clicking the checkbox, this window will appear, then type on the searchbox "gpio" and select the "GPIO:PIO0,18" and click done
  7. Use MCUXpresso Config tools - fig 4
  8. Check the pin configuration to be set as an output in the “Routing Details” window
  9. Use MCUXpresso Config tools - fig 5
  10. Now, it’s time to implement these changes into the project by exporting the new updated pin_mux.c and pin_mux.h files that are generated by the Pins tool. Click Update Project in the menu bar
  11. Use MCUXpresso Config tools - fig 6
  12. Now, save your file to proceed to export the new configuration files. Press either CTRL+S or press on the file tab and click save
  13. The screen that pops up will show the files that are changing and you can click “diff” to see the difference between the current file and the new file generated by the Pins tool
  14. Click on “OK” to overwrite the new files into your project
  15. Use MCUXpresso Config tools - fig 7
  16. In this step you replace the new generated files from the tool created inside a new folder called "board"—located in your examples path as shown in previous steps— where you can copy the files from this folder into the original example folder where to change the project files to the new version
  17. Use MCUXpresso Config tools - fig 8
Use MCUXpresso Config tools - fig 9
Use MCUXpresso Config tools - fig 10
  18. Let’s add some additional code to the example. Open the led_blinky.c file and add the following macros to control and read the SW4 GPIO pin
  19. Use MCUXpresso Config tools - fig 11
  20. Add the two variables to stare the sw state values, those will be used later to control the led state
  21. Use MCUXpresso Config tools - fig 12
  22. In the last while loop, add these modifications
  23. Use MCUXpresso Config tools - fig 13
  24. Build and download the project as done in the previous section
  25. Run the application. Now, every time you press the SW4 the LED will toggle from its current state
  26. Terminate the debug session

5. MCUXpresso Developer Experience

Check out each of the following sections to learn about the ecosystem provided for flexible protyping and development. In the video below, we will introduce you to the FRDM platform, the full-featured EVK and the compatible shields for extended capabilities. In addition we will walk you through our Application Code Hub portal where we provide numerous application examples through NXP's Github.

5.1 FRDM Platform, Full Feature EVK and Shields

For quick prototyping platforms, we offer both the low-cost FRDM platform and the full-featured EVK.

FRDM development boards come with standard form factor and headers, easy access to MCU I/Os, on-board MCU-Link debugger and a USB-C cable. Our full featured evaluation kits include extended I/O and interface access, extendibility with WiFi and additional MCU-Link features. There are also many compatible Click Boards and/or Arduino shields. For those that are supported with an Open CMSIS Pack examples may be available on ACH, but if not, many of them are easy to use via serial interface like I²C, SPI and UART, for which we provide drivers with examples in the MCUXpresso SDK.

5.2 Application Code Hub

The Application Code Hub further enhances our MCUXpresso Developer Experience by giving developers an interactive dashboard to quickly locate software. Visit the ACH  today to start exploring or discover additional details and benefits of the new interactive Application Code Hub.

Software accessible from Application Code Hub is located in NXP’s GitHub repository  so it can be easily accessed and cloned from that location directly.

5.3 Demo Walkthrough

The following demo walks us through importing a project from ACH using a system based on the FRDM platform with a motor control shield and a low cost LCD. Although your evaluation board may differ from this system, the following steps can be replicated and used for all supported platforms.

Support

Support

Connect with other engineers and get expert advice on designing with the MCXW236B-EVK on one of our community sites.