Getting Started with PF09 Power Management IC Evaluation Board.

Last Modified: Jan 7, 2026Supports PF09 Evaluation Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get to Know the Hardware
  • 3

    Configure the Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the KITPF09FRDMEVM board.

1.1 Kit Contents/Packing List

Working with the KITPF09FRDMEVB requires the kit contents, more hardware and a Windows PC workstation with installed software.

The kit contents include:

  • Assembled and tested evaluation board with a preprogrammed KL25Z microcontroller in an antistatic bag
  • 3.0 ft USB-STD A to USB-B-micro cable
  • Six Phoenix connectors, two positions, straight, 10 mm
  • Jumpers mounted on board
  • Quick start guide

1.2 Additional Hardware

In addition to the kit contents, the following hardware is necessary or beneficial when working with this board:

  • Power supply capable of providing 5 V

1.3 Minimum System Requirements

This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board:

  • USB-enabled computer with Windows 7 or Windows 10
  • FTDI USB serial port driver (for FT230X basic UART device)

1.4 Software

Installing software is necessary to work with the KITPF09FRDMEVB evaluation board. All listed software is available on the evaluation board's information page at PF09: 9-Channel PMIC for High-Performance Applications, ASIL D and SIL 2 or from the provided link.

2. Get to Know the Hardware

2.1 Board Features

  • Phoenix (10 mm) male connector or jack connector for power supply input
  • Phoenix (10 mm) male connectors for PMIC switcher outputs
  • Header connectors for I/O configuration
  • Selectable power input for programming
  • Access pin connectors for accessing inputs and outputs
  • Indicator LEDs red and green LEDs to indicate signal or regulator status
  • Blue LED to indicate that the OTP 8 V burning voltage is set
  • Advanced system monitoring via the KL25Z MCU
  • Embedded USB to I²C protocol for easy connection to the software GUI through the KL25Z MCU

2.2 Board Description

The hardware of the kit consists of the KITPF09FRDMEVB program board embedded with a KL25Z microcontroller, and the USB cable required to connect the board to the PC.

The KITPF09FRDMEVB valuation board features a socket that allows the user to fuse an individual PF09 Family using the device’s two time programmable (OTP) feature without extra tools. Connectors, jumpers and switches on the board can be used to configure an evaluation environment that meets specific design requirements. The board also contains LEDs and test points that provide a means of monitoring performance in real time. An emulation mode allows the user to test as many configurations as needed before programming the part.

The KL25Z is soldered on the bottom side of the KITPF09FRDMEVB board. The role of the KL25Z is to manage I²C communication between the KITPF09FRDMEVB board and the GUI installed on the PC. The KL25Z draws power either from the USB cable connected to the PC or from the battery supply (when not connected to the GUI).

Overview Diagram of Communication Between PF09 and NXP GUI

Overview Diagram of Communication Between PF09 and NXP GUI

2.3 Board Components

Figure 2 shows the placement of connectors, configuration headers and signaling LEDs. For information on the default jumper and switch configuration for PF09, see Section 3.

Location of Key KITPF09FRDMEVB – Components

Location of Key KITPF09FRDMEVB – Components

3. Configure the Hardware

3.1 Configure the Hardware

The procedure for setting up the KITPF09FRDMEVB program board is as follows:

  1. Make sure that the board has the jumpers and switches configured in their default positions. The default debug configuration enables the board to be fully controlled by the KL25Z MCU (via I²C) and the GUI. Section 4.4 shows the default jumpers and switches configuration for the PF09 Family.
  2. Connect the power supply to VIN-J47 (Phoenix connector - 10 mm). The power supply should be set to a nominal value of 5 V.
  3. Make sure the USB cable between the board and the PC is securely connected. This connection is critical because the USB port serves as a communication channel between the PC and the KL25Z MCU onboard, and also provides voltages and references to some onboard circuits.

The default debug configuration enables the board to be fully controlled by the KL25Z MCU (via I²C) and the GUI. Figure 2 shows the default jumper and switch configuration for PF09. See below for PF09 default jumpers and switches configuration.

Reference Description Settings for Configuration External Configuration
J1 PWRON pullup voltage selection Pins: 1 to 2 VIN Open
Pins: 2 to 3 VAON Open
J2 VDDOTP connection Pins: 1 to 2 VDIG Open
Pins: 2 to 3 VDDOTP_BST Connected
J9 FCCU0 input level connection Pins: 1 to 2 VDDIO ---
Pins: 2 to 3 GND ---
J10 FCCU1 input level connection Pins: 1 to 2 VDDIO ---
Pins: 2 to 3 GND ---
J20 Power on connection to interface system Pins: 1 to 2 Connected Connected
J24 Selection of external VDDIO voltage (1 to 2: 1.8 V <-> “2 to 3": 3.3 V) Pins: 1 to 2 1.8 V ---
Pins: 2 to 3 3.3 V Connected
J29 RSTB pullup to VDDIO, connect for operation Pins: 1 to 2 Connected Connected
J36 VDDIO power input injection Pins: 1 to 2 External Connected
Pins: 2 to 3 SW1 ---
J48 LDO1 Input voltage Pins: 1 to 2 VSW_IN Connected
Pins: 2 to 3 SW1_OUT ---
J49 LDO2 Input voltage Pins: 1 to 2 VSW_IN Connected
Pins: 2 to 3 SW1_OUT ---
J50 LDO3 Input voltage Pins: 1 to 2 VSW_IN Connected
Pins: 2 to 3 SW1_OUT ---
J54 USB Jumper. Used to connect to USB power. Open for using external power supply (VIN). Connect external power for correct operation Pins: 1 to 2 Used – USB power
Open – External power supply
Open
Reference Function Description
J39 SW2 output PMIC switcher 2 output voltage. Direct connection to PMIC pin
J40 SW3 output PMIC switcher 3 output voltage. Direct connection to PMIC pin
J41 SW4 output PMIC switcher 4 output voltage. Direct connection to PMIC pin
J42 SW5 output PMIC switcher 5 output voltage. Direct connection to PMIC pin
J43 SW1 output PMIC switcher 1 output voltage. Direct connection to PMIC pin
J47 VIN Input voltage supply can come from the power supply. Range from 3.3 V to 5.0 V; according to specification
Reference Function Description Color
BH1 GND Board grounds direct connection -4 easy access points Black
BH2
BH3
BH4
TP119 LDO1IN Monitoring point for the LDO1 input voltage Red
TP120 LDO2IN Monitoring point for the LDO2 input voltage Red
TP121 LDO3IN Monitoring point for the LDO3 input voltage Red
TP61 VLDO1 Monitoring point for the LDO1 output Red
TP60 VLDO2 Monitoring point for the LDO2 output Red
TP59 VLDO3 Monitoring point for the LDO3 output Red
TP15 VAON Monitoring point for the VAON output White
TP90 SW1 FB Monitoring point for the SW1 feedback White
TP86 SW2 FB Monitoring point for the SW2 feedback White
TP87 SW3 FB Monitoring point for the SW3 feedback White
TP91 SW4 FB Monitoring point for the SW4 feedback White
TP92 SW5 FB Monitoring point for the SW5 feedback White
TP78 VMON1 Monitoring point for the external monitor VMON1 Orange
TP79 VMON2 Monitoring point for the external monitor VMON2 Orange
TP65 XFAILB XFAILB PMIC access point - bidirectional pin White
TP57 GPIO1 GPIO1 access point - bidirectional pin White
TP20 GPIO2 GPIO2 access point - bidirectional pin White
TP56 GPIO3 GPIO3 access point - bidirectional pin White
TP8 GPIO4 GPIO4 access point - bidirectional pin White
TP4 I²C-SDA I²C SDA access point - bidirectional pin White
TP5 I²C-SCL I²C SCL access point - bidirectional pin White
TP9 FSYNC FSYNC access point - bidirectional pin White
TP55 AMUX Analog multiplexer output monitoring point White
TP12 RSTB System reset signal output monitoring point White
TP3 FS0B Fail-safe output monitoring point White
TP10 INTB INTB output monitoring point White
TP52 FCCU0 FCCU0 fault monitoring input pin access point White
TP53 FCCU1 FCCU1 fault monitoring input pin access point White
TP6 STBY STBY input pin access point White
TP2 PGOOD PGOOD input pin access point White
TP7 PWRON Power on input pin access point White